Cell Culture Contamination: How to Prevent Fungal, Yeast, and Bacterial Cell Culture Contamination | Corning

You have put in a lot of effort to keep your cell cultures healthy. However, despite following aseptic techniques, cell culture contamination from chemicals, bacteria, or other unwanted microbes can still occur and ruin your hard work.

When cell culture contamination occurs, cells die, and hours of cell growth effort are wasted. But when cell culture contamination goes undetected, it can surreptitiously affect data quality and ultimately render products like vaccines or drugs unusable and unsafe. It may even call into question the legitimacy of past experiments.

It's important to prevent contaminants from affecting your work and to know how to detect cell culture contamination. Here's what life scientists should know about common microbial contaminants and the sources of that contamination.

Types of Cell Culture Contamination:

Types of Cell Culture Contamination:

1. Bacterial Cell Culture Contamination

Bacterial contaminants come from various sources, such as outside personnel, insects, and plants to unfiltered air, humidified incubators, media, and other factors. Generally, bacterial cell contamination is found through microbial cultures, Gram's stain test, visual turbidity, or the pH becoming acidic. Antibiotics, proper filtration, and rigorous disinfection can help with contamination control.

2. Yeast and Fungal Cell Culture Contamination

As with bacterial contamination, yeast and fungal contamination can originate from internal and external sources, such as staff, equipment, or unfiltered air. In addition to microbial cultures, yeast can be detected by their smell and visual cloudiness, while seeing particulates or mycelia is a sign of fungus. Prevention tactics for both are similar to those for bacterial contamination, except antimycotics should be used instead of antibiotics.

3. Viral Cell Culture Contamination

Unwanted viruses can enter the lab through original tissues, serum, staff, and cross-contamination. Viral contaminants are typically detected from co-cultivation, PCR testing, electron microscopy, assays, and in vivo testing. Viral cell culture contamination prevention tactics include ultrafiltration, chemical treatments, gamma-irradiated serums, vapor-phase LN2 storage of cell line stocks, and using animal-free products when possible.

4. Mycoplasma Cell Culture Contamination

Mycoplasma infection is a big problem and has been for a while. It's estimated that between the 1970s and 1990s, up to 15% of U.S. cell cultures were contaminated by mycoplasmas. Typically, contamination derives from contaminated cell lines, serum, media, staff, or biosafety cabinets.

Many infections can be identified through microbial cultures, Hoechst stains, specialized kits, or PCRs. Ultrafiltration, antibiotics, use of animal-free products, and vapor-phase storage are all helpful prevention techniques.

5. Cellular Contamination

No story exemplifies cellular contamination better than the HeLa saga. In the 1960s, a researcher discovered that 100% of that era's commonly used cell lines had been incidentally replaced with cells from the Henrietta Lacks cell line. As that anecdote illustrates, widespread cellular contamination can occur through cross-contamination of cultures. It can also happen due to cross-use of media from different cell lines and biosafety cabinets.

Generally, the only way to detect cellular contamination is through cell authentication, but there are many best practices to prevent it, such as working with only one cell line at a time, conducting thorough cleaning, and using vapor rather than liquid storage.

Aseptic Techniques Are Most Important to Combat Cell Culture Contamination

Biological and chemical contamination can pose serious risks to all stakeholders in science, from the lab technician to the individual in charge of the lab's bottom line to the patients who depend on products every day. As you work to avoid cell culture contamination in your lab, remember that there's no substitute for good aseptic techniques.

Those techniques — combined with the strategic use of antibiotics and antimycotics, cell repositories, and a robust contamination monitoring program — can protect you and your precious cultures from the world's unwanted tiny invaders.

Explore More Resources to Prevent Cell Culture Contamination

Products To Assist in Your Cell Culture Contamination Discovery and Prevention