Pluripotent stem cells (PSCs) have the potential to become any cell type of the adult body and do not exist in the human body except for a brief period in early embryonic development. Investigators culturing these cells, which include human embryonic stem cells (hESCs) and induced pluripotent stem cells (iPSCs), need to carefully manage the cells' microenvironment to help them maintain pluripotency.
According to Padilla, scientists can prevent unwanted differentiation of PSCs by growing them on Corning® Matrigel® matrix, a widely used ECM derived from mouse Engelbreth-Holm-Swarm sarcoma cells, along with managing other factors such as media composition. Corning offers a reduced-variability, hESC-qualified Matrigel matrix product that's pre-screened for stem cell applications.
Multipotent stem cells, also known as adult stem cells, exist in specific locations in the adult body and can differentiate into a limited number of cell types. Choosing the proper coating for bioproduction can help researchers and manufacturers mimic the in vivo environment for each cell type. For example:
- Neural stem cells in the body make important attachments with laminins in the extracellular matrix. Cell culture surfaces that contain laminin help replicate this environment for neural stem cells, and including poly-d-lysine, poly-l-lysine, or poly-l-ornithine can improve neurite outgrowth.
- Mesenchymal stem cells (MSCs) have been investigated in a variety of clinical trials and can differentiate into bone, skin, fat, muscle, and other cell types. MSCs themselves produce ECM proteins, creating an extracellular web. That can be problematic inside bioreactors, so many investigators coat bioreactor surfaces with collagen or fibronectin. Attachment to these ECM proteins sends a signal that prevents MSCs from making their own ECMs.
- Hematopoietic stem cells, which can develop into all blood cell types, are usually cultured in suspension and do not require a coated vessel.
Beyond choosing a coating that's compatible with a specific type of stem cell, investigators need to optimize coatings depending on the application and the desired cell fate. In addition to Matrigel Matrix, Corning offers extensively tested natural and synthetic forms of Fibronectin, Vitronectin, several variants of Laminins, and Collagen, plus pre-coated tissue culture products.
Some cells do best with a coating made from a mixture of ECM proteins, and investigators should optimize the overall concentration of protein as well as the ratios of ECM proteins in a mixture.
The cost of stem cell coatings is also a key consideration. For products intended to be offered to patients, it's important to find ways to drive down the cost of final therapeutic products. Optimizing protein concentration will help ensure coatings are not using costly proteins at unnecessarily high concentrations.
For guidance on choosing and optimizing coatings for stem cells, see Corning's Cell Culture Surfaces Product Selection Guide and other cell culture surface resources.