Some years ago, NTT Advanced Technology performed a study to review what were the causes for which networks failed. The result, 98 percent of installers and 80 percent of network owners reported that fiber connector contamination was the greatest cause of network failure.
On the other hand we have Cisco, where in their “Inspection and Cleaning Procedures for Fiber-Optic Connections” mentions that “any contamination in the fiber connection can cause failure of the component or failure of the whole system” (1) and that “even microscopic dust particles can cause a variety of problems for optical connections” (1)
Additionally, in the SIGCOMM (Association for Computing Machinery's Special Interest Group) conferences in 2017, published a white paper regarding the “Root Causes for Packet Corruption” reporting that the connector contamination contributes from 17 percent to 57 percent for the packet corruption.
The previous information is more than a confirmation of what any installer is already aware of, the importance of cleaning the connector end face, but also at the same time validates the struggle the everyone knows, the desire to reach clean connectivity.
When the connector end face is clean, we will have no issues transmitting the light from one point to another. However when we have dirt, or any particle that can cause contamination present in the end face of our connectors, we will see an impact of the amount of light being transmitted, meaning a degradation of the signal or even a full link failure, that will be recognizable by the presence of strong levels of back reflection and insertion loss.