We have categorised our data centre frequently asked questions into four areas for your convenience. Please choose from the below to quickly navigate to the desired section.
Frequently Asked Questions
Frequently Asked Questions
General Questions
-
What is a Data Centre?
A data centre is a building or portion of a building whose primary function is to house a computer room and its support areas.
-
What TIA Standards Cover Data Centres?
TIA-942 is the TIA standard that covers data centres.
-
What Physical Cable Topology is Recommended by TIA-942?
TIA-942 recommends a Star topology.
-
What is Star Topology?
A topology in which telecommunications cables are distributed from a central point.
-
What are the Four Levels of Redundancy Called in TIA-942?
- Rated 1 (Basic)
- Rated 2 (Redundant Components)
- Rated 3 (Concurrently Maintainable)
- Rated 4 (Fault Tolerant)
-
What are the Recommended Optical Fibre Connectors According to TIA-942?
- LC connector for one or two fibre connections
- MPO connector for connections requiring more than two fibres
-
What is an LC Connector?
LC (Lucent Connector) is a type of fiber connector. Designed for high-density connections and supports SFP and SFP+ transceivers.
-
What is an MPO Connector?
MPO (multifiber push-on) is a type of fibre connector for ribbon cables with four to twenty-four fibres. Designed for high-density connections.
-
What is an Equipment Distribution Area (EDA)?
The computer room space occupied by equipment racks or cabinets.
-
What is a Main Cross-Connect?
Main cross-connect (MC) - The centralized portion of the backbone cabling used to mechanically terminate and administer the backbone cabling, providing connectivity between equipment rooms, entrance facilities, horizontal cross-connects, and intermediate cross-connects.
-
What is Main Distribution Area (MDA)?
The space in a data centre where the main cross-connect is located.
-
What is Storage Area Network (SAN)?
SAN is a high-speed network that uses the Fibre Channel transmission protocol to interconnect different kinds of data storage devices with associated data servers on behalf of a larger network of users.
-
What is Telecommunications Room (TR)?
Telecommunications room (TR) - An enclosed space for housing telecommunications equipment, cable terminations, and cross-connects. The TR is the recognized cross-connect between the backbone and horizontal cabling.
-
What is Main Distribution Area (MDA)?
Main distribution area is the space in a computer room where the main cross-connect is located.
-
What is Structured Cabling?
Structured cabling is a cable infrastructure that provides an organised, standardized to cable network that enables simple moves, adds, and changes (MAC) to a network.
-
What is the Cross-Connect?
A facility enabling the termination of cable elements and their interconnection or cross-connection.
-
What is the Interconnect?
Structured cabling hardware used to connect backbone or horizontal cables.
-
What are the Steps in the Data Centre Design Process?
- Estimate equipment telecommunications, space, power, and cooling requirements of the data centre at full capacity. Anticipate future telecommunications, power, and cooling trends over the lifetime of the data centre.
- Provide space, power, cooling, security, floor loading, grounding, electrical protection, and other facility requirements to architects and engineers. Provide requirements for operations centre, loading dock, storage room, staging areas, and other support areas.
- Coordinate preliminary data centre space plans from architect and engineers. Suggest changes as required.
- Create an equipment floor plan including placement of major rooms and spaces for entrance rooms, main distribution areas, intermediate distribution areas, horizontal distribution areas, zone distribution areas, and equipment distribution areas. Provide expected power, cooling, and floor loading requirements for equipment to engineers. Provide requirements for telecommunications pathways.
- Obtain an updated plan from engineers with telecommunications pathways, electrical equipment, and mechanical equipment added to the data centre floor plan at full capacity.
- Design telecommunications cabling system based on the needs of the existing and planned future equipment to be located in the data centre.
Multi-Tenant Data Centre
-
What is a Multitenant Data Centre?
A multitenant data centre (MTDC), also known as a colocation data centre, is a facility where organisations can rent space to host their data. MTDCs provide the space and networking equipment to connect an organisation to service providers at a minimal cost. Businesses can rent to meet varying needs – from a server rack to a complete purpose-built module. The scalability of usage provides the business benefits of a data centre without the high price. (April, 2018. Fahey, L. and Robinson, T., Multitenant data centres are key to managing data without breaking the bank, Cabling Installation & Maintenance)
-
What is Meet-me-room (MMR)?
Location in a multitenant data center where telecommunications companies can physically connect to one another and exchange data.
-
What is Cage?
An enclosure that subdivides multitenant data centre space within the building using mesh walls, a door, security panels, etc.
-
What is Latency?
Latency is the amount of time it takes to get a response.
-
What is Cloud Computing?
Cloud computing is the practice of storing, managing, and processing regularly used computer data on multiple remote servers that can be accessed through the internet.
-
What is a Private Cloud?
A private cloud is a dedicated cloud infrastructure, designed with the needs of a single business.
-
What is a Public Cloud?
A public cloud is a multi-tenant/shared infrastructure, typically owned and managed by a third party.
-
What is a Hybrid Cloud?
A hybrid cloud is the combination of private cloud and public cloud services in a single hosting solution.
Network Monitoring
-
What is Network Monitoring?
Network monitoring is the use of a system that constantly monitors a network for performance, usage, failing components, and outside threats, and notifies in case of potential issues.
-
Why Network Monitoring?
Essential to ensuring the success of your network system, network monitoring can automatically detect and respond to threats and performance issues.
-
What is Port Tapping?
Port tapping is a method of extracting data out of a live data link to enable network monitoring.
-
What Does “TAP” Stand For?
In the telecommunications industry, “tap” is not an official acronym, but some vendors have created an acronym “test/traffic access port” for the “tap” term. The phrase “tapping” was originally used due to the surveillance nature of connecting into and monitoring communications.
-
What is a Coupler?
A coupler, also called a splitter, is a passive device that takes a single input of optical light and divides it into two or more outputs. (It can also take two or more inputs of light and combine them into a single output.)
-
What are Split Ratios?
A split ratio refers to the percentage of output power going to the live traffic receiver versus the output power going to the monitoring device. In example, if you have a 70/30 split ratio on your tap module, 70 percent of your power is going to the live receiver while 30 percent is going to the monitoring device.
-
What is the Maximum Distance from the TAP Port to the Monitoring Device?
The supportable monitor link lengths are addressed on a case-by-case basis for the different protocol data rates due to the limitation of the monitor link length for unequal split taps and varying monitor equipment receiver sensitivity. For multimode fibre channel applications, the maximum distance of the monitor link shall not exceed 20 meters direct monitor equipment interconnection for all multimode applications.
Data Centre Architecture
-
What is Serial Transmission?
Data is transmitted over a single pair of fibre with one fibre for transmit (tx) and one fibre for receive (Rx).
-
What is Parallel Optics Transmission?
Uses a parallel optical interface to simultaneously transmit and receive data over multiple fibres, typically used in short-to-mid-reach applications.
-
What is Wavelength-Division Multiplexing (WDM) Transmission?
A technology which multiplexes a number of optical signals onto a single fibre by using different wavelengths of laser light.
-
What is BiDi Transmission?
Proprietary network transmission protocol using 2x20G lanes at two different wavelengths.
-
What is the Spine-and-Leaf Architecture?
Two-tier network comprising of spine switches and leaf switches.
-
What is the port breakout?
Breaks 40/100G ports into 4x10 and 4x25G ports.
-
What is TOR?
Top of rack is one common architecture of switch-to-server connections. The switch is placed at the top of the rack for easier accessibility and clearer cable management.
-
What is MOR?
Middle of row. The switch is placed in the middle of the row to reduced cable lengths.
-
What is EOR?
End of row. The switch is placed at the end of the row. Each server in individual racks are directly linked to an aggregation switch eliminating the use of individual switches in each rack.
-
What is the Data Centre Interconnect (DCI)?
The networking of two or more data centres to achieve business or IT objectives. This interconnectivity enables to work together, share resources and pass workloads between data centres.