Corning® Astra™ Glass Chosen for Samsung Display’s Quantum Dot Displays

News Releases
Display Glass
Corning® Astra™ Glass Chosen for Samsung Display’s Quantum Dot Displays
Corning® Astra™ Glass Chosen for Samsung Display’s Quantum Dot Displays
CORNING, N.Y. | Corning Incorporated | Março 21, 2022
Corning and Samsung Display build upon nearly half a century of collaborative innovation to advance emerging display technologies

Corning Incorporated today announced that Samsung Display Corporation (SDC) has selected Corning® AstraGlass for SDC’s new line of Quantum Dot (QD) display panels, which are key to enabling large-size TVs and monitors that feature vivid, intense colors.

QD technology offers advanced benefits to the viewing experience, providing a wider viewing angle, better response time, enhanced color performance, and increased efficiency – all within a thin form factor – when compared with other display technologies.

SDC’s QD display panels are featured in several high-end sets that will be commercially available this year.

“Astra Glass brings performance that is critical to crafting a powerful panel and delivering immersive, life-like displays,” said Han Yim, business director, High Performance Displays and Display Innovations, Corning. “QD displays are poised to raise the world’s expectations of picture quality, and Astra Glass is vital to advancing emerging display technologies.”

Astra Glass provides the optimal blend of attributes critical for the intricate and high-temperature QD manufacturing process, which requires two pieces of high-quality display glass. Corning’s current Display glass portfolio offers high-performance, exceptionally pure, and thin substrates optimized for advanced and emerging display technologies.

About Corning Incorporated

Corning (www.corning.com) is one of the world's leading innovators in materials science, with a 170-year track record of life-changing inventions. Corning applies its unparalleled expertise in glass science, ceramic science, and optical physics along with its deep manufacturing and engineering capabilities to develop category-defining products that transform industries and enhance people's lives. Corning succeeds through sustained investment in RD&E, a unique combination of material and process innovation, and deep, trust-based relationships with customers who are global leaders in their industries. Corning's capabilities are versatile and synergistic, which allows the company to evolve to meet changing market needs, while also helping our customers capture new opportunities in dynamic industries. Today, Corning's markets include optical communications, mobile consumer electronics, display, automotive, and life sciences.

Compartilhar