Corning and Ford to Deliver Joint Research on Lightweight Glass Solutions at SAE World Congress and Exhibition

News

Corning and Ford to Deliver Joint Research on Lightweight Glass Solutions at SAE

Corning and Ford Deliver Joint Research at SAE

News Releases
Comunicación corporativa
Corning and Ford to Deliver Joint Research on Lightweight Glass Solutions at SAE World Congress and Exhibition
Corning and Ford to Deliver Joint Research on Lightweight Glass Solutions at SAE World Congress and Exhibition
CORNING, N.Y. | Corning Incorporated | abril 11, 2016

Corning Incorporated (NYSE:GLW) today announced that the company will be delivering a joint research paper with the Ford Motor Company about thin, lightweight glass for automotive windshields. This paper will be presented on Tuesday, April 12, during the SAE World Congress and Exhibition at the Cobo Center in Detroit, Michigan.

The research with Ford demonstrates the damage resistance and performance of a windshield constructed with three layers: Corning® Gorilla® Glass for Automotive as the inner layer, a plastic adhesive interlayer, and annealed soda lime glass as the outer layer. This construction was compared with windshields made of conventional soda lime glass.

“Our joint research focused on windshield laminate construction designs that deliver significant lightweighting, while still demonstrating high product performance in terms of stone impact,” said Thomas Cleary, manager of reliability sciences at Corning.

The lab research simulated the conditions of a stone impacting a windshield made with either the conventional glass or Gorilla Glass laminate constructions.

“These tests demonstrate that thin windshield constructions (equal to or less than 4 millimeters thick) made with conventional glass exhibit a high frequency of inner-ply fracturing, whereas laminates that include a layer of Gorilla Glass show zero occurrences of inner-ply breakage when subjected to the impact test,” said Cleary. “The windshields with Gorilla Glass provide a more damage-resistant and lighter solution.”

"Ford is eager to present this research with Corning and demonstrate why a windshield with Gorilla Glass is setting new innovation and performance standards for the automotive industry as demonstrated on the Ford GT,” said Chester Walawender, Body Exterior - Global Core Systems Engineering, Ford Motor Company.

The full details of this testing and the joint research paper will be presented during the SAE World Congress and Exhibition at the Cobo Center in room 313 B at 10 a.m. EDT.

Ford and Corning have worked together for more than four decades on emissions control technologies, and both companies are building on that long collaboration to innovate with Gorilla Glass for Automotive. Late last year, Corning and Ford announced that the Ford GT would be the first production vehicle to use lightweight Gorilla Glass in a windshield application.

Corning’s Environmental Technologies business will also be presenting technical papers during the SAE World Congress and Exhibition on the topics of next-generation substrates and filters for emissions control. 

Forward-Looking and Cautionary Statements

This press release contains “forward-looking statements” (within the meaning of the Private Securities Litigation Reform Act of 1995), which are based on current expectations and assumptions about Corning’s financial results and business operations, that involve substantial risks and uncertainties that could cause actual results to differ materially. These risks and uncertainties include: the effect of global political, economic and business conditions; conditions in the financial and credit markets; currency fluctuations; tax rates; product demand and industry capacity; competition; reliance on a concentrated customer base; manufacturing efficiencies; cost reductions; availability of critical components and materials; new product commercialization; pricing fluctuations and changes in the mix of sales between premium and non-premium products; new plant start-up or restructuring costs; possible disruption in commercial activities due to terrorist activity, armed conflict, political or financial instability, natural disasters, adverse weather conditions, or major health concerns; adequacy of insurance; equity company activities; acquisition and divestiture activities; the level of excess or obsolete inventory; the rate of technology change; the ability to enforce patents; product and components performance issues; retention of key personnel; stock price fluctuations; and adverse litigation or regulatory developments. These and other risk factors are detailed in Corning’s filings with the Securities and Exchange Commission. Forward-looking statements speak only as of the day that they are made, and Corning undertakes no obligation to update them in light of new information or future events.

Digital Media Disclosure

In accordance with guidance provided by the SEC regarding the use of company websites and social media channels to disclose material information, Corning Incorporated (“Corning”) wishes to notify investors, media, and other interested parties that it intends to use its website (http://www.corning.com/worldwide/en/about-us/news-events.html) to publish important information about the company, including information that may be deemed material to investors. The list of websites and social media channels that the company uses may be updated on Corning’s media and website from time to time. Corning encourages investors, media, and other interested parties to review the information Corning may publish through its website and social media channels as described above, in addition to the company’s SEC filings, press releases, conference calls, and webcasts.

About Corning Incorporated

Corning (www.corning.com) is one of the world’s leading innovators in materials science. For more than 160 years, Corning has applied its unparalleled expertise in specialty glass, ceramics, and optical physics to develop products that have created new industries and transformed people’s lives. Corning succeeds through sustained investment in R&D, a unique combination of material and process innovation, and close collaboration with customers to solve tough technology challenges. Corning’s businesses and markets are constantly evolving. Today, Corning’s products enable diverse industries such as consumer electronics, telecommunications, transportation, and life sciences. They include damage-resistant cover glass for smartphones and tablets; precision glass for advanced displays; optical fiber, wireless technologies, and connectivity solutions for high-speed communications networks; trusted products that accelerate drug discovery and manufacturing; and emissions-control products for cars, trucks, and off-road vehicles.

Compartir