While traditional cell culture flasks and dishes are reliable for day-to-day MSC research, they can’t yet account for the cell numbers that are needed for clinical applications. As capacity increases in traditional cell culture models, this can only be achieved by adding more vessels, which requires more incubator space.
Novel technologies like stacked vessels address this by concentrating growth surface area into a smaller volumetric space. Multi-layer vessels, such as Corning’s CellSTACK® chambers, consolidate surface area and streamline routine tasks like feeding and harvesting, supporting early scale-out. This platform also scales with the user. Process development may start with a one-layer cell stack of 636 cm2 and eventually scale up to a 40-layer system, with each vessel consisting of 25,440 cm2 of cell culture volume. As programs grow into allogeneic pipelines and multiple indications, higher-density planar formats become more practical.
Another space-saving innovation is Corning’s® HYPERFlask®, which is engineered with reduced headspace due to its gas-permeable layers. This allows for significantly more surface area in a smaller volumetric footprint. It also has the advantage of higher-density, multi-layer formats that stack multiple gas-optimized planar layers within a single enclosed module. Standardized surface options, such as Corning’s CellBIND®, across all cell culture vessels ensure surface continuity. It incorporates a net negative charge in the cell culture surfaces, making them more wettable and facilitating better cell attachment and growth from early development through later optimization.
Corning® HYPERStack® vessels further extend this benefit through the addition of 12-layer and 36-layer configurations, which deliver thousands of square centimeters of growth area. According to Sherman, HYPERStack vessels provide a very high cell growth surface area (up to ~18,000 cm² per vessel) while maintaining a footprint that fits easily into standard incubators. This allows many high-density vessels to run in parallel without requiring additional incubator space.
In recent years, the increasing demand for MSCs to support large-scale therapeutic applications has prompted developers to explore alternatives with higher cell surface areas and more automated systems. The Corning CellCube® modules represent a promising solution for achieving high-yield MSC expansion in a compact footprint while offering enhanced process control. The CellCube-100 module, with an impressive surface area of 85,000 cm², can be combined with up to four other modules in a single batch to deliver a total growth area of 340,000 cm². This scalability, paired with its small physical footprint, makes the CellCube system another efficient tool for meeting the demands of clinical and commercial cell production.
What sets the CellCube system apart is its ability to combine the characteristics of stack vessel culture with the advantages of a bioreactor system. This integration enables better control of critical process parameters, such as nutrient delivery, gas exchange, and waste removal while also facilitating the harvest process. The modular design also supports consistent workflow execution and minimizes operator variability, making it ideal for high-throughput manufacturing. Since cells are cultivated within enclosed modules, the CellCube system offers a strategic advantage for exosome production, providing a controlled environment to maximize the yield and quality of these valuable therapeutic components. As MSC therapies continue to expand, the CellCube system provides an innovative and scalable solution to optimize both cell and exosome production aligned with the Corning closed-system solution.