The following article originally appeared on October 2, 2017 in The Cell Culture Dish here.
For the past 30 years, Corning Matrigel matrix has been used by researchers across the globe in essential applications through to cutting-edge, life-changing research. The number of citations for Matrigel matrix recently climbed over 10,000 citations and spans applications areas from cancer research to stem cells, and from organoid cultures to neuroscience.
Researchers have turned to Matrigel matrix, a solubilized basement membrane, over and over again to create more in vivo-like environments, whether it be for 2D or 3D cell culture applications.
Matrigel matrix is available is several formulations and can be used in a variety of different ways. With this flexibility comes the opportunity for expert advice and guidance to optimize the product selection and protocols most appropriate for particular cell types or applications. Corning published “The Ultimate Guide to Matrigel matrix” to share some of the best tips, tricks and expert advice. We encourage you to request your copy of the guide, available in both electronic and hard copy versions.
About Our Experts
Katie Slater and Paula Flaherty are part of an extensive team of scientists that manufacture, test and develop products for applications that are used to modulate the in vitro behavior of cells via extracellular matrix proteins, cell culture surfaces, media and cultureware design. Paula is a member of the Corning Life Sciences leadership team as Technology Manager and of the Discovery Labware R&D team since 1984. She has extensive experience in developing cell based assays. Katie, a Senior Scientist since 2000, is a subject matter expert for the Corning extracellular matrix product line, focusing on the isolation, manufacture and testing of Corning Matrigel matrix and other clinically important extracellular matrix proteins.
Can you thaw Matrigel matrix overnight?
Yes, you can thaw Corning Matrigel matrix overnight in a refrigerator. First submerge Matrigel matrix vials in an ice bucket filled with ice at 2°C to 8°C. Place the covered ice bucket toward the back of the refrigerator where it will not be subjected to temperature change. Use an adequate amount of ice so that the Matrigel matrix vial is in ice for the entire thawing process (not in cold water). Once thawed, swirl the vials in ice to ensure the material is evenly distributed.
What is the difference in phenol-red containing and phenol-red free formulations of Matrigel matrix?
Phenol red-free formulations are manufactured using DMEM that does not contain phenol red, so as a result the product is colorless. Phenol red-free formulations are recommended for assays that require color detection. Phenol red may exhibit estrogenic effects, so we recommend using phenol red-free Matrigel matrix if estrogenic effects are an application concern.
Phenol red containing formulations are manufactured with DMEM containing phenol red. The color variations that are observed in frozen & thawed Matrigel matrix products that contain phenol red may range from straw yellow to dark red. This is due to the interaction of carbon dioxide with the bicarbonate buffer and the phenol red. The color variation does not affect product efficacy, and will disappear upon equilibration with 5% CO2.
I am thinking about moving to pre-coated plates. Can you tell me the benefits and drawbacks of plates precoated with Matrigel matrix?
Corning Matrigel matrix precoated plates are well suited in circumstances where a specific application protocol is being followed. Test conditions necessary for optimal cell functionality, including Matrigel concentration and volume, have been empirically demonstrated and a protocol provided. Examples of such assays are angiogenesis tube formation, primary hepatocyte culture, tumor invasion and stem cell culture; all of which benefit from proven, published protocols and the reliability of precoated plates. Manufacturing consistency, quality control testing, shelf life, stability testing and off-the-shelf use are key benefits.
For less established protocols, a drawback to precoated plates is the inability to titrate concentration and volume to drive to the functional cell response desired.
If a specific Matrigel matrix formulation is needed, Corning can work with you to provide a custom precoated Matrigel matrix solution in various formats, ranging from high-throughput for drug screening and toxicity applications to multi-well plates and flasks for cell culture. Please contact your Corning representative for details on custom Matrigel matrix custom solutions.
What is the proper storage temperature of Matrigel matrix?
Store Matrigel matrix at -20°C in a non-frost-free freezer. If you aliquot Matrigel matrix after the first thaw, store at -70°C or -20°C in a non-frost-free freezer using polypropylene or other compatible tubes that can withstand the cold temperature.
What are the minimum protein concentrations required for Matrigel matrix to form a gel?
The minimum protein concentration may be application dependent. You should use the lot specific protein concentration from the Certificate of Analysis to determine the optimal protein concentration range for your specific application. In general, Matrigel matrix diluted to a concentration of 3 mg/mL will form a firm gel. For in vivo applications do not dilute Matrigel to a final concentration below 4 mg/mL.
My lab has begun culturing MSCs at small scale. I saw that you have several choices when it comes to Matrigel matrix. Do you have a recommendation for which would be best?
The choice of substrate for mesenchymal stem cells (MSC) in planar cultures is best determined in the context of the entire in vitro environment, including the media. For serum containing media, substrates such as tissue culture treated (TC) or Corning CellBIND® surfaces are recommended. If you are using xeno or animal free media then we recommend Corning human fibronectin, Corning PureCoat™ fibronectin mimetic or Synthemax® surfaces.
In a 3D culture environment, MSCs have been cultured, co-cultured and differentiated on Matrigel matrix. Li. et. al., have demonstrated that 3D co-culture of BM-MSCs and eccrine sweat gland cells in Matrigel matrix promotes trans-differentiation of BM-MSCs (J Mol. Histol. 2015. 46:431-8). Matrigel matrix can also be used in vitro as a thick gel where cells can be embedded or seeded on top of the matrix layer (overlay method). Furthermore, the elastic moduli of Matrigel matrix can also be tuned by providing softer or stiffer gels to suit application need (See Corning Application Note CLS-AC-AN-449).
Our lab is using Corning Matrigel matrix to co-culture cells in 3D on a microfluidic chip. I read that we should be using a thick layer of Matrigel matrix, but I’ve noticed that the amount of Matrigel matrix keeps going down each day and I need to add more. Do you have any recommendations so I can avoid having to add Matrigel matrix or should I be adding something else instead?
Combining microfluidics and extracellular matrices (ECM) has shown to be a promising system to create more in vivo-like 3D environments. Some publications have shown different methods to craft such environments. For example:
Bruzewicz, et al. (Lab Chip. 2008 May;8(5):663-71. doi: 10.1039/b719806j. Epub 2008 Mar 20) have shown that using a soft-lithographic molding gel such as Matrigel matrix or Collagen to encapsulate cells in a microfluidic channel and chambers yielded a permeable system where media could flow to feed the encapsulated cells.
Jang, et al. (ACS Appl Mater Interfaces. 2015 Feb 4;7(4):2183-8. doi: 10.1021/am508292t. Epub 2015 Jan 21) have applied flow across the bulk gel during the gelation process to orient the ECM components with the direction of the flow, compared with randomly cross-linked Matrigel matrix.
Tumour-on-a-chip: microfluidic models of tumour morphology, growth and microenvironment is a recently published review article by Tsai, et al. (J R Soc Interface. 2017 Jun; 14(131): 20170137).
Understanding the biophysical cues of the 3D environment such as topography, stiffness, viscosity and porosity have shown to be important to mimic the in vivo environment. Modulating and tuning the tensile strength of the Matrigel matrix gel in a 3D environment may be beneficial to provide softer or stiffer gels to suit application need. Empirical studies may show that a stiffer gel (higher protein concentration), may reduce dilution of the gel caused by the flow in the microfluidic chip.
As we keep learning about these techniques and methods, we recommend you reach out to our global scientific support team to help you find the right solution for your work.
What do you recommend as the best method for harvesting spheroids from Matrigel matrix?
Corning Dispase or Corning cell recovery solution is recommended for recovering cells cultured on Corning Matrigel matrix. The Dispase enzyme will yield a single cell suspension more gently and effectively than trypsin, collagenase, or other proteolytic enzymes, as it minimizes cell damage and surface protein cleavage. Corning cell recovery solution is another option for cells/spheroids cultured in Matrigel matrix. This solution will allow non-enzymatic cell retrieval in small clumps and is frequently used in metabolic/RNA recovery experimentations. It can de-polymerize a thick Matrigel matrix layer at 4°C and facilitate cell retrieval. Cell-cell interactions can also be disrupted through the use of chelators and/or proteolytic enzymes such as Trypsin or Dispase. Using the solution at low temperature (on ice) and applying mechanical disruption such as pipetting or the use of an orbital shaker are other alternative methods to de-polymerize the Matrigel matrix.
How should I change media in a culture with Matrigel matrix? And how often?
Avoid disrupting the Matrigel matrix layer or coating by carefully aspirating and adding medium. When aspirating the spent medium, tilt the vessel to pool the medium to one side minimizing contact with the Matrigel matrix layer. When adding medium, if possible, rest the tip along the side of the vessel and allow the liquid to slowly flow down and across the growth surface.
Cell culture medium should be changed as necessary to maintain the proper culture environment.
My question is about the future potential for Matrigel. Specifically, I’m interested in how Matrigel might be used as a bioink for 3D bioprinting. Have people been bioprinting with their cells in a Matrigel mixture? If so, what kinds of results have been seen (any publications I could read?) Besides bioprinting, are there any other new 3D cell culture techniques on the horizon?
Corning Matrigel is poised to play an integral role in many 3D cell culture techniques, including bio-printing. Scientists have been using it to print many different tissues types. Listed below is a table that summarizes articles that have been published in this space recently that use Corning Matrigel in 3D bioprinting. Other 3D techniques that use Matrigel matrix are microfluidics and organ-on-a-chip for scaffold systems. For scaffold-free systems, Corning provides spheroid plates where the user can generate and analyze 3D spheres formed by one or more cell types. There is often a cross use of spheroid plates with Matrigel matrix if the customer is interested in generating self-assembled 3D structures.
Literature Summary: Use of Corning Matrigel Basement Membrane Matrix in bio-printing
I am working on a cell invasion assay using melanoma cells. I have found mixed information online about the thickness of the Matrigel matrix I should use, how to load it, and how cells should be passaged for different cancer cell types. Could you please advise or provide a resource? Thanks.
Invasion assays for cancer cell analysis is an extensively studied and published application area where Matrigel matrix has been effectively used. To establish a reproducible assay many factors need optimization, some examples are:
- Cell seed
- Chemoattractant type and concentration
- Matrigel matrix protein concentration and volume (which relates to thickness)
- Duration of the assay
- Use (or not) of serum starvation prior to the assay
- Selection of the appropriate control
As a starting point we recommend coating an 8 micron 24-well insert (Corning Cat. No. 353097) with 0.1 mL of 200 to 300 μg/mL of Corning Matrigel matrix (Corning Cat. Nos. 354234 and 354230) per insert. Titration of the concentration and volume will help to tighten the conditions for your assay. There are many helpful documents on the Corning website, including:
Here are some examples from other literature:
- Current Opinion in Cell Biology, Vol 36, Oct 2015, 13-22. Modes of cancer cell invasion and the role of the microenvironment, G. Clark, D. Matic Vignjevic
- Cancer Res. 2016 Aug 15;76 (16):4595-7. Extracellular Matrix Invasion in Metastases and Angiogenesis: Commentary on the Matrigel "Chemoinvasion Assay", Albini A.
What analytical methods are used to evaluate 3D cultures in Matrigel matrix?
Cell viability, immunofluorescence analysis and advanced imaging technologies are frequently used to interrogate Matrigel matrix enabled 3D cultures.
Viability can be measured via the detection of DNA synthesis in proliferating cells, based on the incorporation of 5-ethynyl-2′-deoxyuridine (EdU). A protocol can be found below:
A chemical method for fast and sensitive detection of DNA synthesis in vivo
The labs of Mina Bissell at Lawrence Berkeley National Laboratory and Joan Brugge at Harvard Medical School have published extensively on 3D models using Matrigel matrix and have included a widely used immunofluorescence analysis preparation method. A few protocols can be found below:
ErbB2, but not ErbB1, reinitiates proliferation and induces luminal repopulation in epithelial acini
Three-dimensional culture models of normal and malignant breast epithelial cells
Many labs have studied 3D architecture utilizing advanced imaging technologies. In the publication by Jorgens, et al. many of these methods were employed and are covered in the materials and methods section of the paper. Spheroid/organoid size and morphology, as well as cryogenic techniques, volume electron microscopy, and super-resolution light microscopy have been used to study phenotypic and functional attributes. A protocol can be found below:
Finally, recovery of cells from 3D Matrigel matrix cultures to be used for cell number determination, RNA isolation, and qPCR analysis can be accomplished using Corning cell recovery solution. Using the solution at low temperature (on ice) and applying mechanical disruption such as pipetting or the use of an orbital shaker will help de-polymerize the Matrigel matrix. Cell-cell interactions can be disrupted through the use of chelators and/or proteolytic enzymes such as Trypsin or Dispase3
Is there a set of best practices for imaging using fluorescent labeling with Corning Matrigel matrix? Is there a specific type of Matrigel I should be using or a protocol you can recommend?
There are many methods that can be used to fluorescently label and image cells in a Matrigel matrix system. Here we cover three topics: labeling cells in Matrigel matrix assays, immunofluorescence analysis for surface markers (such as those used in 3D culture and culture of pluripotent stem cells), and fixing and embedding cells in Matrigel matrix prior to sectioning.
Staining has been done with all types of Matrigel matrix. However, the use of phenol red-free Matrigel matrix will reduce autofluorescence. We also recommend the use of Falcon® culture slides (Corning Cat No. 354180) for in situ analysis such as immunofluorescence studies. The slides are a specially cleaned and triple rinsed glass with an upper polystyrene chamber.
Labeling Cells in Matrigel Matrix Assays
Labeling is easiest if you culture cells on a thin coat of Matrigel matrix or you image cells from a Matrigel matrix assay such as invasion or tube formation. Most fluorescent methods can be used directly as described by manufacturers. In addition to pre-labeling intrinsic dyes such as green fluorescent protein (GFP), Calcien AM and DiI are frequently used, depending on how long the dye is required to remain stable.
Protocol for labeling cells using Corning Calcein AM dye:
Corning Calcein AM dye is generally used at 8 μg/mL in Hanks Balanced Salt Solution (HBSS). HBSS is recommended because the use of culture medium results in autohydrolysis of the label, which results in unacceptably high backgrounds. Remove medium from the plates being careful to avoid disruption of the matrix by gently aspirating the medium using a Pasteur pipet. Wash the plate with HBSS and repeat the wash a second time. Label the cells by adding 8 μg/mL Calcein AM in HBSS and incubate for 30 to 40 minutes at 37°C, 5% CO2. Gently remove the labeling solution and wash twice with HBSS. The plate is now ready for image acquisition using an automated imager or for taking pictures using a fluorescent microscope. NOTE: Once hydrolysis occurs, Calcein AM leaks out of cells resulting in a higher background. Labeled plates can be stored at 4°C for 1 to 2 hours with minimum increase in background.
Immunofluorescence Analysis with Matrigel Matrix
Immunofluorescence analysis preparation methods using Matrigel as a 3D matrix have been widely published and are represented by this method:
Protocol for immunofluorescence analysis:
Using the above cited method, “structures were fixed either in 2% paraformaldehyde at room temperature for 15 min. or in methanol:acetone (50:50) at -20°C for 10 min. Fixed structures were washed three times in PBS:glycine (130 mM NaCl, 7 mM Na2HPO4, 3.5 mM NaH2PO4, 100 mM glycine) for 15 min. each. The washed structures were blocked first in IF buffer (130 mM NaCl, 7 mM Na2HPO4, 3.5 mM NaH2PO4, 7.7 mM NaN3, 0.1% BSA, 0.2% Triton™ X-100, 0.05% TWEEN® 20) plus 10% goat serum (GS) for 1–2 hr. and subsequently with 2° blocking buffer (IF buffer containing 10% GS and 20 μg ml−1 goat anti-mouse F(ab′)2) for 30–45 min. Primary antibodies were diluted in 2° blocking buffer and incubated overnight at 4°C. Unbound primary antibodies were removed by washing three times in IF buffer for 15 min. each. Anti-mouse or anti-rabbit secondary antibodies coupled with Alexa Fluor® dyes (Molecular Probes) were diluted in IF buffer containing 10% GS and incubated for 45–60 min. Unbound secondary antibodies were washed as described above. Finally, the structures were incubated for 15 min. with PBS containing 5 μM TO-PRO®-3 (Molecular Probes) and 0.5 ng ml−1 DAPI (Roche) before being mounted with the anti-fade agent ProLong® (Molecular Probes). Confocal analyses were performed.”
Fixing and Embedding Cultures in Matrigel Matrix
Rijal and Li have recently published a method for histological studies:
Sci Adv. 2017 Sep; 3(9): e1700764. A versatile 3D tissue matrix scaffold system for tumor modeling and drug screening, Girdhari Rijal and Weimin Li
Protocol for histology and immunostaining:
“The cell-laden scaffolds from the tissue cultures were washed twice with ice-cold 1X PBS and fixed in 10% neutral buffer formalin solution for 24–48 hours at 4°C. After rinsing with cold 1X PBS, the 3D cultures were embedded into OCT or paraffin following standard protocols and sectioned at a thickness of 10 μm using a cryostat or a microtome. For the sections produced using the paraffin fixation, a deparaffinization and rehydration process was performed, followed by antigen retrieval using the tris-EDTA buffer [10 mM tris base, 1 mM EDTA solution, and 0.05% TWEEN 20 (pH 9.0)]. The sections were washed several times with water, stained with H&E or IF antibodies (corresponding primary and Alexa fluorophore–conjugated secondary antibodies) as described previously (Circ. Res. 100, 79–87 (2007), and imaged using light or fluorescence microscopy for further analysis.”
I am getting ready to move my ES cells from MEF cells to Matrigel matrix. Do you have any recommendations for the best method, and are there any special requirements for the media?
Corning Matrigel hESC-qualified matrix has been used extensively as a substrate for culturing human embryonic stem cells (hESC) and human induced pluripotent stem cells (hiPSCs) with numerous hPSC culture media such as mTeSR™1, TeSR™2, E8, and MEF conditioned media.
Transitioning hPSCs from mouse embryonic fibroblasts (MEFs) to Matrigel matrix does not typically require any special process steps. Cells can be plated in medium of your choice on Matrigel hESC-qualified matrix-coated vessels at the time of passage. You should optimize your passaging conditions based on the cell line used, media, and dissociation technique. You can watch a video on how to passage ES cells from MEFs to Matrigel hESC-qualified matrix on the Journal of Visual Experiments (JoVE) web site.
For further support or troubleshooting advice, feel free to reach to the Corning Scientific Support team.
Do all types of Corning Matrigel matrix support hESC culture?
Not always. Corning offers hESC-qualified Corning Matrigel matrix (Corning Cat. No. 354277) which is QC tested for hESC maintenance to ensure consistency, reproducibility, and reliability in performance. This product has been qualified for use with STEMCELL Technologies’ mTeSR™1 medium. It has been shown that human embryonic stem cells grown in mTeSR1 on Corning Matrigel matrix hESC-qualified matrix-coated plates for five passages remain undifferentiated by standard morphology and surface marker expression.
In addition, Corning BioCoat™ Matrigel matrix 6-well plates (Corning Cat. No. 354671) are ready to use and offer lot-to-lot consistency for culturing human ES cells while maintaining their ability for self-renewal and pluripotency. Although non-hESC-qualified Corning Matrigel matrix may work for this application, the results may vary because these products are not qualified for use with hES cells.
For more information, please see Corning Matrigel Matrix.