How to Set Up a New Cell Culture Lab from Scratch | Cell Culture Lab Startup Checklist | Corning

Starting a research lab is an exciting but daunting process. Decisions made now will set a course for your team's future research. While some aspects can be adjusted later, planning ahead and getting on the right course from the start can help prevent expensive and time-consuming detours.

Making a lab setup checklist can help. No matter what area of life science you focus on, you'll need to secure the right resources in three main areas: laboratory equipment, physical space, and supplies. Here are three key steps for your lab setup checklist:

Step 1: Identify Necessary Lab Equipment

To understand your laboratory space and layout needs, you'll first need to make a list of the equipment you'll need. Include both common lab tools and appliances such as freezers, centrifuges, pipets, and cell culture incubators, as well as more specialized instruments needed for your research.

Some expensive equipment might be available in an institutional core facility or shared incubator space, or you may be able to set up a sharing agreement with another lab. Outsourcing certain techniques may be a possibility. But if the equipment will have a central role in your lab's operations, it's more important to keep it onsite and fully under your control.

Consider sustainability when choosing equipment and planning your layout. Because laboratories tend to be heavy users of resources, selecting appliances that use less energy or water, or that take up less space can lead to considerable cost savings as well as lower environmental impacts in the long run.

Step 2: Find the Right Lab Space

Your lab space options will vary depending on your available capital and other resources. For startups, there are several options. You could obtain shared laboratory space in a startup incubator or co-working space, or you could sign a long-term lease in a commercial building. Local institutions and organizations will have more information. The California Life Sciences 2025 Startup Resource Guide, for example, lists incubator spaces serving the life sciences community in California, while the Massachusetts Life Sciences Center website does the same for Massachusetts.

If you're in academia, you will need to look at what your university or institution offers in the way of laboratory space for faculty. Consider the physical bench space and desk space your lab members will need, as well as equipment space and storage space.

When you find a space, assess the utility inputs, such as electric plugs, gas lines, water, and sinks, to make sure their placement works for your needs. Consider how your workflow will play out in the new space. Will there be enough counter space for your equipment? Do the traffic patterns make for a good flow, or will scientists bump into each other? Are desk spaces set far enough away from the principal work areas to not interrupt bench work? These questions—and others—will matter as you weigh your options.

Step 3: Stock Up With the Right Cell Culture Supplies

Start with the essential products to get your cell cultures going: cell culture flasks, media, cell culture surfaces, and microplates. This new lab startup sample kit can help you select the tools you need to succeed. In addition, a growing number of sustainably designed laboratory supplies are available—such as Corning EcoChoice™, presenting additional opportunities to plan for a more sustainable lab.

When planning your lab's startup, remember that it can take weeks or months to fully stock your inventory to suit your workflows. To make sure your lab members can enjoy a smooth, productive start to their projects, plan ahead to secure the resources needed for experiments.

You've Got This!

Starting a research lab can be challenging, but it can also be incredibly rewarding. Find colleagues who have gone through the process and ask them for advice. Plan more than you think you need to, and take time to get everything done safely and correctly. With this lab setup checklist in hand, you and your lab members can get a running start.

Ready to get started? Get 25% off lab supplies when you stock your new lab through Corning Life Sciences.

Find the Right Space

Your lab space options will vary depending on your available capital. You could share or borrow a starter space, Science says, or you could sign a long-term lease in a commercial building. An incubator could be an option, if you can find one near you. Local institutions and organizations will have more information; the California Life Sciences Association, for example, lists incubators and lab space by region, size, and available equipment.

When you find a space, assess the utility inputs — electric plugs, gas lines, sinks, and such — to make sure their placement works for your needs. Consider how your workflow would play out in the new space. Will there be enough counter space for your equipment? Do the traffic patterns make for a good flow, or will scientists bump into each other? Are desk spaces set far enough away from the principal work areas to not interrupt bench work? These questions — and others — will matter as you weigh your options.

Carefully Plan Modifications

If you're able to make changes to the space, great — just plan them carefully. Treat a lab renovation like you would a home renovation: Work with experienced professionals who can help you account for wet lab considerations (such as water or gas lines), pick out optimal countertop surfaces that can withstand spills, and select sturdy flooring material for minimal slip-and-fall risk. Your modifications will affect lab safety, so take extra caution during the planning process.

Lab Manager gives a peek into what renovations look like — but you can always start with modest upgrades, such as replacing the cabinetry, if your budget is lean.

Create Adaptable Protocols

Standardize and codify your care and maintenance protocols manuals and checklists, but leave room to amend them so you can adapt to the unexpected, as you did during the COVID-19 pandemic. For example, you might need to conduct your cleaning regimen more often than you did before the pandemic to account for increased containment risk. And now that social distancing merits staggered schedules and staffing changes, team-based experiment protocols might need to shift to account for evolving factors.

Stock Up With the Right Supplies

Start with the essentials to get your cell cultures going: cell culture flasks, filtration systems, well plates, media, and surfaces. This new lab start-up shopping list can help you get the tools you need to succeed.

Just remember that it can take weeks or months to fully stock your inventory to suit your workflows. You might not even realize that you need a piece of technology and or some supplies until you're midway through an experiment.

You've Got This!

Learning how to set up a new lab can be challenging, but it can also be incredibly rewarding. Start small, plan more than you think you need to, and take time to get everything done safely and correctly so that you don't have to fix mistakes or oversights down the line.

Ready to get started? Get 25 percent off on lab supplies when you stock your new lab through Corning Life Sciences.