3D cell culture is exploding. To capture the energy and excitement of this moment in research, Corning recently brought together industry leaders and innovators for a global virtual 3D Cell Culture Summit to share ideas and information, and to discuss the future of 3D applications, including spheroid, organoid and tissue models.
Access a Range of 3D Cell Culture Topics from a Roster of Global Speakers
Access a Range of 3D Cell Culture Topics from a Roster of Global Speakers
Objectives:
- Gather leading researchers from across the globe to discuss 3D applications as well as novel and advanced models
- Introduce new users to best practices and tips to get started in 3D cell culture
- Foster discussion among industry leaders on 3D workflow optimization, trends, and innovation
This event content is now available on demand.
Speakers and Panelists

Kacey Ronaldson-Bouchard, Ph.D.
: Kacey Ronaldson-Bouchard, Ph.D.Associate Research Scientist, Columbia University
Engineering Integrated Multi-Tissue Platforms for Modeling Systemic Human Pathologies
Bioengineered tissue platforms offer a new paradigm for modeling human pathophysiology and testing drug efficacy and safety. To model whole-body physiology and systemic diseases, we developed the biomimetic InterOrgan platform in which matured human tissues are connected in a way that allows maintaining distinct functionalities of different organs. Each tissue is cultured in its own optimized environment and integrated via recirculating vascular flow containing monocytes, by a matured and selectively permeable endothelial barrier. Tissues linked by vascular perfusion maintained their molecular, structural, and functional phenotypes over four weeks of culture, recapitulate multi-organ toxicity of doxorubicin and clinically relevant miRNA biomarkers, and show utility for immune-oncology applications.

Robert Vries, Ph.D.
: Robert Vries, Ph.D.Chief Executive Officer
Hubrecht Organoid Technology (HUB)
Understanding Mechanisms of Disease and Identifying Therapeutic Interventions with HUB Organoids™
HUB Organoids are one-of-a-kind models that can be developed from any epithelial disease and any patient, thus bridging the gap between the lab and the clinic and effectively bringing “patients inside the lab”. Thanks to accurately predicting patient response, organoids are already been used to test drug efficacy and toxicity and predict patient response based on in vitro sensitivity data. HUB Organoids faithfully recapitulate original patient disease allowing to reduce animal usage, accelerate drug development timelines, and optimize patient selections in clinical trials, thus contributing to reducing the high attrition rate of new drugs and making personalized medicine a reality. This talk will present an overview of how HUB Organoids have contributed to understanding mechanism of human disease and have successfully predicted patient response to treatment.

Sylvia Boj, Ph.D.
: Sylvia Boj, Ph.D.Chief Scientific Officer
Hubrecht Organoid Technology (HUB)
The Landscape of Emerging Inflammatory Diseases: Lessons Learnt from Organoids
The lack of preclinical cellular models that recapitulate human inflammatory diseases is a major setback in the study of non-oncogenic conditions with an inflammatory component. HUB Organoid Technology is the only technology capable of generating in vitro models from non-transformed or non-malignant cells, which has allowed us to successfully establish organoid models and design specific assays to study conditions such as Inflammatory Bowel Disease (IBD), Crohn’s Disease, Ulcerative Colitis, and COPD. This talk will present how HUB Organoids can be effectively used to model human inflammatory diseases and test novel treatment strategies.”

Nicolas Aznar, Ph.D.
: Nicolas Aznar, Ph.D.Young Investigator CRCN CNRS
Cancer Research Center of Lyon (CRCL), France
Counteracting Organoid Stemness Exhaustion by Controlling Stem Cell Microenvironment: On the Road to Standardization
Nowadays, stem cells (SCs) and their direct derivatives offer promising perspectives in regenerative medicine. Additionally, studying their properties, determination and plasticity turn out as determinant in understanding the development of various pathologies as dysregulation of their biology constitute the initiating step toward pathogenicity. Thanks to tremendous amount of publicly available protocols, isolating SCs is not critical anymore. Nonetheless, due to their sensitivity to microenvironmental changes, generation of organoids from SCs still remains challenging and researchers face technical issues in maintaining stemness phenotype to generate robust data. To overcome these obstacles, standard SC culture conditions still need to be further improved to gain in standardization and reliability.
In an effort to tackle these questions, we have developed a system that fine-tunes cellular microenvironment conditions mimicking optimized long term “high quality” SCs culture conditions improving therefore organoid technology reliability and performance.

Joshua Adam Bagley, Ph.D.
: Joshua Adam Bagley, Ph.D.Chief Scientific Officer, A:head Bio AG
Mirroring the human brain
Finding new therapies for brain diseases requires preclinical models and assays with increased clinical relevance. a:head aims to develop a human-based platform for generating complex brain-like tissue and analyzing neuronal network activity. Brain organoids are a biomedical revolution representing the most advanced in vitro experimental model of human brain. These 3D cultures mimic the structure and function of the brain with the promise of scalability to enable high-throughput screening of patient neural networks. This talk will cover our efforts toward the development of a brain organoid-based drug discovery engine.

Shuibing Chen, Ph.D.
: Shuibing Chen, Ph.D.Kilts Family Associate Professor, Director of Diabetes Program, Weill Cornell Medicine, Department of Surgery
Human Pluripotent Stem Cell-Derived Organoids for COVID-19 Disease Modeling and Drug Screening
hPSC-derived cells/organoids provide a platform to systematically evaluate the tropism and cellular response upon viral infection, which can be adapted to screen for anti-viral drugs. We assemble a large consortium team to create a panel of hPSC-derived cells/organoids to study SARS-CoV-2 tropism. By screening ten different type of cells and organoids, we found that lung, colon, heart, liver, pancreatic cells and neurons can be infected by SARS-CoV-2. Furthermore, we reported the first organoid-based screen and identified several drug candidates blocking SARS-CoV-2 entry. One identified drug, imatinib, is currently being evaluated in several phase 2/3 clinical trials globally.

Constanza Curotto
: Constanza CurottoField Application Scientist
Corning Life Sciences
Spotlight: Corning® Elplasia® plates
Join Corning Field Application Specialist Constanza Curotto for an overview of Corning® Elplasia® plates, which feature microcavity technology that simplify high volume spheroid production to deliver simple spheroid formation and culture, high density production as well as uniformity, reproducibility, and consistency.
Spotlight: 3D Cell Culture Workflow
Join Corning Field Application Specialist Constanza Curotto for an overview of Corning 3D Cell Culture solutions for spheroid, organoid and tissue models.

Benjamin D. Hopkins, Ph.D.
: Benjamin D. Hopkins, Ph.D.Assistant Professor, Department of Genetics and Genomic Sciences, Department of Oncological Sciences, Tisch Cancer Institute, Icahn School of Medicine at Mount Sinai
Pairing Comprehensive Genomics with Combination Drug Screening to Identify Mutation Specific Therapeutic Approaches
As tumors develop, tumor cells rewire their signaling and metabolic networks in order to sustain their hyperproliferative state. In doing so they can create tumor specific vulnerabilities. By pairing Whole Exome, Single Cell and RNA Sequencing with combination drug testing of three-dimensional organoid models our automated functional genomics pipeline works to uncover these tumor specific vulnerabilities and identify therapeutic strategies that can be evaluated in the clinic.

Iva Kelava, Ph.D.
: Iva Kelava, Ph.D.Postdoctoral Fellow
MRC Laboratory of Molecular Biology
Male Sex Hormones Increase Excitatory Neuron Production in Human Cerebral Organoids
Male-female brain differences have traditionally been difficult to clearly elucidate. Yet negating the existence of biological differences has detrimental consequences for all sexes and genders, particularly for the development of accurate diagnostic tools, effective drugs and understanding of disease. The most well-established morphological difference is size, with males having on average a larger brain than females; yet a mechanistic understanding of how this difference arises remains to be elucidated. Here, we use brain organoids to demonstrate that while sex chromosomal complement has no observable effect on neurogenesis, sex steroids, namely androgens, lead to increased proliferation of cortical radial glial progenitors and an increased neurogenic pool. Furthermore, transcriptomic analysis and functional studies demonstrate downstream effects on HDAC activity and mTOR pathway, both of which are also implicated in the male-biased conditions autism spectrum disorder and schizophrenia. Finally, we show that androgens specifically increase neurogenic output of excitatory neuronal progenitors, while inhibitory neuronal progenitors are not increased. These findings uncover a hitherto unknown role for male sex hormones in regulating excitatory neuron number within the human neocortex and represent a first step towards understanding the origin of human sex-related brain differences.

Mariusz Madej
: Mariusz MadejSenior Scientist of Oncology, Head of Biobanking
OcellO B.V. Leiden, the Netherlands
High content screening in organoids; combining complex 3D biology and 3D image analysis in a high throughput 384-well format
In recent years, the number of pre-clinical advanced in vitro models that use patient-derived cultures from various tissue has increased but their full potential in drug discovery has not been fully exploited. Often current assays lack sensitive or clinically relevant endpoint measurements, or they are not suitable for high throughput screenings. Therefore, we developed a unique screening platform that combines complex 3D biology with high content phenotype-based image analysis to provide precise visualization and quantification of various novel therapeutic effects on organoids derived from healthy and diseased tissue. This advanced pre-clinical drug screening platform helps to bridge the translational gap between in vitro and in vivo studies.

Florencia Madorsky Rowdo, Ph.D.
: Florencia Madorsky Rowdo, Ph.D.Postdoctoral Associate at Englander Institute for Precision Medicine, Weill Cornell Medicine
Characterization and Diagnostic Applications of Patient-derived Tumor Organoids
As part of the Englander Institute for Precision Medicine, the Tumor Organoid Platform is an active program focused on development of 3D patient derived tumor organoids (PDTO) from metastatic and primary anatomic sites, obtained through biopsies, surgical resections and rapid autopsy procedures. In this setting, the Tumor Organoid Platform has established a “living biobank” of 160 patient tumor organoids comprising 14 different tumor types. These models are used for High Throughput Drug Screening, the identification of new targets using CRISPR Cas9 Screenings and the generation of co-cultures with different cell types present in the tumor microenvironment, including immune cells and fibroblasts.

Hilary Sherman
: Hilary ShermanSenior Scientist, Corning Life Sciences
Tips and Tricks for 3D Cell Culture
This presentation will cover important considerations for optimizing 3D cell culture including both scaffold and scaffold free systems. The presentation will also discuss helpful tips and tricks for handling and downstream applications including staining, imaging and protein extraction from 3D cultures.

Richa Singhania, Ph.D.
: Richa Singhania, Ph.D.Director, The Starr Foundation Glioma Cerebral Organoid Translational Core, Weill Cornell Medicine
Tackling brain tumors with a new organoid model
This session will provide an overview of how brain organoids are used to model a Glioblastoma multiforme (GBM) brain tumor. Specifically, this session will cover how a new organoid GBM model has allowed for the capture of the characteristic phenotypic and molecular features of GBM in a dish. The presentation will also address fundamental questions of brain tumor development as well as how to test and exploit therapeutic vulnerabilities of this cancer in a way that cannot be achieved with traditional cell lines and animal models.

Lynsey Willetts, MBA, Ph.D.
: Lynsey Willetts, MBA, Ph.D.Cell Solutions Business Operations Director
Event Host

Linyu (Claire) Zhang, Ph.D.
: Linyu (Claire) Zhang, Ph.D.Application Scientist
Asia Technology Center, Shanghai
3D Cell Culture and Organoids for COVID-19 Researchers
3D cell culture techniques are emerging as versatile and biologically relevant research models to help support the current fight against COVID-19. This webinar will summarize studies on organoids that were used as experimental virology platforms to study SARS-CoV-2 infectivity and immune responses, and as tools for antiviral drug discovery and development. Recent data from Corning on the characterization of airway and alveolar organoid models for COVID-19 drug screening using the Corning® Matrigel® Matrix 3D-plate and Corning Transwell® permeable support will also be presented.
Panel Discussion: Organoids as Patient Avatars for Personalized Medicine
Organoids have become a valuable and reliable tool in pre-clinical and translational research, demonstrating their ability to be used as patient-specific avatars of disease and drug response. In this expert panel discussion of Memorial Sloan Kettering Cancer Center scientific and medical professionals, the discussion is centered around what enabled the early and current success of organoid models as well as the evolution into more complex organoid models to study specific areas of cancer and personalized drug therapies. Panelists also exchange views on organoid system advantages as well as current challenges, model validations and more.
Level Up: A Panel Discussion on 3 Dimensional Cultures in a High Throughput Environment
This expert panel discussion covers the various 3D cultures and discusses the pros and cons of various models. Ideas are also exchanged on where 3D cultures can add the most value in research and drug screening, making the move to mid and high throughput environments, successful methods and tools as well as challenges in working with these cultures. Finally they panel reviews their blue sky ideas on the future of 3D models.