FAQ Config Details
Do standard-performance UniCam® Connectors have a composite ferrule?
No. All single-fiber UniCam Connectors utilize a zirconia ceramic ferrule.
FAQ Config Details
What is the difference between a ceramic ferrule and a polymer ferrule?
Zirconia ceramic ferrules offer several distinct advantages over polymers, which is why Corning uses zirconia ceramic ferrules exclusively in single-fiber UniCam Connectors: Ceramic ferrules are chip and crack resistant; smaller grain sizes achieve smoother finishes; their thermal expansion coefficients are closer to that of the fiber; and they have a higher modulus of elasticity and greater impact resistance.
FAQ Config Details
Will our connectors work with our competitors adapters?
No, keys are proprietary to each manufacturer. Corning offers keyed LC UniCam Connectors and Adapters, as well as other keyed products , in 8 different keyed colors; blue, orange, green, red, yellow, slate, black and violet.
FAQ Config Details
Can I use the TKT-UNICAM-PFC to install APC connectors?

Customers can install APC connectors using the installation tools provided in the TKT-UNICAM-PFC kit; however, the cleaver in this kit provides flat cleaves, so a different cleaver will needed to generate an angled cleave before terminating the APC connector in the installation tool, assuming an angled cleave is desired. At room temperatures, using a flat cleave is acceptable. An angled cleave is needed when the connector is installed in environments with temperature swings (outdoor environments).​

Corning Optical Communications offers an angled cleaver, the FBC-014 that can be used with APC UniCam Connectors.