Corning Adds to its Optical Connectivity Offerings with New UniCam™ Toolkit, MTP® Connector Technologies
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
News Releases
Corporate Communications
Corning Adds to its Optical Connectivity Offerings with New UniCam™ Toolkit, MTP® Connector Technologies
Corning Adds to its Optical Connectivity Offerings with New UniCam™ Toolkit, MTP® Connector Technologies
Corning, NY | Corning Incorporated | February 02, 2018

Corning Incorporated (NYSE:GLW) today announced two new additions to its optical connectivity offering. The UniCam high-performance toolkit 2 and the MTP® PRO connector both help simplify the installation of optical connectors in the field, providing critical time savings in today’s demanding, time-sensitive deployments.

Both products will be featured in Corning’s booth (#1013) at the 2018 BICSI Winter Conference & Exhibition, Feb. 4-8 in Orlando, Florida.

The UniCam high-performance toolkit 2 demonstrates the continued evolution of Corning’s no-epoxy, no-polish connector technology, providing a reduction in the termination time of a single connector as well as improved feedback and guidance throughout the termination process. The new toolkit cuts the number of steps required for connector installation by 45 percent (from 18 steps to just 10), reducing the termination time by as much as 25 percent.

Offering improved operational feedback and guidance, the new installation tool includes an onboard LCD screen made of Corning® Gorilla® Glass. On-screen icons and animations vary and are determined by the tool automatically, based on the type of connector being terminated.  If a mistake is detected, the tool will notify the user and advise on how to correct it.

The toolkit also includes a separate 7-inch LCD panel with preloaded, step-by-step videos to guide the user through the termination process. With the elimination of several installation steps and simplified connector loading, the UniCam high-performance toolkit 2 allows installers to more quickly connectorize in the field.

Corning’s UniCam products – including connectors, tool kits, and optimized accessories – provide best-in-class optical performance in a fast, easy field-termination solution.

Corning is also adding the new MTP PRO connector to its portfolio. The MTP PRO connector offers increased flexibility in the field and minimizes the risk of delays for customers leveraging MTP-based solutions. With it, installers can easily change pinning and polarity in the field. With the use of a simple hand-held tool, polarity can be changed and pins can be added or removed, all without removing the connector housing.

Now, when pinning or polarity changes are needed, customers don’t have to order and wait for a new product to arrive. The MTP PRO connector is available for harnesses and jumpers in the EDGE, EDGE8, and Plug & Play product families. Inventory management can be simplified by stocking these jumpers in the most common configurations and using the tool to quickly add or remove pins, or change polarity as needed.

The UniCam and MTP connector solutions are the result of Corning’s core technologies in optical physics and ceramic science, and are engineered and manufactured through its vapor deposition and precision forming processes.

Forward-Looking and Cautionary Statements
This press release contains “forward-looking statements” (within the meaning of the Private Securities Litigation Reform Act of 1995), which are based on current expectations and assumptions about Corning’s financial results and business operations, that involve substantial risks and uncertainties that could cause actual results to differ materially. These risks and uncertainties include: the effect of global political, economic and business conditions; conditions in the financial and credit markets; currency fluctuations; tax rates; product demand and industry capacity; competition; reliance on a concentrated customer base; manufacturing efficiencies; cost reductions; availability of critical components and materials; new product commercialization; pricing fluctuations and changes in the mix of sales between premium and non-premium products; new plant start-up or restructuring costs; possible disruption in commercial activities due to terrorist activity, armed conflict, political or financial instability, natural disasters, adverse weather conditions, or major health concerns; adequacy of insurance; equity company activities; acquisition and divestiture activities; the level of excess or obsolete inventory; the rate of technology change; the ability to enforce patents; product and components performance issues; retention of key personnel; stock price fluctuations; and adverse litigation or regulatory developments. These and other risk factors are detailed in Corning’s filings with the Securities and Exchange Commission. Forward-looking statements speak only as of the day that they are made, and Corning undertakes no obligation to update them in light of new information or future events.

Web Disclosure
In accordance with guidance provided by the SEC regarding the use of company websites and social media channels to disclose material information, Corning Incorporated (“Corning”) wishes to notify investors, media, and other interested parties that it intends to use its website (http://www.corning.com/worldwide/en/about-us/news-events.html) to publish important information about the company, including information that may be deemed material to investors. The list of websites and social media channels that the company uses may be updated on Corning’s media and website from time to time. Corning encourages investors, media, and other interested parties to review the information Corning may publish through its website and social media channels as described above, in addition to the company’s SEC filings, press releases, conference calls, and webcasts.

About Corning Incorporated
Corning (www.corning.com) is one of the world’s leading innovators in materials science, with a 166-year track record of life-changing inventions. Corning applies its unparalleled expertise in glass science, ceramics science, and optical physics along with its deep manufacturing and engineering capabilities to develop category-defining products that transform industries and enhance people’s lives. Corning succeeds through sustained investment in RD&E, a unique combination of material and process innovation, and deep, trust-based relationships with customers who are global leaders in their industries.

Corning’s capabilities are versatile and synergistic, which allows the company to evolve to meet changing market needs, while also helping our customers capture new opportunities in dynamic industries. Today, Corning’s markets include optical communications, mobile consumer electronics, display technology, automotive, and life sciences vessels. Corning’s industry-leading products include damage-resistant cover glass for mobile devices; precision glass for advanced displays; optical fiber, wireless technologies, and connectivity solutions for state-of-the-art communications networks; trusted products to accelerate drug discovery and delivery; and clean-air technologies for cars and trucks.