Our CAH ConnectionsSM Gold Program represents the highest standard for manufacturers of optical patch cords. Member companies purchase Corning materials, adhere to recommended manufacturing processes, and pass annual audits conducted by our experts. As a result of this demonstrated manufacturing and business excellence, we offer our 25-year Extended WarrantySM Program coverage to include simplex and duplex patch cords manufactured by CAH Connections Gold Program members for projects installed by certified NPI members.
Program Overview
Program Overview
CAH Connection Gold Members
| Gold Member | Address | Phone |
|---|---|---|
| Accurate Connections, Inc | 13801 Hutton Dr. Farmers Branch, TX 75234 | 866-670-4010 |
| BS Cable | 334 Goodshall Dr. Harleysville, PA 19438 | 800-204-0628 |
| Cables Unlimited | 3 Old Dock Road Yaphank, NY 11980 | 800-590-9965 |
| C Enterprises | 2445 Cades Way Vista, CA 92081 | 800-334-3815 |
| Comnet Telecom Supply | 1 Kimberly Rd Building 101 East Brunswick, NJ 08816 | 800-603-7824 |
| CP Technologies | 17110 Armstrong Ave Irvine, CA 92614 | 800-876-8889 |
| CSC/Fibertron | Suite 120 2202 South 7th Street Phoenix, AZ 85034 | 800-745-3344 |
| Fiber Connections Inc. | 30 Aerospace Blvd Slemon Park, P.E.I. Canada C0B 2A0 | 800-353-1127 |
| Lynn Electronics LLC | 154 Railroad Drive, Ivyland, PA. 18974 | 800-523-6075 |
| Major Custom Cable | 281 Lotus Dr Jackson, MO 63755 | 800-455-6224 |
| Microlink | Enrique Palacios Street # 360, Office 407, Miraflores, Lima | +51 (1) 6162060 ext 2030 |
| NetSource | 25 West Street Bolton, CT 06043 | 800-557-8818 |
| Zero Connect | 6604 201st Street, Albia, IA 52531 | 844.zero123 or 844.937.6123 |
CAH Connections Gold Program
24 Hour Ship Program
24 Hour Ship Program
24 Hour Ship Program
Read MoreMany of our most popular cables used for patch cords are in stock and ready to ship today.
In-stock cables ship on same day if order is received and entered by noon(EST). In-stock cable orders entered after noon (EST) will be shipped the following business day. If cable is not in stock, ARO lead time is one to three business days.
Many of our most popular cables used for patch cords are in stock and ready to ship today.
In-stock cables ship on same day if order is received and entered by noon(EST). In-stock cable orders entered after noon (EST) will be shipped the following business day. If cable is not in stock, ARO lead time is one to three business days.
Cable Specifications
Cable Specifications
Learn MoreSee a list of cable specifications available for use.
See a list of cable specifications available for use.