There are 45 percent fewer termination steps, from 18 to10. This reduces the time to terminate a UniCam® connector by 25 percent with the new tool. Integrated intelligence provides step-by-step guidance throughout the termination process, as well as corrective guidance in the event that a process error occurs.
Termination guidance is provided by an integrated LCD panel that features Corning® Gorilla® Glass.
The toolkit also includes a 7-in LCD panel with preloaded, step-by-step videos to guide the user through the fiber preparation and termination process.
TKT-UNICAM-PFC2 (Kit)
TL-UCP2 (Installation Tool Only)