Can a mid-sized building have more capacity than a small city?
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
Can a mid-sized building have more capacity than a small city?

Capacity: Mid-sized building vs. small city?

A question to mobile operators: You have just acquired the rights to deploy an indoor system inside a large building and are about to deploy 50+ antennas inside the building. Now, would you like to add a full LTE cell to each antenna? That’s right… would you like a complete LTE single-sector base station where you were planning to install just an antenna? What about two LTE base stations where you were planning to install just an antenna?

Adding an LTE (or 3G) cell in the macro network is expensive, very expensive, and difficult as h*$%! So, rather than getting more cell sites, operators try to increase capacity by buying more spectrum (billions), and improving spectral efficiency (even more billions). As frequent readers of this blog know, SpiderCloud offers a way to add a massive amount of capacity indoors – using scalable small cell systems.

One of SpiderCloud’s customers recently asked our system engineering team to estimate the capacity of a SpiderCloud dual-carrier LTE system. We have a rather sophisticated modeling tool that accounts for interference between small cells and macros, generates randomized distribution of users and more. So, for this analysis, we took an 180,000 ft2 4-floor building. Based on the building’s floor plans, 24 radio nodes were sufficient to provide coverage, and this system was capable of delivering more than 2.5 Gbps of throughput, at less than 50% loading!

2.5 Gbps in an 180,000 ft2 is a lot of capacity, enough to stream HD movies to 500 Netflix subscribers simultaneously! Not surprising, since this building has 48 LTE cells, equivalent to 16 3-sector macro base stations, sufficient to cover a small city. Though the actual capacity delivered by a SpiderCloud system will depend upon the backhaul connection commissioned by the operator, adding capacity is as easy as provisioning more backhaul.

SpiderCloud’s approach is very different from big macro base stations vendors, all of whom are still looking for a way to somehow make their macro base station technology (Dots, Lamps, and everything else) applicable to indoor. Macro base station roadmaps are rightfully designed to incrementally squeeze more bps out of existing macro cell site grid, and more $$s out of operators. The whole point is to sell the operator increasingly expensive-to-deploy features like coordinated multipoint and 4×4 MIMO on existing platforms – basically, a gravy train for the big vendors, a sink-hole for their customers.

SpiderCloud’s offers a disruptive alternative – a really easy to deploy system with so much capacity on day one that our customers do not have to buy a capacity upgrade for a very, very long time.