EDGE™/EDGE8® Tap Modules | Corning

Elevate your network's potential with passive TAP modules

Elevate your network's potential with passive TAP modules

Why should you consider network monitoring?

Network monitoring is essential to ensuring the success of your network system. It can automatically detect and respond to threats and performance issues.

Let's Connect

EDGE™/EDGE8® TAP Modules Features & Benefits

 

Benefits of Passive Optical Tapping vs. Spanning
Benefit TAP SPAN
Passive TAPs are passive devices and don't require power or configuration. SPAN ports can cause network issues like bridging loops if spanning tree is not disabled on a SPAN port. Can occur during network refresh when SPAN ports are deployed as network ports.
All Access They make copies of all data in real-time with no traffic delay without burdening the live network. SPAN ports do not receive all data: for example, corrupt and improperly sized packets may not be received, in addition, SPAN data has the lowest priority.
Low-Cost TAPs are low-cost and a highly reliable way to provide data nonintrusively to network tools for multiple generations of optics. The cost of transceivers used for SPAN ports increases with every generation of optic, causing your monitoring cost to increase.
Density Since they are part of the structured cabling, TAPs allow you to retain use of ports on network switches. SPAN requires two ports on network switch when monitoring full-duplex communication between two devices (ingress and egress).
Security & Reliability TAPs are completely secure because they are not part of the network (can't be hacked). SPAN changes the timing (delays) of the frame/packet interaction and places an extra burden on the production network (replication of traffic).

Network Monitoring with TAP Modules FAQs

Read more about TAP modules by clicking on the questions below.

  • What is the difference between active and passive network monitoring?

    Active monitoring involves actively sending test traffic or queries to the network to assess its performance and identify issues. 

    Passive monitoring, on the other hand, involves observing existing network traffic without introducing additional traffic.

  • How to extract network data?

    Network layer data must first be extracted in order to apply the analysis tools. There are two commonly used methods to extract the network data so it can be analyzed:

    - SPAN ports, switch port for analysis (active) – SPAN (port mirroring) was created to replicate packets of a single port (or VLAN) for monitoring.

    - TAP (traffic access point) ports – TAP modules use passive splitting to transmit in-line traffic to an attached monitoring device without data stream interference.

  • How does a passive optical TAP work?

    TAPs work by capturing and redirecting a copy of network traffic for analysis purposes. Passive TAPs, like optical taps, do this without interfering with the original traffic flow.

  • What are the advantages of port tapping over SPAN ports (port mirroring)?

    There are five primary advantages of port tapping has – whether via Corning EDGE™ and EDGE8® Solutions or other passive devices – versus SPAN ports: 

    - Port tapping is completely passive and does not require power, switch configurations, or switch programming. This allows you to avoid network issues such as bridging loops that could occur with SPAN ports during a network refresh. 

    - Port tapping splits the signal in real time without burdening your live network while SPAN ports replicating your signal can change the timing of frame/packet interactions and create an extra burden on the production network. 

    - Port tapping components are low cost and highly reliable. You can use passive components with multiple generations of optics while SPAN ports can increase in price with every data rate protocol upgrade. 

    - Port tapping does not require an oversubscription ratio as it is part of your structured cabling while SPAN ports require two   ports (one for your live network and one for the monitoring device) for full duplex port monitoring. 

    - Port tapping passes on all traffic in the live link to the monitoring device. SPAN ports do not receive all network data, such as   corrupt data or improperly sized packets, so it may not give the full picture of how your system is performing. 

    Corning uses passive port tapping through our extensive line of EDGE and EDGE8 tap modules. 

  • More questions? Please download our complete FAQ document

Tools & Resources

Need help deploying TAP modules in your network?

Whether you need help with your current implementation or planning for the future, we can help. Complete this form to get started.

Thank You!

A Corning representative will be contacting you shortly about your inquiry. Should you need immediate assistance please call our customer service line at +49 30 5303 2100.