One of the most important factors when it comes to looking for an MTDC is locality. Your business should be close to your facility, because reducing latency and increasing bandwidth are two of the biggest challenges associated with outsourcing. For example, if businesses colocate within MTDCs in another city or state, connection speeds may drop and can negatively impact on the output of IT applications.
From an infrastructure perspective, scalability is key. Scalability within the data center will support simple migration to higher data rate connections and applications—a vital factor for meeting future bandwidth and transmission speeds that the IT applications require. As data continues to generate and technological advancements continue to increase, the need for your organization to meet customer demands for zero latency and real-time access to data will as well.
An MTDC facility also provides a variety of cloud service provider and telecommunication carrier options. For example, if your organization delivers cloud services that require high speeds, you can look to outsource just that part of your business. Alternatively, if you solely need storage, then another MTDC facility might better suit your needs. As most businesses have a range of needs that more than one facility can address, it is important not to restrict your business to choosing one facility when the best solution might involve multiple.
Finally, network and physical security are important factors in choosing an MTDC facility. If your network is colocated, you will want to be certain it is protected from inappropriate access. For example, facilities with layered security zones would only allow authorized personnel to access certain network areas and physical barriers, like fencing and locks. You’ll also want an operator that has monitoring systems—such as CCTV or other systems that detect emergencies like fires or flooding. Background on security and monitoring will provide insight into how the MTDC facility will protect your data and support client security. Knowing the importance of these factors, it is common for MTDCs to address security as a business imperative.
You should also consider additional services when choosing an MTDC facility. In addition to the typical space, power, and connectivity services, many MTDC providers offer an extensive range of consultative services to ensure the organization complies with mandatory regulations and/or other industry requirements. Even when the customer is educated on and aware of these requirements, the MTDC provider may have dedicated teams of regional, national, and international regulatory compliance personnel whose sole aim is to keep abreast of the latest developments.
For business operators both big and small, running an IT network that processes massive amounts of data is no easy task. Migrating computing needs to an MTDC takes the pain out of data management and reduces operational expenditure. A future-ready MTDC should offer scalability, flexibility, modularity, and stringent SLAs to assure maximum uptime, client peace of mind, and rapid deployments to high-density applications when you need it—fast.
*As stated in this article.