PPG Receives EPA Registration for COPPER ARMOR™ Paint Powered by Corning® Guardiant®

康宁的重要合作伙伴PPG近日宣布,其采用Corning Guardiant™康宁抗微生物铜离子技术的PPG Copper Armor™涂料已成功获得美国国家环境保护局 (EPA) 的产品注册认证3,这是美国首款通过EPA认证的含有Corning Guardiant的涂料产品1,标志着该技术在商业可用性方面又迈进一步。

日常生活中使用的传统消毒剂,在挥发后即无法继续保持杀灭病菌的作用。对于高频接触的表面,中国疾控中心则建议每日至少进行一次消毒清洁7。然而,对于墙壁这类通常不会每天进行清洁消毒的表面,抗微生物功效的长效性至关重要。Corning Guardiant为表面增添了额外一层防护,能够持续地杀灭涂层表面的特定细菌和病毒。

“早在几年前,当我们认识到铜能为表面病菌防护带来切实有效的帮助时,康宁的科学家们已开始着手研发Corning Guardiant这项产品,”特殊表面事业部副总裁兼项目总监Joydeep Lahiri表示。“如今,我们很高兴可以和PPG合作,见证这款Copper Armor新产品的推出,并将抗微生物涂层技术推广至公众,为消费者带来更安心的使用体验。”

根据美国国家环境保护局 (EPA) 的规定,在美国声称具有广谱抗病菌功效的产品,需要先通过一种能模拟现实污染环境的测试方法——干燥测试法4,这也是Copper Armor涂料在上市前所采用并通过的测试方法。通过Corning Guardiant的赋能,PPG Copper Armor涂料能在两小时内杀灭涂层表面多种特定的细菌和病毒,且在模拟测试中其功效能持续长达五年6为墙面、内饰和门提供持续保护,防止有害微生物的滋生。该款涂料有eggshell (蛋壳光),satin (哑光),semi-gloss (半光) 三种光泽效果,以及PPG涂料调色板中超过600多种颜色可供选择。在获得EPA认证后,该产品将在2021年底登陆美国的PPG PAINTS™商店、独立零售店和其他家居用品商店。

康宁执行副总裁兼创新官Marty Curran表示:“康宁一直乐于在新兴创新领域研发改善生活方式的新产品,Corning Guardiant的诞生展现了康宁致力于为客户和消费者解决棘手难题的不断承诺。创新需要极大的耐心,而Corning Guardiant团队能在一个崭新的领域持续开拓创新,这令我们感到激动和自豪。”

Corning Guardiant技术近期还收获了几项行业认可,包括入选2021年国际最佳商业奖 (Best in Biz Awards 2021 International) 年度最佳创新产品榜单,并荣获健康医疗类5金奖,以及今年早期在2021年爱迪生奖上获得金奖。同时,该项目也入围了R&D 100创新奖中机械与材料类的候选名单。

在中国,Corning Guardiant也积极与立邦和嘉宝莉品牌展开合作,并实现了该产品的商业化,我们将不断致力于为中国消费者带来更多的抗微生物涂料产品。

 

注释:

1. 基于美国国家环境保护局批准的营销声明(注册号:56601-4),Corning Guardiant™是美国首款用于建筑涂料的铜基抗微生物添加剂。https://www.epa.gov/pesticides/chem_search/ppls/056601-00004-20211014.pdf

2. 在包括亚利桑那大学在内的第三方实验室测试结果表明,Corning Guardiant能杀灭涂层表面99.9%的特定有害病菌,包括诺如病毒、5型腺病毒、金黄色葡萄球菌、绿脓杆菌、耐甲氧西林金黄色葡萄球菌、冠状病毒229E、甲型H1N1流感病毒等,且(在实验室模拟环境下)功效能维持六年。

3. 美国国家环境保护局注册号:56601-4;注册日期:10/4/21;注册产品名:Copper Armor

4. https://www.epa.gov/pesticide-registration/interim-guidance-review-products-adding-residual-efficacy-claims

5. “健康医疗类”仅为国际最佳商业奖的奖项设置类别,Corning Guardiant 未在中国注册为医疗健康类产品。

6. https://www.ppgpaints.com/copper-armor-paint

7. 中国疾控动态.《手把手教您做好消毒》 https://mp.weixin.qq.com/s/_N12E362oCuGMeNKQ99aZA   

免责声明:声称对人体有害病原体具有抗微生物功效的产品可能需要获得有关政府部门的认证。康宁不认可或承担任何掺有Corning Guardiant的产品均符合适当的法规要求和/或认证。

The Copper Armor product’s efficacy was measured using tests that simulate real-world contamination that are mandated by the EPA for products making claims against a broad spectrum of harmful pathogens. PPG’s Copper Armor paint with Corning Guardiant technology continuously kills viruses and bacteria within two hours of contact with the painted surface for up to five years, providing a safeguard against harmful microbes on walls, trim, and doors. 

“Corning doesn’t shy away from working in new areas to develop life-changing innovations, and this program is a great example of Corning’s continued commitment to solving tough customer challenges,” said Marty Curran, executive vice president and innovation officer. “Innovation takes a lot of patience, and the Guardiant team’s drive to continue to push this innovation in a space that’s fairly new to the company is very exciting.”

Guardiant technology has also received some recent industry recognitions including a gold Best in Biz International Award for Most Innovative Product of the Year in the healthcare and medical category and a gold win at the 2021 Edison Awards earlier this year. The program is also a finalist for the R&D World’s annual R&D 100 Awards in the Mechanical/Materials category.