Corning Introduces Lab Reactor System at Annual Reactor Technology Conference

Corning Introduces Lab Reactor System at Annual Reactor Technology Conference

Corning Introduces Lab Reactor System

News Releases
企业通信
Corning Introduces Lab Reactor System at Annual Reactor Technology Conference
Corning Introduces Lab Reactor System at Annual Reactor Technology Conference
CORNING, N.Y. | Corning Incorporated | 2017年3月6日

Corning Incorporated (NYSE: GLW) today introduced the Corning Lab Reactor system as the newest product available in its Advanced Flow™ reactor (AFR) portfolio at the seventh Corning Reactor Technology Annual Conference in Changzhou, China, today through March 7.

The Lab Reactor is metal-free in all process fluid paths with a patented “heart-cell” channel design enabling high-chemical durability and outstanding mixing and heat exchange. The reactor’s fluidic module is made of Corning specialty glass, providing a transparent window for chemists to see what’s happening inside. In addition, its “plug and play” open system includes data monitoring and storage, and easily connects with process analytical technology (PAT).

“The Lab Reactor is a great solution for our customers in academia and research institutes,” said Dr. Yi Jiang, business director, Corning AFR Technologies. “It has a low internal volume, but with similar mixing and heat-transfer characteristics that enable a seamless scale-up with other AFR products such as the G1 reactor for lab and small production, and the G4 reactor for dedicated production. The reactor installs quickly and easily, and is ready to operate within a few minutes, helping researchers conduct their work in a more efficient manner.”

The Lab Reactor system has a photo reactor option that offers efficient light penetration with illumination on both sides of the glass fluidic module. The photo reactor also features a tunable LED irradiation source with six different wavelengths – with the LED lighting intensity higher than 100 mW/cm2. The option also enables wireless control of wavelength selection and intensity.

“We designed an LED lighting source with a cooling mechanism that enables increased temperature accuracy during the photoreaction process,” said Olivier Lobet, global product engineer, Corning Reactor Technologies. “The extended photo-flow reactor option also helps expand the horizon of the chemistry with consistent control within the operating system.”

Corning announced this new system during the Reactor Technology Annual Conference with approximately 500 attendees from academia as well as the pharmaceutical, fine, and specialty chemical processing industries.

“Flow-chemistry education is one of the big themes for us during this year’s conference,” Yi said. “And it’s exciting that we have a new, integrated, user-friendly lab system to help many students step into the flow-chemistry arena. Flow chemistry is not yet part of a course curriculum or training for chemists and chemical engineers in most universities and institutes, but we think it will be a valuable tool for their future careers.”

Customers can now place orders for the new Lab Reactor systems through Corning’s regional sales channels. The systems are manufactured at Corning’s S.A.S. facility in France with quality after-sale services delivered by Corning’s regional technical and commercial teams around the world.

Corning’s AFR technology enables the continuous processing of chemicals with a smaller footprint than conventional batch reactors. They are also specially designed to enable the conversion of batch chemical processes to continuous processes. Corning’s reactors provide customers with cost-effective solutions, specialized engineering support, and process expertise.

Compared with traditional batch reactors, Corning’s reactors can enable at least 100 times enhancement in mixing, 1,000 times improvement in heat transfer performance, and seamless, efficient scale-up from the lab to full-scale production of chemicals for the pharmaceutical, specialty, and fine chemical industries.

Forward-Looking and Cautionary Statements

This press release contains “forward-looking statements” (within the meaning of the Private Securities Litigation Reform Act of 1995), which are based on current expectations and assumptions about Corning’s financial results and business operations, that involve substantial risks and uncertainties that could cause actual results to differ materially. These risks and uncertainties include: the effect of global political, economic and business conditions; conditions in the financial and credit markets; currency fluctuations; tax rates; product demand and industry capacity; competition; reliance on a concentrated customer base; manufacturing efficiencies; cost reductions; availability of critical components and materials; new product commercialization; pricing fluctuations and changes in the mix of sales between premium and non-premium products; new plant start-up or restructuring costs; possible disruption in commercial activities due to terrorist activity, armed conflict, political or financial instability, natural disasters, adverse weather conditions, or major health concerns; adequacy of insurance; equity company activities; acquisition and divestiture activities; the level of excess or obsolete inventory; the rate of technology change; the ability to enforce patents; product and components performance issues; retention of key personnel; stock price fluctuations; and adverse litigation or regulatory developments. These and other risk factors are detailed in Corning’s filings with the Securities and Exchange Commission. Forward-looking statements speak only as of the day that they are made, and Corning undertakes no obligation to update them in light of new information or future events.

Digital Media Disclosure

In accordance with guidance provided by the SEC regarding the use of company websites and social media channels to disclose material information, Corning Incorporated (“Corning”) wishes to notify investors, media, and other interested parties that it intends to use its website (http://www.corning.com/worldwide/en/about-us/news-events.html) to publish important information about the company, including information that may be deemed material to investors. The list of websites and social media channels that the company uses may be updated on Corning’s media and website from time to time. Corning encourages investors, media, and other interested parties to review the information Corning may publish through its website and social media channels as described above, in addition to the company’s SEC filings, press releases, conference calls, and webcasts.

About Corning Incorporated

Corning (www.corning.com) is one of the world’s leading innovators in materials science. For more than 160 years, Corning has applied its unparalleled expertise in specialty glass, ceramics, and optical physics to develop products that have created new industries and transformed people’s lives. Corning succeeds through sustained investment in R&D, a unique combination of material and process innovation, and close collaboration with customers to solve tough technology challenges. Corning’s businesses and markets are constantly evolving. Today, Corning’s products enable diverse industries such as consumer electronics, telecommunications, transportation, and life sciences. They include damage-resistant cover glass for smartphones and tablets; precision glass for advanced displays; optical fiber, wireless technologies, and connectivity solutions for high-speed communications networks; trusted products that accelerate drug discovery and manufacturing; and emissions-control products for cars, trucks, and off-road vehicles.