Corning ONE™ Wireless Platform Enables Best-in-Class Fan Experience at Texas A&M Kyle Field Stadium

Corning ONE™ Wireless Platform Enables Best-in-Class Fan Experience at Texas A&M Kyle Field Stadium

Corning ONE Wireless Platform at Texas A&M Stadium

News Releases
Optical Communications
Corning ONE™ Wireless Platform Enables Best-in-Class Fan Experience at Texas A&M Kyle Field Stadium
Corning ONE™ Wireless Platform Enables Best-in-Class Fan Experience at Texas A&M Kyle Field Stadium
CORNING, N.Y. | Corning Incorporated | 2015年10月20日

Corning Incorporated (NYSE:GLW) today announced the deployment of its ONE Wireless platform at Texas A&M University’s Kyle Field.

One of the largest college football stadiums in the U.S., the newly renovated home of the Texas A&M Aggies, now includes a state-of-the art optical fiber infrastructure that delivers increased capacity and more reliable wireless service. ONE Wireless enables more than 100,000 fans to call, text, and tweet about being at the big game – all at the same time.

“Texas A&M Chancellor John Sharp empowered us to build a state-of-the-art facility - one that would rival or surpass NFL stadiums as well as enhance upon Kyle Field’s already legendary game-day fan experience, truly the best in all of collegiate sports,” said Phillip Ray, vice chancellor of Business Affairs for the Texas A&M University System. “He wanted iconic Kyle Field to have the most-connected fans anywhere in the country, and we are confident that the Corning ONE Wireless platform will deliver just that.”

The IBM-designed network includes Corning’s ONE Wireless Platform, the first all-optical solution to converge nearly every wired and wireless connectivity need into a single, unified infrastructure.

“IBM’s collaboration with Corning went beyond the typical manufacturer-integrator relationship,” said Sam Maatallah, vice president, Networking Services, Infrastructure Services – North America, IBM. “Their commitment to innovation, coupled with the inherent flexibility of the ONE platform, enabled a network design that allows customers to engage the full complement of IBM resources. Together, we functioned as one team, working to deliver the ultimate connected fan experience in a world-class football stadium.”

ONE Wireless used half the space of, required significantly less material than, and will use less power than legacy copper-based networks or hybrid-fiber coax DAS solutions – while delivering near record-setting Wi-Fi network performance. When Kyle Field opened for Texas A&M’s 2015 football season on Sept. 12, happy fans took to social media to praise their best-in-class connectivity – with one user proudly tweeting his network speed test results.

“Today, the Aggies are among the most connected fans anywhere, with a DAS network capable of delivering coverage for all four leading service providers, and a Wi-Fi network capable of handling a 100,000 photos uploaded to social media every second,” said Mike O’Day, vice president of Wireless Networks for Corning Optical Communications. “Plus, the ONE platform enables multiple point-of-sales systems, a network of IPTVs, and it stands ready to tackle anything else Texas A&M adds in the future.”

For a more technical look at Kyle Field’s new network, please contact Todd Christner, ChristneRT@corning.com at Corning.

Forward-Looking and Cautionary Statements

This press release contains “forward-looking statements” (within the meaning of the Private Securities Litigation Reform Act of 1995), which are based on current expectations and assumptions about Corning’s financial results and business operations, that involve substantial risks and uncertainties that could cause actual results to differ materially. These risks and uncertainties include: the effect of global political, economic and business conditions; conditions in the financial and credit markets; currency fluctuations; tax rates; product demand and industry capacity; competition; reliance on a concentrated customer base; manufacturing efficiencies; cost reductions; availability of critical components and materials; new product commercialization; pricing fluctuations and changes in the mix of sales between premium and non-premium products; new plant start-up or restructuring costs; possible disruption in commercial activities due to terrorist activity, armed conflict, political or financial instability, natural disasters, adverse weather conditions, or major health concerns; adequacy of insurance; equity company activities; acquisition and divestiture activities; the level of excess or obsolete inventory; the rate of technology change; the ability to enforce patents; product and components performance issues; retention of key personnel; stock price fluctuations; and adverse litigation or regulatory developments. These and other risk factors are detailed in Corning’s filings with the Securities and Exchange Commission. Forward-looking statements speak only as of the day that they are made, and Corning undertakes no obligation to update them in light of new information or future events.

About Corning Incorporated

Corning (www.corning.com) is one of the world’s leading innovators in materials science. For more than 160 years, Corning has applied its unparalleled expertise in specialty glass, ceramics, and optical physics to develop products that have created new industries and transformed people’s lives. Corning succeeds through sustained investment in R&D, a unique combination of material and process innovation, and close collaboration with customers to solve tough technology challenges. Corning’s businesses and markets are constantly evolving. Today, Corning’s products enable diverse industries such as consumer electronics, telecommunications, transportation, and life sciences. They include damage-resistant cover glass for smartphones and tablets; precision glass for advanced displays; optical fiber, wireless technologies, and connectivity solutions for high-speed communications networks; trusted products that accelerate drug discovery and manufacturing; and emissions-control products for cars, trucks, and off-road vehicles.