LEAF® Optical Fiber | Long-haul and Metro Network Solution | Corning
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
LEAF® Optical Fiber

LEAF® Optical Fiber

LEAF® Optical Fiber

World’s most widely-deployed non-zero dispersion-shifted fiber

LEAF® Optical Fiber

LEAF® Optical Fiber

LEAF® optical fiber has become the go-to solution for long-haul and metro networks. In the race to satisfy the global demand for bandwidth, LEAF fiber is the clear winner as the world's most widely deployed non-zero dispersion-shifted fiber (NZDSF).

Additionally, LEAF fiber is the industry leader in polarization mode dispersion (PMD) specifications and has the lowest attenuation of any NZDSF on the market.

Built to withstand decades of demands in challenging environments, LEAF fiber can be used in multiple network architectures and can help existing networks evolve from 10G to the 40G and 100G systems of the future.

Additional Resources

Additional Resources

In The News

In The News

100G Direct Detection Across Record Distance Achieved

In partnership with ADVA Optical Networking, ADVA 100G Metro solution has been used to successfully transport data over 600km of Corning® LEAF® optical fiber. The demonstration represents the first time that direct-detection 100G technology has been used outside of the metro environment and positions it as a genuine 100G solution for regional networks.

Read More

Next-Generation Network To Be Deployed in South Africa

FibreCo Telecommunications, a South African open-access network provider, will deploy Corning® optical fiber in its new ultra-high-speed, long-distance fiber optic network in South Africa.

Read More

Increased 100G Efficiency for Metro Networks To Be Showcased

ADVA Optical Networking and Corning will demonstrate a 100G solution for the metro environment at the Optical Fiber Communication/National Fiber Optic Engineers Conference in Los Angeles. This demonstration will profile the lowest cost-per-bit 100G transmission available over a distance of 125 km without inline amplification or passive dispersion compensation.

Read More

Corning’s LEAF® Optical Fiber Now Available with New Lower-Loss Specification

Corning® LEAF® optical fiber, the world’s first large-effective-area, non-zero dispersion-shifted fiber (NZ-DSF) is now further optimized for long-haul networks by applying Corning’s low-loss technology. Already the lowest-loss NZ-DSF fiber on the market, Corning low-loss technology reduces LEAF fiber’s attenuation specification to 0.19dB/km at 1550nm.

Read More