Corning Offers New Multipurpose High-Precision Laser Processing Tool
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
Corning Offers New Multipurpose High-Precision Laser Processing Tool

Corning Offers New Multipurpose High-Precision Laser Processing Tool

Corning Offers New Laser Processing Tool

News Releases
Advanced Optics
Corning Offers New Multipurpose High-Precision Laser Processing Tool
Corning Offers New Multipurpose High-Precision Laser Processing Tool
CORNING, N.Y. | CORNING INCORPORATED | December 20, 2016
New CLT 45G NX laser system for high-volume manufacturing and R&D

Corning Incorporated (NYSE: GLW) today announced the commercial availability of a new high-precision laser processing tool ideal for research and development and high-volume manufacturing. The Corning® 45G NX laser system is specifically designed for cutting and drilling strengthened and nonstrengthened glass and other crystalline materials, as well as processing micro materials such as OLED, polyimide, wafers, ceramics, and plastics.

To ensure the highest precision, the machine base and vertical structure are made from solid granite blocks. An advanced X-Y-split axis design with linear motors and sophisticated CNC control allow the processing head to move with a maximum speed of 1,000 mm/s and an acceleration of up to 10 m/s2. With optional automatic loading and unloading units, the system is ideally suited for high-volume production applications.

The CLT 45G NX has an axis-repeatability accuracy of better than 2 microns for demanding micro machining. To process a wide array of different materials quickly and efficiently, the system can be equipped with up to three different laser sources, each feeding individual processing heads. This flexibility is ideal for research and development applications as well as for volume manufacturing needs.

“Corning Laser Technologies laser glass cutting systems enable a high-quality output and yield as a result of low-surface roughness of the processed material, increased cut-bend strength of the processed material, and a high-system throughput,” said Michael Mueller, business director, Corning Laser Technologies. “Our latest system innovation brings further flexibility and efficiencies to our global customers."

Forward-Looking and Cautionary Statements
This press release contains “forward-looking statements” (within the meaning of the Private Securities Litigation Reform Act of 1995), which are based on current expectations and assumptions about Corning’s financial results and business operations, that involve substantial risks and uncertainties that could cause actual results to differ materially. These risks and uncertainties include: the effect of global political, economic and business conditions; conditions in the financial and credit markets; currency fluctuations; tax rates; product demand and industry capacity; competition; reliance on a concentrated customer base; manufacturing efficiencies; cost reductions; availability of critical components and materials; new product commercialization; pricing fluctuations and changes in the mix of sales between premium and non-premium products; new plant start-up or restructuring costs; possible disruption in commercial activities due to terrorist activity, armed conflict, political or financial instability, natural disasters, adverse weather conditions, or major health concerns; adequacy of insurance; equity company activities; acquisition and divestiture activities; the level of excess or obsolete inventory; the rate of technology change; the ability to enforce patents; product and components performance issues; retention of key personnel; stock price fluctuations; and adverse litigation or regulatory developments. These and other risk factors are detailed in Corning’s filings with the Securities and Exchange Commission. Forward-looking statements speak only as of the day that they are made, and Corning undertakes no obligation to update them in light of new information or future events.

Digital Media Disclosure
In accordance with guidance provided by the SEC regarding the use of company websites and social media channels to disclose material information, Corning Incorporated (“Corning”) wishes to notify investors, media, and other interested parties that it intends to use its website (http://www.corning.com/worldwide/en/about-us/news-events.html) to publish important information about the company, including information that may be deemed material to investors. The list of websites and social media channels that the company uses may be updated on Corning’s media and website from time to time. Corning encourages investors, media, and other interested parties to review the information Corning may publish through its website and social media channels as described above, in addition to the company’s SEC filings, press releases, conference calls, and webcasts.

About Corning Incorporated
Corning (www.corning.com) is one of the world’s leading innovators in materials science. For more than 160 years, Corning has applied its unparalleled expertise in specialty glass, ceramics, and optical physics to develop products that have created new industries and transformed people’s lives. Corning succeeds through sustained investment in R&D, a unique combination of material and process innovation, and close collaboration with customers to solve tough technology challenges. Corning’s businesses and markets are constantly evolving. Today, Corning’s products enable diverse industries such as consumer electronics, telecommunications, transportation, and life sciences. They include damage-resistant cover glass for smartphones and tablets; precision glass for advanced displays; optical fiber, wireless technologies, and connectivity solutions for high-speed communications networks; trusted products that accelerate drug discovery and manufacturing; and emissions-control products for cars, trucks, and off-road vehicles.