65 Tb/s Transoceanic Transmission Using Probabilistically-Shaped PDM-64QAM
G.654.E optical fibers for high-data-rate terrestrial transmission systems with long reach
By John D. Downie et al. in Proceedings of SPIE, vol. 10561, no. 105610, pp. 1-11, April 12, 2018. © 2018 SPIE. (SPIE’s official online version)
Maximum Capacities in Submarine Cables With Fixed Power Constraints for C-Band, C+L-Band, and Multicore Fiber Systems
© 2018 IEEE. Personal use of this material is permitted. Permission from IEEE must be obtained for all other uses, in any current or future media, including reprinting/republishing this material for advertising or promotional purposes, creating new collective works, for resale or redistribution to servers or lists, or reuse of any copyrighted component of this work in other works. (Digital Object Identifier 10.1109/JLT.2018.2858194)
Maximum Submarine Cable Capacity Analysis with C-Band, C+L-Band, and Multicore Fiber C-Band
Probabilistically shaped PDM 4096-QAM transmission over up to 200 km of fiber using standard intradyne detection
© 2018 Optical Society of America. Users may use, reuse, and build upon the article, or use the article for text or data mining, so long as such uses are for non-commercial purposes and appropriate attribution is maintained. All other rights are reserved. https://doi.org/10.1364/OE.26.004522
100 Gb/s wavelength division multiplexing four-level pulse amplitude modulated transmission over 160 km using advanced optical fibres
This paper is a postprint of a paper submitted to and accepted for publication in Electronics Letters and is subject to Institution of Engineering and Technology Copyright. The copy of record is available at the IET Digital Library.
The advantages of using reduced coating diameter optical fibers (200 µm) in ADSS cables for deployment
This paper has been presented at the IWCS 2017 Orlando International Cable & Connectivity Symposium, October 8 – 11, 2017 (www.iwcs.org)
Evaluating 200G/400G Solutions for Practical Deployments in Long-haul Network
By Y. Ma et al. in ELECTRONICS LETTERS, vol. 52, no. 19, pp. 1624-1625, September 15, 2016. © The Institution of Engineering and Technology 2016. DOI: 10.1049/el.2016.2221. Reproduced by permission of the Institution of Engineering & Technology.
Optical Fibers for Flexible Networks
By J. Downie et al., Journal of Optical Communications and Networking, vol. 8, no. 7, pp. A1-A11, May 25, 2016. Journal © 2016 Optical Society of America. http://dx.doi.org/10.1364/JOCN.8.0000A1
Amplification Schemes and Multi-Channel DBP for Unrepeatered Transmission
By L. Galdino et al. in Journal of Lightwave Technology, vol. 34, no. 9, pp. 2221-2227, May 1, 2016. © 2016 IEEE. doi: 10.1109/JLT.2016.2521002
Ultra-low Loss Fiber and Advanced Raman Amplification Deliver Record Unrepeated 100G Transmission
By D. Chang et al. in Emerging Subsea Networks, pp. 1-6, 2016. © SubOptic2016
100G unrepeatered transmission over 626.8 km with a span loss in excess of 100 dB
By D. Chang et al.
Impact of Adaptive-Rate Transponders and Fiber Attributes on the Achievable Capacity
By S. Makovejs et al. in Journal of Optical Communications and Networking, vol. 7, no. 3, pp. 172-175, March 3, 2015. © 2015 Optical Society of America. http://dx.doi.org/10.1364/JOCN.7.000172
Record 500 km unrepeatered 1 Tbits/s (10x100G) transmission over an ultra-low loss fiber
By V. Gainov et al. in Optics Express, vol. 22, no. 19, pp. 22308-22313, September 22, 2014. © 2014 OSA. doi: 10.1364/OE.22.022308
Towards Superior Transmission Performance in Submarine Systems: Leveraging UltraLow Attenuation and Large Effective Area
By S. Makovejs et al. in Journal of Lightwave Technology, vol. 34, no. 1, pp. 114-120, January 1, 2016. © 2015 IEEE. doi: 10.1109/JLT.2015.2492821
Reduction of Splice Loss Between Fibers With Dissimilar Effective Areas
By S. Makovejs et al. in Emerging Subsea Networks, pp. 1-7, 2016. © SubOptic2016