Increased connectivity and mobility requirements have driven significant network changes creating management, visibility, performance, and security challenges.
Future Network Needs
Networks Are Evolving
Networks Are Evolving
Learn MoreIncreased connectivity and mobility requirements have driven a layered/parallel network growth creating management, visibility, performance, and security challenges in the horizontal network/edge network.
Consider a fiber optic infrastructure that delivers assured and secure bandwidth and has the capabilities to support cloud-based application access, and more device connectivity than planned.
Increased connectivity and mobility requirements have driven a layered/parallel network growth creating management, visibility, performance, and security challenges in the horizontal network/edge network.
Consider a fiber optic infrastructure that delivers assured and secure bandwidth and has the capabilities to support cloud-based application access, and more device connectivity than planned.
The Rule of Three
Three Key Requirements for Any Future Network
Secure and Dedicated Bandwidth
Secure and Dedicated Bandwidth
Increased connectivity and mobility requirements have driven a layered/parallel network growth creating management, visibility, performance, and security challenges. Consider infrastructure that delivers assured and secure bandwidth for enterprise-critical applications, and has the capabilities to support cloud-based application access, and more device connectivity than planned.
Increased connectivity and mobility requirements have driven a layered/parallel network growth creating management, visibility, performance, and security challenges. Consider infrastructure that delivers assured and secure bandwidth for enterprise-critical applications, and has the capabilities to support cloud-based application access, and more device connectivity than planned.
Future-Ready Infrastructure
Future-Ready Infrastructure
A future-ready network is one that can address adds and changes relatively seamlessly and without the need to disturb the enterprise to add media for delivery. In order to ensure a future-ready network, careful consideration needs to be made on your cable plant, active network elements, and overall network design. Specifically, active electronics with modular service support, network design that allows easily reconfigured or added Ethernet drops, and a media that supports assured, secure, and virtually unlimited bandwidth are all requirements for a future-ready network.
A future-ready network is one that can address adds and changes relatively seamlessly and without the need to disturb the enterprise to add media for delivery. In order to ensure a future-ready network, careful consideration needs to be made on your cable plant, active network elements, and overall network design. Specifically, active electronics with modular service support, network design that allows easily reconfigured or added Ethernet drops, and a media that supports assured, secure, and virtually unlimited bandwidth are all requirements for a future-ready network.
Cost-Effective Deployment and Management
Cost-Effective Deployment and Management
Your network infrastructure should be built to last… similar to the expectations of your base building infrastructure. Additionally, your network infrastructure should be able to scale to address new users, applications, protocols, and services easily without the need to run more cable. Careful selection, provisioning, design, and planning will ensure a cost-effective and easily managed network.
Your network infrastructure should be built to last… similar to the expectations of your base building infrastructure. Additionally, your network infrastructure should be able to scale to address new users, applications, protocols, and services easily without the need to run more cable. Careful selection, provisioning, design, and planning will ensure a cost-effective and easily managed network.
What the WAN Means for Your LAN
What the WAN Means for Your LAN
How the Evolution of the Wide Area Network Is Changing Local Area Network Infrastructure Requirements
In the early to mid-2000s, the traditional software model began to move to software-as-a-service (SaaS) and cloud-based delivery, which began to shift local IT thinking in how they support end users. As storage and application left local servers and began to be hosted in data centers, less equipment and on-premise device management was needed, but more emphasis was needed on ISP service delivery and infrastructure ability to handle the speed and payload needed for applications to be supported.
That trend has continued, virtually eliminating the software-in-a-box delivery to an entirely cloud-hosted model. This change in local delivery to data center-hosted and delivered service, coupled with mobile device proliferation and rich media content consumption, drove data center expansion and the need to architect the data center for faster delivery moving from 10Gbps to now 40 and 100Gbps.
As the core network infrastructure changes so too must the local area network, if end users and the overall enterprise are to receive safe, reliable, and high-quality service for all their application needs. To receive the benefits of the evolution, data centers moving to 40 and 100Gbps require a fiber-rich environment in the LAN as well. Whether you are a hospital that requires assured and secure bandwidth for your ER telemetry system or an enterprise that is conducting live HD video conferencing between its remote product management and development teams – latency, capacity limitations, and an inability to ensure dedicated bandwidth at a port are serious considerations in designing and building your network infrastructure.
Fiber vs. Copper
Copper Unshielded Twisted-Pair at 10G and Beyond
Copper Unshielded Twisted-Pair at 10G and Beyond
Learn MoreIf you plan to deploy or migrate your network to 10G – and in your horizontal network, you’ll want to start thinking about it – don't let those bulky copper cables fool you. Complex to design with and to install, they create more issues than they resolve at 10G and beyond. The real facts are: unshielded copper twisted-pair at higher data rates, including 10G, is overcomplicated, overweight, overheated, and overcapacity.
If you plan to deploy or migrate your network to 10G – and in your horizontal network, you’ll want to start thinking about it – don't let those bulky copper cables fool you. Complex to design with and to install, they create more issues than they resolve at 10G and beyond. The real facts are: unshielded copper twisted-pair at higher data rates, including 10G, is overcomplicated, overweight, overheated, and overcapacity.
There’s Simply No Comparison
There’s Simply No Comparison
Optical Fiber | Copper Cable | |
---|---|---|
Capex Cost (2,000 user optical LAN) | < $300,000 | >$1,000,000 |
Lifecycle | 30 - 50 years | 5 years |
Distance | 12 Miles | 300 feet |
Weight (per 1,000 ft.) | 4 lbs. | 39 lbs. |
Energy Consumed | 2 watts per user | More than 10 watts per user |
Max. Bandwidth | 69 Tbps | 10 Gbps |
Security | Hard to tap, easy to alarm | Emits EMI |
Project Spotlight
Project Spotlight
Corning ONE™ Wireless Platform Enables Best-in-Class Fan Experience at Texas A&M Kyle Field Stadium
One of the largest college football stadiums in the U.S., the newly renovated home of the Texas A&M Aggies, now includes a state-of-the art optical fiber infrastructure that delivers increased capacity and more reliable wireless service. ONE Wireless enables more than 100,000 fans to call, text, and tweet about being at the big game – all at the same time.
Read Mobile Sports Report Article (11/9/15) >
Trade Shows and Events
Trade Shows and Events
Learn MoreWe present and exhibit at trade shows and exhibitions on fiber optic technology, issues, and trends. Come see where we’ll be and how to find us.
We present and exhibit at trade shows and exhibitions on fiber optic technology, issues, and trends. Come see where we’ll be and how to find us.
SEE the LIGHT® Training Seminars
Training Programs
Learn MoreWhether you are new to the industry, a veteran installer, a network manager, or a designer, See the Light® seminars offer something for everyone. Our curriculum includes hands-on training, intensive instructional courses, and webinars.
Whether you are new to the industry, a veteran installer, a network manager, or a designer, See the Light® seminars offer something for everyone. Our curriculum includes hands-on training, intensive instructional courses, and webinars.
Request a Sales Demo
Request a Sales Demo
Contact UsWe can send one of our trained sales engineers to your location to give a demonstration of the solutions you’re interested in and answer any questions you might have about Corning and our technology.
We can send one of our trained sales engineers to your location to give a demonstration of the solutions you’re interested in and answer any questions you might have about Corning and our technology.
Stay connected!
Stay connected!
Sign-up NowSign up to receive the latest Corning information at our Communications Preference Center.
Sign up to receive the latest Corning information at our Communications Preference Center.
Explore Communication Networks Resources
Interactive Schematic
Interactive Schematic
See our products in action with the interactive schematic
See our products in action with the interactive schematic
Read MoreInstallation Videos
Installation Videos
Browse our list of Product Installation Videos and learn from the experts.
Browse our list of Product Installation Videos and learn from the experts.
Learn MoreOptical Fiber 101
Optical Fiber 101
Corning is committed to providing education and technical support to ensure the basics of optical fiber, its composition, and its capabilities are understood.
Corning is committed to providing education and technical support to ensure the basics of optical fiber, its composition, and its capabilities are understood.
Learn MoreView Product Catalog
View Our Product Catalog
View our various products offerings in our online catalog.
View our various products offerings in our online catalog.
Learn More