-
Composite
A product made by combining different materials. The purpose is to obtain a final product comprising a range of qualities and properties superior to those found in each material taken individually:
- organic materials: light weight,
- mineral glasses: photochromism and scratch resistance.
-
Composition
In glass manufacture, composition denotes the specified mixture of different vitrifiable, natural, or refined materials peculiar to each type of glass which determines its properties. It is this composition which, when mixed with cullet, is put in the furnace. Composition is also used to describe the nature and percentage of oxides which take part in the constitution of the glass.
-
Constringence (See Abbe number)
-
Crown
a. In scientific optics, a low-refractive-index, high-constringence glass which, when combined with a glass of higher index (Flint), produces chromatic lenses.
b. In ophthalmic optics, glass with a refractive index of nd = 1.523, comprising the most extensively used material.
-
Crucible
A container made from heat-resistant materials in which glass is produced through the successive phases of melting, fining, and conditioning. Crucible melting (a manufacturing technique almost discontinued nowadays) is used only for certain kinds of special optical glass.
-
Crystal
A white, highly refractive glass containing at least 24 percent of lead in its composition, with a sonority and particular brilliance as well as high weight for its volume.
-
Cullet
Waste glass which is re-melted and added to the batch. Its presence facilitates melting and saves energy.
-
Curing
Heat transfer energy is used in the manufacturing of plastic lenses. When in the glass mold, the monomer resin is ready to be polymerized either by a combination of ultraviolet (UV) and thermal curing or by thermal curing alone.
See our Manufacturing Techniques – Plastic Lenses Web page for more details.
-
Fading
After returning indoors or by deactivating ultraviolet (UV) light, the appearance of a darkened photochromic lens will gradually fade back/return to its original clear state.
More technical info in our Photochromism Web page.
-
Fixed tint glasses
Fixed- (or solid-) tint glasses, as opposed to white (clear) glass, are designed to absorb some portion of visible-spectrum radiation. Generally speaking, these products are obtained by taking the composition of white glass and adding small quantities of metal oxides or rare earths such as iron, cobalt, nickel, erbium, or neodymium oxides and the like.
-
Flint
- In scientific optics, lead-based glass with a high refractive index and low constringence which, when associated with Crown glass, is used for producing achromatic lenses.
- In ophthalmic optics, Flint (lead-based) glasses have been largely replaced by barium glasses for single-vision lenses segments used in fused multifocals, and by titanium glasses for single-vision lenses for high correction. These glasses provide greater constringence than lead glasses and afford considerable reduction in transverse chromatic aberrations caused by light dispersion, while also lowering the true density.
-
Frequency of light
Light is an electromagnetic radiation of wavelengths that are either visible or invisible to the human eye. Visible from 400 to 700 nm (all the colors of the prism, from violet to red),
Invisible from 10 nm to 400 nm (ultra-violet light, including UVB from 280 to 315 nm and UVA from 315 to 400 nm) and from 700nm to 1mm (infrared light, divided into 3 categories A = up to 1400nm, B = up to 3000nm, C = up to 1mm).
-
Mid-index and high-index lenses
Refractive indices up to 1.56 are generally described as “mid index” and those above are “high indices”. Plastic materials (such as nylon, polycarbonate, Sunsensors®, …) can be found within the 1.5 – 1.71 range of indices, whereas glass reaches 1.9. Due to their lighter weight and thinner-profile advantage over low-index lenses (n = 1.50), mid- and high-index lenses are increasingly demanded by ophthalmic lens wearers.
More technical info in our High Index Web page.
-
Mineral glass
-
Mold
In ophthalmic glass making, the tooling on the press table which collects the gob of hot glass which is then pressed to form a lens blank, or «moulding». The edge of the mould («ring») produces the cylindrical shape, and the bottom of the mould («valve») forms the convex face of the moulding.
-
Molding (pressing or «blank»)
A raw glass disc or similar shape obtained by pressing a hot glass gob which will later be processed into a spectacle lens to meet prescription requirements. The curves of mouldings destined for mass-production machining are formed as closely as possible to the curves of the finished lens.
-
Monomers - Polymers
In chemical terms, a monomer is an organic compound whose molecules can join together to form three-dimensional networks of polymer chains, thanks to a reaction called “polymerization.” Polymers are large molecules, more complex than monomers and with much more diverse shapes and properties, made up of many simple repeated units. Specific types of monomers and polymerization reactions are used to manufacture plastic lenses.
-
OHSAS (Occupational Health and Safety Assessment Series)
As defined by British Standards International (BSI):
The OHSAS specification gives requirements for an occupational health and safety (OH&S) management system, to enable an organization to control its OH&S risks and improve its performance. It does not state specific OH&S performance criteria, nor does it give detailed specifications for the design of a management system.
OHSAS 18001 has been developed to be compatible with the ISO 9001 (Quality) and ISO 14001 (Environmental) management systems standards, in order to facilitate the integration of quality, environmental, and occupational health and safety management systems by organizations.
-
Organic compound
In chemical terms, a compound containing hydrocarbon groups. Manufacturing ophthalmic plastic lenses mainly relies on organic chemistry. (Manufacturing ophthalmic glass lenses mainly relies on mineral chemistry).
-
Organic glass
Opposite of mineral glass.
Transparent plastic material made from organic chemistry (monomers/ resins/ catalysts/ polymerization), which has several common properties with glass; this is why the ophthalmic market relies on both categories to address diverse customers’ needs and expectations. Plastic lenses are less scratch-resistant than glass lenses (thus requiring Hard Coating), not as perfectly transparent, but they are much lighter and some of them are highly resistant to impact.
-
Parison
A drop, or gob, of glass which is cut by shears as it leaves the delivery tube. The parison then falls into the mould to be pressed into a lens blank. The weight of the parison corresponds exactly to the weight of the pressed blank.
-
Photochromic coating technology
The coating technology offers both high performance and flexibility. It consists in applying photochromic resin on the white lens substrate by spin or dip coat to form a thin photochromic layer on the lens surface. Such technology can be applied on high-index and polycarbonate substrates. Corning’s HPC technology is based on coating technology: HPC = High Performance Coating
See our Web pages: Photochromism and Manufacturing Techniques – Plastic Lenses.
-
Photochromic dye
The photochromic dye is an organic molecule which undergoes a reversible chemical reaction when exposed to ultraviolet A (UVA): the opening or closing of its structure, respectively causing the fading or darkening of the lens. Most of the time, a photochromic plastic lens will incorporate a specific mix of several dyes, all of them photochromic.
More technical info in our Photochromism Web page.
-
Photochromic in-mass technology
The in-mass photochromic technology disperses photochromic dyes throughout the lens material with a specific manufacturing process ensuring that they are distributed evenly. As ultraviolet (UV) exposure may, in the long run, degrade some of these molecules (those closer to the convex curve), others as yet inactivated replace them, providing a long-lasting, consistent color over the life of the prescription.
See our Web pages: Photochromism and Manufacturing Techniques – Plastic Lenses.
-
Photochromic plastic resin
-
Photochromism (photochromicity)
Photochromism may be defined as the modification by solar radiation of a material's light absorption characteristics. Thus, certain glazed articles are susceptible to a slight darkening after some years of exposure.
In general, this phenomenon is not reversible. In photographs, for example, sensitive particles undergo a definitive transformation on exposure to radiation in the near-ultraviolet portion of the spectrum. The invention of photochromic glass, on the other hand, has introduced a family of products in which the active elements, silver halide particles, are capable of undergoing a succession of darkening / clearing cycles without evidence of fatigue as manifested by a slowdown in their light response capacity. A representation of the elementary mechanism involved corresponds to the following electronic exchange between the silver atoms and their immediate environment:
Equilibrium is moved towards the right under the effect of ultraviolet or short-wavelength visible radiations. In the absence of this type of radiation, the system tends to revert to its original state :
-
Plastic lenses
Plastic lens raw materials can be divided in two groups: thermosetting and thermoplastic resins.
- Thermosetting resins, such as nylon, medium & high index lens resins, are hardened by heating without any possibility of reshaping. This type of resin is transformed into lens by casting.
- Thermoplastic resins, such as polycarbonate, soften when heated and can thus be reshaped at specific temperatures. This type of liquid resin is transformed into lens by injection.
See our Manufacturing Techniques – Plastic Lenses Web page for more details.
-
Platinum
A noble metal used in those parts of the furnace which are heated to the highest temperatures. Platinum is used for its heat-resistant and non-polluting properties, and for its chemical inertia.
-
Plunger
That part of the tooling fixed to the piston rod which presses the parison in the mould. The shape of the plunger determines the curvature of the concave face.
-
Poise (See also Viscosity)
A poise is the unit of measurement of the dynamic viscosity of a liquid manifesting a resistance of 1 dyne when sliding on a flat surface of 1 sq. cm. with an increasing speed of 1 cm per second / per cm.
-
Polarized glass
In simple terms, polarized sunglasses eliminate most of the annoying glare coming from flat reflective surfaces (roads, snow, lawns, lake water,…). This effect is obtained by the presence of a polarizing film between two thin layers of glass, one being a tinted glass (external side, with all necessary sunglass treatments), and the other one being a neutral glass.
More technical info in our Sunglass educational Web page.
-
Polishing
The treatment of a ground lens surface (see smoothing) to make it absolutely transparent. Polishing occurs by rubbing on a tool covered with felt or a plastic sheet while the lens is constantly sprayed with water containing finely powdered cerium oxide in suspension.
This operation should in no way alter the curves of the lens previously generated and smoothed.
-
Polycarbonate lenses
Polycarbonate is one among several plastic materials used to manufacture ophthalmic lenses.
Its main benefits for patients are its excellent impact resistance, light weight, and high refractive index (n= 1.59). Its market share is quite significant in the USA.
Polycarbonate is a thermoplastic polymer. Such lenses are made by injection molding. The adequate lens forming technology consists of melting the raw material granules by heating, then injecting into metallic or glass molds at high temperature for a few seconds.
-
Shears
In the context of glass-making, mechanical cutters equipped with special alloy blades to cut the glass as it leaves the delivery tube so as to obtain a repeated series of very accurately weighted parisons for pressing in moulds.
-
Silver halide
Silver halides are compounds blending silver with elements which are halogens, such as chlorine or bromine. In their pure state they correspond to the formulae AgCl and AgBr. When added to a glass composition, silver halides are dispersed throughout the substance of the material as minute particles (about 100 angstroms). The number and size of these particles is determined by the application of thermal treatment, to ensure the reproducibility of the photochromic glass materials transmission characteristics and colour (gray or brown).
-
Smoothing (fine grinding)
This operation is designed to refine the rough surface of the lens following the process of generation. Smoothing is achieved by mechanical rubbing of the lens surface on a cast-iron counterform, while the lens is sprayed with a solution of emery in water suspension. Lens smoothing can also be effected using a counterform impregnated with small pellets of diamond sunk into a sintered bronze matrix. Smoothing should not alter the lens curve previously generated.
-
Soda-lime glasses
These are the most prevalent glass types (used for window glass, tableware, and so on). In addition to silicon, which accounts for about 70 percent of their composition, these glasses also contain sodium and calcium oxides. For spectacle lenses, ordinary Crowns belong to this category of glass. They differ essentially according to the raw materials selected and the choice of additional ingredients to determine their optical and physical properties.
-
Substrate
The primary material or the underlying layer on which other materials (such as a coating, a paint, or a treatment) is applied.
-
Titanium glasses (See High Index glasses)
-
Top-siding (of a fused bifocal lens)
An operation which consists of grinding away all the surplus thickness of the near vision segment fused onto the «major» lens. After top-siding, the whole of the convex face of the rough bifocal lens becomes a continuous spherical surface on which, because of the difference in material index, the exterior contour of the near vision segment can be seen.
-
Torr
Unit of pressure adapted for measuring high vacuums and derived from the name of the Italian physicist TORRICELLI.
1 Torr = 1 mm of mercury
Units for surface treatment through vacuum depositing operate under residual pressures of 10-4 to 10-6 Torr.
-
Transmission
For a given wavelength, this is the quotient of transmitted light flux Φt, to the incident light flux Φi
The transmission factor, spectral transmittance, varies with wavelength. The variation of this factor as a function of wavelength is represented by the transmission curve.
The difference in values of transmitted light flux and incident light flux are caused by:
- the intrinsic absorption of glass (this is negligible for certain lenses such as clear (white) lenses),
- a loss by reflection on both sides of air / lens diopter (see the chapter on «Anti-reflection and tint coatings»).
-
True density
This is the quotient between the mass and the volume of the glass. True density is expressed in terms of grams / cubic centimetres. For glass spectacle lenses density can vary from 2.4 to 4.0 g/cm3.