Overview
Educational Information
Plastic Solutions
Glass Solutions
Polarizing Solutions

Glass


AtomArgent_thumb.jpg

Photochromism: a phenomenon of chemistry   

ControlLenses

Quality Control

PhotochromicLens

Photochromic lenses 

Photochromic glass lenses

A specific mode of action: Silver atoms
The photochromic mechanism that takes place in a glass photochromic lens is very different from what happens with plastic.

The light-reactive properties of silver atoms have long been known. Photography is a key example, but in this field, the process is not reversible.

Photochromic glass lenses, on the other hand, where the reaction is mediated by atoms of silver in the matrix of a specially constituted vitreous environment, are capable of continuous and reversible change between the clear and darkened states. The number of atoms present, and their distribution within the lens, will directly influence transmission levels and lens color. Additionally, the basic composition of the lens determines the rate of change through the darkening-clearing cycle.

The basic principles governing this change of state in the atoms of silver are schematically represented in our animation. Influenced by UV-A or short-wave visible spectrum radiation, an atom is able to modify its external electronic structure by deployment of the electrons present in the vitreous structure. When such radiation is no longer present, the system returns to its original state.

Stable and durable 
Laboratory tests involving several tens of thousands of darkening-clearing cycles, corresponding to long years – or even decades – of normal use, have revealed no significant fatigue in this phenomenon. Indeed, it shows remarkable reversibility under natural lighting conditions. This, added to the natural transparency of glass and the in-mass presence of the photochromic agent, explains how stable glass photochromic lenses can be in the long run.

A complex process 
Optimum precision in product manufacturing is required to regulate photochromic performance, especially during the critical stage of annealing. After melting and pressing, the carrying of a lens through an annealing lehr (at temperatures up to 700°C depending on the nature and softening point* of the glass) is a commonly used internal stress-reduction process. But when it comes to photochromic glass, annealing is also the way to activate the silver-halide crystals, and its temperature has to be regulated with a precision of 1°C, taking into account the size and number of crystals, the glass composition and volume, and the photochromic characteristics – a very complex process which Corning pioneered in the mid 1960s and never stopped improving since then.

Corning Ophthalmic offers a wide variety of glass photochromic lens materials worldwide. Patented in-mass technology provides photochromics throughout the lens material; guaranteed lens matching, batch after batch; and color consistency during activation – plus, the well-known advantages of natural scratch-resistance and anti-reflective (AR*) glass compatibility.