visit Life Sciences at Corning.com
visit corning.com
  what's new  
  cell culture history  
  inside life sciences  
  news center  
  products + solutions  
    product catalog  
    warranty/guarantee
  registration
 
    product literature  
    corning surfaces  
    equipment   compatibility guide  
    stirrer and hot plate   selection guide  
  technical information  
  our locations  
  events  
  careers  
  contact us  
    inquiries  
    order information  
    our distributors  
    corning partners
  network
 
  order information  
  corning dealer network  
 
     
 


 catalog only   

 other site sections

corning home > life sciences > US + Canada > products + solutions > surfaces > assay >

Corning Surfaces
> Assay
> General Assay
> Cell-based Assay
> Cell Culture
> Microarray
 
Additional Information
  • > Request a sample, price quote,
       account manager follow up or
       technical presentation
  • > Register for the Corning Live
       Scientific Seminar Series
  • > Visit us at an upcoming trade
       show or conference
view what's new...
 

Corning® Assay Surfaces

Corning offers a variety of modified polystyrene surfaces for the binding or covalent immobilization of cells, proteins, nucleic acids, and other types of biomolecules for use in microplate-based assays that do not require cell attachment (see Table 1). Check Corning® Cell Culture Surfaces for information on assay surfaces for cell-based assays.

Choosing the appropriate assay surface requires that the structure of the molecule to be immobilized be known, so that functional groups available on the molecule can be matched with the correct surface. Of particular concern is that the functional group on the biomolecule interacting with the surface must be positioned in such a manner that immobilization does not interfere with its immunological or enzymatic activity.


Table 1. Corning® microplate assay surfaces

Corning Surface
Binding Interaction
Sample Properties
NBS™ coated polystyrene surface None - Inhibits hydrophobic and ionic interactions Significantly reduces (<2 ng/cm2) protein and nucleic acid binding
Medium Binding (Untreated) modified polystyrene surface Hydrophobic Large biomolecules >20kD with large or abundant hydrophobic regions
High Binding modified polystyrene suface Hydrophobic and ionic (negatively charged) Improves binding of medium to large biomolecules (>10kD) that are positively charged with or without hydrophobic regions.
Aminated-modified polystyrene surface Hydrophilic and ionic (positively charged); allows covalent immobilization Small negatively charged biomolecules OR biomolecules possessing an appropriate functional amine, carboxyl or thiol group.
DNA-BIND® modified polystyrene surface Allows covalent immobilization to amine groups via binding to NOS groups Small to medium biomolecules, especially DNA, possessing an available amine group.
Sulfhydryl-BIND™ modified polystyrene surface Allows covalent immobilization via SH moietics on maleimide groups Biomolecules possessing an accessible sulfhydryl group or reducible disulfide bond.
Carbo-BIND™ modified polystyrene surface Allows covalent immobilization via binding to hydrazide groups Biomolecules possessing carbohydrate moieties available for periodate activation.
Universal-BIND™ modified polystyrene surface Allows covalent immobilization via UV cross-linking to abstractable hydrogen Biomolecules with abstractable hydrogen.
Standard Tissue Culture Surface Hydrophilic and ionic interactions (negatively charged) Allows cell attachment and binding to polystyrene
Corning® CellBIND® Surface Hydrophilic and ionic interactions (negatively charged) Improves cell attachment uniformity and binding to polystyrene
Poly-D-lysine-Coated Surface Hydrophilic and ionic interactions (positively charged) Improves cell attachment and binding to polystyrene
Ultra Low Attachment Surface Nonionic hydrogel layer reduces or eliminates ionic and hydrophobic interactions Inhibits or prevents cell attachment and binding to polystyrene


Figure 1. Polystyrene can be surface modified by the addition of a variety of different chemical groups, breaking the carbon chain backbone or opening the benzene ring. Here the benzene groups have been replaced by amine groups to create an aminated surface.

Overview

The first 96 well microplates were manufactured from a variety of plastic resins in the 1950's for use in virus titration studies. By the mid 1960's, most of these microplates were made from polystyrene, a long carbon chain polymer with benzene rings attached to every other carbon. Polystyrene was chosen because it has excellent optical clarity, is easy to mold and is relatively inexpensive. In addition, the normally hydrophobic surface of polystyrene can be easily modified by a variety of chemical and physical (corona discharge, gas-plasma or irradiation) methods to make the surface hydrophilic and thus suitable for cell attachment and culture (Figure 1). By the late 1970's, these microplates were also being used as reaction vessels for Enzyme-Linked Immunosorbent Assays (ELISA) which require surfaces suitable for immobilizing proteins and other biomolecules. By altering the chemical and physical surface treatment methods, a variety of chemical groups can readily be grafted onto the polymer to allow the covalent attachment of a variety of reactive groups for the subsequent covalent immobilization of biomolecules. Corning offers microplates in a wide variety of formats and well designs (see Table 2).


Table 2. Corning® microplate surface selection chart

Surface Type Microplate Format
96 Well 96 Stripwell™ Microplate 96 Half Area Well (190無) 384 Well(112無) 384 Low Volume (35-50無) 1536 Solid Well (10無) 1536 Low Volume Well (2無)
For General Assay
NBS™ Surface x x x x x x
Medium Binding (Untreated) x x x x x x x
High Binding x x x x x
x
Aminated Surface
x




DNA-BIND™ Surface x x




Sulfhydryl-BIND™ Surface x x




Carbo-BIND™ Surface x x




Universal-BIND™ Surface x x




For Cell-Based Assays
Ultra Low Attachment x





Tissue culture x x x x x x x
Corning® CellBIND® Surface x

x


Poly-D-lysine x

x


Immobilization Mechanisms

Proteins and other biomolecules attach to surfaces by several different mechanisms. (Please refer to Corning Technical Bulletin Immobilization Principles - Selecting the Surface for additional information.) Passive adsorption consists of primarily hydrophobic interactions or hydrophobic/ionic interactions between the biomolecules and the surface. Typical nomenclature for passive binding surfaces includes Medium Binding (Untreated) for hydrophobic surfaces and High Binding for surfaces that are modified to have a small number of ionic carboxyl groups resulting in a slightly ionic, hydrophobic surface. Covalent immobilization to polystyrene can be accomplished through several means. On surfaces that are aminated or carboxylated, covalent coupling is achieved using bifunctional crosslinkers that couple the amine or carboxyl group on the surface to a functional group, such as an amine or sulfhydryl, on the biomolecule. Selection of the crosslinker determines the type of covalent bond that will be formed. Functional and covalently reactive groups, such as N-oxysuccinimide, maleimide and hydrazide groups, can also be grafted onto a polystyrene surface. These reactive groups are coupled to the polystyrene via a photolinkable spacer arm resulting in a stable, yet reactive surface.


corning.com | inside corning | products + services | discovery center | media center | investor relations | careers

Copyright © 2008 Corning Incorporated. All rights reserved. | Legal Notices and Privacy Policy