Terrier missile being test fired from the deck of the USS Harry E. Yarnell
DLG-17. These anti-aircraft missiles were equipped with Corning Pyroceram
radomes (nosecones) during the late 1950s. Photo courtesy of Carlos Royal.
Originally developed in the
early 1950’s by Corning for use by the military, Pyroceram glass-ceramic is
extremely durable, corrosion resistant and has a very low coefficient of
expansion. It is also transparent to radar, which made it ideal for use as
nosecones on anti-aircraft missiles.
These space age
characteristics allowed Pyroceram glass-ceramic to be very successfully adapted
for commercial use as Corningware® products for cooking in 1959. Its
transparency to radar (microwaves) also allowed Corningware products to be
used in microwave ovens, greatly extending their versatility in the kitchen.
Pyroceram glass-ceramic next found a place in
biology and chemistry laboratories when it was used in 1964 to make tops for
hot plates and stirrers. Unlike metal tops, glass ceramic is easy to clean,
highly resistant to scratches, corrosion and chemical attack. Pyroceram tops
heat up hotter than metal typically providing temperatures 200°C above metal
top products. Pyroceram tops are also white allowing easy viewing of color
contrasts in such applications as titrations. As a result, it has been the
material of choice for Corning hot plates for over forty years.
Corningware Pyroceram heat resistant cookware was an instant
hit with people who liked their looks as well as their performance.
Corning’s new digital hot plates and stirrers
still offer the same unique Pyroceram tops that have set the standard for
quality for over 40 years.