A digital subscriber line, or DSL, uses the same copper wire as traditional telephones. Cable modem provides service through existing hybrid fiber-copper, or HFC, lines. It is important to understand that toth of these transmission media have significantly less bandwidth capability than glass fiber. DSL connections are also more likely to be slowed due to the deterioration of the copper lines, most of which were installed more than 15 years ago. Cable modem subscribers share their bandwidth with other subscribers in the area, which also slows cable modem speeds.
Finally, DSLs and cable modems are typically "asymmetrical" in order to maximize, as much as possible, their more limited bandwidth capabilities. Asymmetrical networks maximize their limited bandwidth capacity by offering faster data rates "downstream" to your home than upstream from your home. So, for example, you can receive e-mails with picture attachments very quickly, but send out your own e-mails with pictures attached much more slowly.
Ultimately, cable modem and ADSL are little more than broadband "bandages," temporary solutions that will ultimately be replaced by optical fiber, which has virtually unlimited bandwidth. Optical fiber is the smart, long-term solution for broadband to your home.