University of Colorado Anschutz Medical Campus

Industries: Academic, Medical

World-class cellular + fiber network = 5G ready

World-class cellular + fiber network = 5G ready

The Customer

The Anschutz Medical Campus in Aurora, Colorado spans more than 200 acres with more than 19 buildings that depend on a connected experience. But at times, students, researchers, doctors and staff across 4 campuses were left with no bars, dropped calls and lots of frustration. For this top-tier academic medical facility, second-rate connectivity wasn’t an option. 

The Challenge: Upgrade DAS and prepare for the future

Performance issues became the norm for this campus’ outdated coax-fed DAS. Software upgrades became almost constant. As the campus began a renovation project, the network infrastructure team on campus set out to find a connectivity solution to today’s problem that could support future technologies.

The Solution

With the help of integrator KLA Laboratories and distributor partner WESCO|Anixter, a connectivity solution to fit the needs of the campus was found.

Cellular SolutionsThe 5G-ready multi-carrier DAS solution got the campus connectivity up to speed quickly. With increased capacity and coverage and industry leading 5G capability, they are ready for what’s next as cellular connectivity continues to evolve.

Horizontal LAN (Fiber to the Edge)ActiFi® Composite Cable with copper conductors and optical fiber (12x12) in one cable spanned distances greater than traditional copper, bringing power and bandwidth across the 200+-acre campus. While all 12 fibers are not needed today, they will be critically important soon enough as more applications are deployed. 

Click here to download the full case study PDF or learn more about our technology solutions for higher education

“If I chose a different solution, I’d have to do a full rip and replace in 2-3 years. But now, the infrastructure is there. You might not use all the strands now, but they are there to utilize.”

- John Fuson, IT Telecom Network & Infrastructure Manager

Scalable Network

 

33% Capex Savings
26% less after 5G mm Wave and Private LTE adds 33% less after digital DAS, MIMO upgrade in Year 5

 

Cost Effective

 

70% Energy Savings
Less HVAC cooling for equipment means saving on energy expenses

 

Reliable

 

62% Fewer Telecom Rooms
Reduction in telecom rooms means more efficient space usage

 

Contact us today!

Contact your Corning Sales Engineer or contact our Business Development Representative Chris Williams by filling out the form below.

Thank you!

Thank you for your inquiry. One of our representatives will be in touch with you shortly. 

Read More