Corning® Gorilla® Glass and Krystal™ Glass Writing Boards Deliver Creative Approach to Markerboard Market
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
IE is bad

News Release

News Release

News Release

News Releases
Gorilla Glass
Corning® Gorilla® Glass and Krystal™ Glass Writing Boards Deliver Creative Approach to Markerboard Market
Corning® Gorilla® Glass and Krystal™ Glass Writing Boards Deliver Creative Approach to Markerboard Market
Corning, NY | Corning Incorporated | September 03, 2013

CORNING, N.Y., September 3, 2013 -- Corning Incorporated (NYSE:GLW) announced plans to collaborate with Krystal™ Glass Writing Boards on a new approach to traditional markerboard designs and configurations.

Industry leading Corning® Gorilla® Glass, known for its thin, durable, and scratch-resistant surface, is now delivering its unique qualities to the markerboard market. Gorilla Glass not only helps address the markerboard issue of ghosting or double imaging — often seen in thicker glass board products — but also provides mounting and installation cost savings, and expanded design options.

“Gorilla Glass is the ideal solution for solving issues end users have had with markerboards for years,” said Charlie Baker, chief executive officer of Krystal Glass Writing Boards. “Melamine and porcelain whiteboards are typically replaced every three to five years due to stains and damage issues. We have found that Gorilla Glass is stain-resistant and exceptionally durable, increasing the life span of boards versus those using traditional materials. Additionally, Gorilla Glass brings new design and configuration options that have not previously been available to our market.”

“We believe these markets are looking for a new solution that can deliver improved functionality with an aesthetic appeal that is retained even with prolonged use,” said David Loeber, Corning Large Cover Glass business director. “Gorilla Glass retains its damage resistance despite its thin form factor and offers customers enhanced optical clarity over traditional glass markerboards for an improved viewing experience. Corning is pleased to work with Krystal to deliver these benefits to end users.”

For more information on Gorilla Glass for markerboards, or to find a list of manufacturers incorporating Gorilla Glass into their markerboard designs, please visit:


Forward-Looking and Cautionary Statements
This press release contains “forward-looking statements” (within the meaning of the Private Securities Litigation Reform Act of 1995), which are based on current expectations and assumptions about Corning’s financial results and business operations, that involve substantial risks and uncertainties that could cause actual results to differ materially. These risks and uncertainties include: the effect of global political, economic and business conditions; conditions in the financial and credit markets; currency fluctuations; tax rates; product demand and industry capacity; competition; reliance on a concentrated customer base; manufacturing efficiencies; cost reductions; availability of critical components and materials; new product commercialization; pricing fluctuations and changes in the mix of sales between premium and non-premium products; new plant start-up or restructuring costs; possible disruption in commercial activities due to terrorist activity, armed conflict, political or financial instability, natural disasters, adverse weather conditions, or major health concerns; adequacy of insurance; equity company activities; acquisition and divestiture activities; the level of excess or obsolete inventory; the rate of technology change; the ability to enforce patents; product and components performance issues; retention of key personnel; stock price fluctuations; and adverse litigation or regulatory developments. These and other risk factors are detailed in Corning’s filings with the Securities and Exchange Commission. Forward-looking statements speak only as of the day that they are made, and Corning undertakes no obligation to update them in light of new information or future events.

About Krystal Glass Writing Boards
Krystal™ Writing Boards, Inc. ( offers the highest quality glass writing board systems available. The innovative design replaces the old, stained, whiteboards of the past. Our custom manufacturing allows us to individualize the build process, customizing the graphics, mounting options and color backings, specifically for each client. Each glass dry erase board is inspected after each phase of the production at our New York factory and is manufactured using the finest “green” ecologically friendly materials and processes.
Since 2008 Krystal™ Glass Writing Boards are made of tempered safety glass, and we incorporate special coatings to allow for decades of crisp clear use. We continually develop cutting-edge processes and products for the glass dry-erase marketplace.

About Corning Incorporated
Corning Incorporated ( is the world leader in specialty glass and ceramics. Drawing on more than 160 years of materials science and process engineering knowledge, Corning creates and makes keystone components that enable high-technology systems for consumer electronics, mobile emissions control, telecommunications and life sciences. Our products include glass substrates for LCD televisions, computer monitors and laptops; ceramic substrates and filters for mobile emission control systems; optical fiber, cable, hardware & equipment for telecommunications networks; optical biosensors for drug discovery; and other advanced optics and specialty glass solutions for a number of industries including semiconductor, aerospace, defense, astronomy, and metrology.

Media Relations Contact:
Anna I. Giambrone
(607) 974-5933

M. Elizabeth Dann
(607) 974-4989

Investor Relations Contact:
Ann H. S. Nicholson
(607) 974-6716