Glass for Smartwatches and Wearables | Incredibly Tough | Corning Gorilla Glass



Whatever Your Thing — Corning® Gorilla® Glass for Wearables

Whatever Your Thing — Gorilla® Glass for Wearables

Today’s athletes, whether amateurs or professionals, have embraced wearable devices as a training tool of choice to track workouts, navigate routes, count steps, measure heart rates, receive texts, take calls or just tell the time. Untethered from smartphones, these devices can take, make and create data on the run. Yet, to hold value, the seemingly indispensable wearable device must withstand the tough circumstances that come with territory. Indoors, outdoors, on dry land, or in the water, today’s wearable devices need to be just as tough as the person who is putting in the effort. Not surprisingly, leading device manufacturers have designed in Corning® Gorilla® Glass for robust, high-performance Smartwatches and wearable fitness aids. In 2016, Corning introduced Corning Gorilla Glass SR+. Specifically developed for wearable devices, Gorilla Glass SR+ combines the legendary toughness, optical clarity and touch sensitivity of Gorilla Glass with superior scratch resistance approaching that of luxury watch cover materials. Check out the list below to discover recent wearable devices featuring Gorilla Glass. Whatever your thing — tough wears well.   

 

Recent Wearables featuring Corning® Gorilla® Glass

  • Samsung

    Samsung Gear S3 (Corning® Gorilla® Glass Sr+)

    Samsung Gear Sport (Corning® Gorilla® Glass 3)

    Samsung Gear Fit2 Pro (Corning® Gorilla® Glass 3)

    Samsung Gear S (Corning® Gorilla® Glass 3)

    Samsung Gear 2 (Corning® Gorilla® Glass 3)

    Samsung Gear Fit (Corning® Gorilla® Glass 3)

    Samsung Gear 2 Neo (Corning® Gorilla® Glass 3)

    Samsung Gear (Corning® Gorilla® Glass 3)

  • Acer

    Acer Leap Ware (Corning® Gorilla® Glass Sr+)

  • ASUS

    ASUS ZenWatch (Corning® Gorilla® Glass 3)

  • LG

    LG G Watch (Corning® Gorilla® Glass 3)

  • Motorola

    Moto 360 (Corning® Gorilla® Glass 3)

    MOTOACTV (Corning® Gorilla® Glass)

INCREDIBLY TOUGH

share