Skip to main content

Corning’s Gorilla Glass 6 will help your phone survive up to 15 drops before it shatters

Corning
Corning Incorporated

Corning has long been the go-to for smartphone manufacturers who want a nice, tough piece of glass to keep their devices safe in the event of a drop or scratch. Now, the company is stepping things up with the launch of Gorilla Glass 6, which Corning says is up to two times better than the previous version, Gorilla Glass 5.

Phone designs have changed a lot over the years, making the strength of the glass used on phones more important than ever. When smartphones were first released, for example, they often had thick metal or plastic frames, which was the first part of the phone to often make contact when a phone was dropped. Now, smartphones have curved edges and glass backs, resulting in an almost completely glass exterior.

Often, your phone won’t break the first time you drop it, and that’s because up until that point there aren’t any flaws in the glass. With a drop, however, small flaws can be introduced into the glass — meaning that the next time you drop your phone, the weakened glass can more easily break. That’s an issue that Corning has been trying to fix with Gorilla Glass 6, the company told Digital Trends. Gorilla Glass 6 can survive 15 drops from 1 meter before it breaks — which is a solid improvement over the 11 drops Gorilla Glass 5 could get through. Corning said that people, on average, drop their phones seven times per year, so being able to survive 15 drops means the glass should get a phone through a standard two-year upgrade cycle.

These numbers are based on lab tests, though, and real-world drops are often a different beast. Out and about, drops aren’t controlled, and if a phone is dropped when you’re standing, it’s usually from more than 1 meter. Still, any improvement on glass strength is a win-win, whether or not the glass actually survives 15 drops or not.

Gorilla Glass 6
Image used with permission by copyright holder

On top of improving glass durability, Corning has also been working on improving how its glass looks — and has developed a technology to print designs on glass without compromising durability. At a media event, the company showed off a number of interesting designs, including one that mimics the look and feel of wood.

Corning isn’t only focusing on smartphones. The company also unveiled Gorilla Glass DX and Gorilla Glass DX+, which is aimed specifically at wearables and other similar devices. The DX-series replaces the Gorilla Glass SR series, and Corning said it vastly improves on optics, cutting down on glare — which is crucial for wearable devices. In fact, compared to so-called “normal glass,” Corning said DX and DX+ glass cuts down on reflection by up to 75 percent.  Gorilla Glass DX+ is more scratch-resistant than Gorilla Glass DX, but it’s also a little more expensive.

Gorilla Glass 6
Image used with permission by copyright holder

Corning is in a pretty good position right now. The world is finally moving to wireless charging, and you need glass on the back of the phone to make the technology work. In other words, strong glass is more important than ever in phone design, which is good news for the company.

There’s no word on specific phones to feature Gorilla Glass 6, but the company said we’ll see phones with the new glass by the end of the year.

Updated on July 18: We’ve added more details after attending a media event.

Editors' Recommendations

Christian de Looper
Christian’s interest in technology began as a child in Australia, when he stumbled upon a computer at a garage sale that he…
We finally know when Apple will announce its 2024 iPads
Official artwork for Apple event in May 2024.

(more…)

Read more
One of the biggest Oura Ring competitors just did something huge
The Ultrahuman Ring Air and the Oura Ring, resting on a table.

Ultrahuman, the maker of the Ultrahuman Ring Air, is making its way to U.S. production grounds. The company is setting up a production facility in Indiana, which will mark the first time a smart ring from Ultrahuman will be assembled from scratch on U.S. soil.

“The UltraFactory will offer an end-to-end production capability and is based on the company’s first operational model of such a facility in India,” the company says.

Read more
Best Verizon new customer deals: Galaxy S24, iPhone and more
Verizon logo on a smartphone screen in a dark room and a finger touching it.

If you’re in the market for one of the best phones, or any new phone for that matter, you’re going to need a good carrier. Verizon has long been one of the most popular options, as it boasts one of the most reliable networks in the United States. It offers some of the best cell phone plans out there, and for new customers Verizon also offers some pretty impressive discounts on new phones. In many cases this means you can brand new, recently released phones entirely for free when signing up with Verizon. And that’s the case right now, as we’re currently seeing some of the best Verizon new customer deals we’ve seen. You can pretty easily land a new iPhone, Samsung Galaxy phone, and Google Pixel for free, and we’ve got all of the details on how to do so. If that sounds enticing, read onward and start shopping the best Verizon new customer deals available right now.
Free iPhone SE (3rd Gen)

The 2022 release of the Apple iPhone SE is yours for free when you sign up for a new 5G data plan on Verizon -- no trade-ins required. It's the best small smartphone in our list of the best smartphones with a 4.7-inch Liquid Retina display, but it doesn't sacrifice performance as it's powered by Apple's A15 Bionic chip that's also found in the iPhone 13 line and pre-installed with iOS 15. The latest iPhone SE is equipped with a single 12MP rear sensor and 7MP selfie camera, which are boosted by Apple's software to enable better photographs.

Read more