Gorilla Glass | Corning Gorilla Glass
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
Gorilla Glass 4

Gorilla Glass Types

Gorilla Glass Types

Gorilla Glass 4

CORNING® GORILLA® GLASS

Today’s smartphones have become the primary tools consumers use to capture, view, create, send and consume digital content. And the cover glass is the interface for all that touching, typing and swiping. The last thing anyone wants is a scratched or damaged screen. That’s why consumers count on Corning Gorilla Glass to deliver superior damage resistance, optical clarity and touch sensitivity. Gorilla Glass is chemically strengthened through an Ion-exchange process that creates a deep compression layer on the surface of the glass substrate. This layer acts as “armor” to reduce the introduction of flaws. Just as important, Corning’s proprietary fusion process gives Gorilla Glass an exceptionally clean, smooth, flat surfaces and outstanding optical clarity. It should come as no surprise that Gorilla Glass has been designed into more than 5 billion devices by more than 40 major OEMs. Is it on yours?

SEE THE ADVANTAGES

No Current News