Corning Works with Micromax to Deliver Corning® Gorilla® Glass on New Vdeo Series of Smartphones

Comunicado de imprensa

Comunicado de imprensa

Comunicado de imprensa

Comunicado de imprensa
Gorilla Glass
Corning Works with Micromax to Deliver Corning® Gorilla® Glass on New Vdeo Series of Smartphones
Corning Works with Micromax to Deliver Corning® Gorilla® Glass on New Vdeo Series of Smartphones
Corning, NY | Corning | Fevereiro 08, 2017

India’s leading device manufacturer brings Gorilla Glass to value-segment devices

CORNING, N.Y., February 8, 2017  — Corning Incorporated (NYSE:GLW) today announced that it has collaborated with Micromax for its Vdeo smartphones, designed for the “value-segment” consumer. The recently launched devices are among the first across India’s mobile phone entry segment to incorporate Corning® Gorilla® Glass to help protect against damage.

“Value-segment smartphone customers typically spend a significant portion of their income buying a device,” said John Bayne, vice president and general manager, Corning Gorilla Glass. “Many of these first-time smartphone users simply cannot afford to repair or to replace a damaged device. That’s why it’s essential to protect these devices with a material such as tough, damage-resistant Corning Gorilla Glass.”

A recent consumer poll* conducted in India, which is the second largest smartphone market in the world, highlights the needs of India’s critical value-segment smartphone category predominantly serviced by devices ranging in price from Rs 5,000 to Rs 10,000 ($75 to $150).

The study focuses on the participants’ expectations and performance of devices they currently own. Highlights of the study results include:“

  • Approximately 58% said that their smartphone is the most expensive thing that they carry with them daily, and their single biggest worry is damaging their device. Also, 68% of respondents said they worry about dropping and breaking their screen.
  • Over 65% of value-segment smartphones are reported to have significant screen damage with more scratches per device than consumers in other segments.
  • When they do replace their smartphones, the majority (52%) said that they plan to spend almost the same amount on a new device as their current one, but expect it to have better functions and capabilities.

Bayne added, “For all mobile phone consumers, their device is critical. It is often the most valuable thing they carry on their person every day and something they use not just to communicate but, in many cases, as their primary access to information. We are thrilled that Micromax – one of India’s premier device manufacturers – has designed Gorilla Glass into its Vdeo smartphones to give value-segment users the protection that they not only need, but they deserve. This level of performance is not possible with other material options.”

“It is important for the entire ecosystem to come together to deliver a compelling and complete solution to consumer needs. With the Micromax Vdeo range we have broken the perception that a durable, high-quality display is limited to premium devices,” said Shubhajit Sen, chief marketing officer, Micromax. “We believe our continued collaboration with Corning will help propel adoption of smart phones with consumers in the value segment."

The Vdeo range of smartphones are designed keeping in mind the basic needs that Indian consumers demand from their smartphones and are fully loaded with best-in-class features for an entry level Smartphone – including 4G VoLTE, Android Marshmallow, great battery performance, HD display and housed in a premium and stylish metal body.

Leveraging its strengths in glass science and fusion manufacturing, Corning leads the cover glass industry it created nearly 10 years ago. Corning Gorilla Glass has been used on nearly 5 billion devices worldwide, including more than 1,800 product models across 40 major brands.

*The consumer poll was conducted across four cities in India, using an online survey, with over 1,200 smartphone users responding. The research was conducted through a combination of online polling and secondary analysis by ValueNotes Research in India.

Forward-Looking and Cautionary Statements
This press release contains “forward-looking statements” (within the meaning of the Private Securities Litigation Reform Act of 1995), which are based on current expectations and assumptions about Corning’s financial results and business operations, that involve substantial risks and uncertainties that could cause actual results to differ materially. These risks and uncertainties include: the effect of global political, economic and business conditions; conditions in the financial and credit markets; currency fluctuations; tax rates; product demand and industry capacity; competition; reliance on a concentrated customer base; manufacturing efficiencies; cost reductions; availability of critical components and materials; new product commercialization; pricing fluctuations and changes in the mix of sales between premium and non-premium products; new plant start-up or restructuring costs; possible disruption in commercial activities due to terrorist activity, armed conflict, political or financial instability, natural disasters, adverse weather conditions, or major health concerns; adequacy of insurance; equity company activities; acquisition and divestiture activities; the level of excess or obsolete inventory; the rate of technology change; the ability to enforce patents; product and components performance issues; retention of key personnel; stock price fluctuations; and adverse litigation or regulatory developments. These and other risk factors are detailed in Corning’s filings with the Securities and Exchange Commission. Forward-looking statements speak only as of the day that they are made, and Corning undertakes no obligation to update them in light of new information or future events.

Digital Media Disclosure
In accordance with guidance provided by the SEC regarding the use of company websites and social media channels to disclose material information, Corning Incorporated (“Corning”) wishes to notify investors, media, and other interested parties that it intends to use its website (http://www.corning.com/worldwide/en/about-us/news-events.html) to publish important information about the company, including information that may be deemed material to investors. The list of websites and social media channels that the company uses may be updated on Corning’s media and website from time to time. Corning encourages investors, media, and other interested parties to review the information Corning may publish through its website and social media channels as described above, in addition to the company’s SEC filings, press releases, conference calls, and webcasts.


About Micromax Informatics
Micromax Informatics Limited is the 10th largest mobile brand in the world (Counterpoint Research) and one of the leading consumer electronics companies. Over the past decade, Micromax has pioneered the democratization of technology for the masses by offering affordable innovations through their products and removing barriers for large-scale adoption of advanced technologies. The brand embraces an innovative product portfolio ranging from feature rich, dual ¬SIM phones, 4G Android smartphones, tablets, smart televisions, air conditioners and laptops. With successful operations across India, Russia and other SAARC markets, Micromax sells more than 3 million mobility devices every month.

About Corning Incorporated
Corning (www.corning.com) is one of the world’s leading innovators in materials science. For more than 160 years, Corning has applied its unparalleled expertise in specialty glass, ceramics, and optical physics to develop products that have created new industries and transformed people’s lives. Corning succeeds through sustained investment in R&D, a unique combination of material and process innovation, and close collaboration with customers to solve tough technology challenges. Corning’s businesses and markets are constantly evolving. Today, Corning’s products enable diverse industries such as consumer electronics, telecommunications, transportation, and life sciences. They include damage-resistant cover glass for smartphones and tablets; precision glass for advanced displays; optical fiber, wireless technologies, and connectivity solutions for high-speed communications networks; trusted products that accelerate drug discovery and manufacturing; and emissions-control products for cars, trucks, and off-road vehicles.

Media Relations Contacts:                          

Brittany Salgado
(607) 377-6370
salgadobm2@corning.com

Sonia Jung                            
82-2-709-3446                                              
jungsy@corning.com

Investor Relations Contact:
Ann H.S. Nicholson
(607) 974-6716
nicholsoas@corning.com