LEAF® Optical Fibre
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
LEAF® Optical Fibre

LEAF® Optical Fibre

LEAF® Optical Fibre

World’s most widely-deployed non-zero dispersion-shifted fibre

LEAF® Optical Fibre

LEAF® Optical Fibre

LEAF® optical fibre has become the go-to solution for long-haul and metro networks. In the race to satisfy the global demand for bandwidth, LEAF fibre is the clear winner as the world's most widely deployed non-zero dispersion-shifted fibre (NZDSF).

Additionally, LEAF fibre is the industry leader in polarization mode dispersion (PMD) specifications and has the lowest attenuation of any NZDSF on the market.

Built to withstand decades of demands in challenging environments, LEAF fibre can be used in multiple network architectures and can help existing networks evolve from 10G to the 40G and 100G systems of the future.

In The News

In The News

100G Direct Detection Across Record Distance Achieved

In partnership with ADVA Optical Networking, ADVA 100G Metro solution has been used to successfully transport data over 600km of Corning® LEAF® optical fibre. The demonstration represents the first time that direct-detection 100G technology has been used outside of the metro environment and positions it as a genuine 100G solution for regional networks.

Next-Generation Network To Be Deployed in South Africa

FibreCo Telecommunications, a South African open-access network provider, will deploy Corning® optical fibre in its new ultra-high-speed, long-distance fibre optic network in South Africa.

Increased 100G Efficiency for Metro Networks To Be Showcased

ADVA Optical Networking and Corning will demonstrate a 100G solution for the metro environment at the Optical fibre Communication/National fibre Optic Engineers Conference in Los Angeles. This demonstration will profile the lowest cost-per-bit 100G transmission available over a distance of 125 km without inline amplification or passive dispersion compensation.

Corning’s LEAF® Optical Fibre Now Available with New Lower-Loss Specification

Corning® LEAF® optical fibre, the world’s first large-effective-area, non-zero dispersion-shifted fibre (NZ-DSF) is now further optimised for long-haul networks by applying Corning’s low-loss technology. Already the lowest-loss NZ-DSF fibre on the market, Corning low-loss technology reduces LEAF fibre’s attenuation specification to 0.19dB/km at 1550nm.