Future Technologies

Corning is already at work on new compositions with even higher strain points and temperature tolerances. In addition, Jade will help enable emerging display technologies such as organic light emitting diodes (OLEDs). As current-driven devices, OLEDs require the improved electron mobility of p-Si based TFTs to carry the required current load. The benefits of Jade as a polysilicon backplane can provide that foundation, allowing OLEDs to take full advantage of the technology.

Customers can further optimize OLED performance by using Jade in conjunction with Corning's Vita™ hermetic sealing solution for OLEDs, which increases the lifetime of OLED displays. With Jade and Vita, Corning has solved two of the major issues facing the OLED industry-backplane performance and lifetime.