The Corning® ClearCurve™ Advantage

ClearCurve™ Products & Solutions

The fastest route is not always a straight line.

The world of fiber-to-the-home (FTTH) just turned a major corner. Historically, optical fiber was known to suffer from signal loss when bent tightly. That hurdle is history.

Corning presents the ideal FTTH solution
Working with telecom industry visionaries and leveraging 30 years of interactions with technical field personnel at service providers around the world, Corning has developed the ClearCurve™ solution which is based on a new optical fiber that is hundreds of times more bendable than standard single-mode fiber. It’s now economically feasible to deliver the high speed services customers crave to 680 million apartment homes worldwide.

 What's new
Verizon Purchases Corning® ClearCurve™ Cable Solution Following Successful Field Trials

Time Magazine names the ClearCurve solution to it's list of the "Best Inventions of the Year."

View a video demonstration of the bending performance of the ClearCurve™ solution. 56K | 100K | 300K