Specialty Glass Material Technologies and Innovations | Glass Materials Science | Corning

Extreme closeup of rounded corners of thin glass, multicolored background

What is Advanced Glass?

What is Advanced Glass?

With glass, it's the science — and ongoing innovation — that solves difficult problems.

What is Advanced Glass?

First created as early as 2000 B.C. in the form of decorative beads, glass has long been the standard material for containers, windows, and other essential items in daily life. The vast majority of glass produced in the world remains in this category — mostly from similar soda-lime compositions with a focus on low-cost mass production.

Advanced glass, on the other hand, applies science to the craft of glassmaking. Deep research, relentless experimentation, and constant innovation help improve scientists’ understanding of the fundamental nature of glass down to the molecular level. In so doing, they can exploit the versatility of the material and offer glass-based solutions to some of industry’s toughest problems.

Consider, for example, the pressure on the electronics industry a decade ago to transition to environmentally conscious LCD glass — a material free of heavy metals that could contaminate the earth when computers, TVs, and other devices reached the end of their useful lives. The challenge was enormous for advanced glass makers like Corning since it eliminated elements like antimony, barium, and arsenic — all previously essential ingredients in the making of LCD substrates. The company’s top scientific minds devised a new glass composition that met the new requirements and still enabled brilliant images. Just as importantly, they created a painstakingly accurate melting process to go along with it. The result: EAGLE XG® glass, the first environmentally conscious glass for the LCD industry.

Scientific exploration of glass — and thus, the creation of advanced glass — is still a relatively new endeavor. Over the 4,000-year lifespan of glass as a material, science entered into the glassmaking picture less than 350 years ago, with the work of 17th-century alchemists. Hundreds of years passed between significant innovations in specialty glass.

It wasn’t until companies like Corning began investing in dedicated research and development that advanced glass solutions became a powerful force in shaping industries and transforming lives. 

Read featured facts about Advanced Glass.

Compartilhar