Wireless Convergence
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
Future Networks

Future Networks

Future Networks

Increased connectivity and mobility requirements have driven significant network changes creating management, visibility, performance, and security challenges.

Future Network Needs

The Rule of Three

Three Key Requirements for Any Future Network

What the WAN Means for Your LAN

What the WAN Means for Your LAN

How the Evolution of the Wide Area Network Is Changing Local Area Network Infrastructure Requirements

In the early to mid-2000s, the traditional software model began to move to software-as-a-service (SaaS) and cloud-based delivery, which began to shift local IT thinking in how they support end users. As storage and application left local servers and began to be hosted in data centers, less equipment and on-premise device management was needed, but more emphasis was needed on ISP service delivery and infrastructure ability to handle the speed and payload needed for applications to be supported.

That trend has continued, virtually eliminating the software-in-a-box delivery to an entirely cloud-hosted model. This change in local delivery to data center-hosted and delivered service, coupled with mobile device proliferation and rich media content consumption, drove data center expansion and the need to architect the data center for faster delivery moving from 10Gbps to now 40 and 100Gbps.

As the core network infrastructure changes so too must the local area network, if end users and the overall enterprise are to receive safe, reliable, and high-quality service for all their application needs. To receive the benefits of the evolution, data centers moving to 40 and 100Gbps require a fiber-rich environment in the LAN as well. Whether you are a hospital that requires assured and secure bandwidth for your ER telemetry system or an enterprise that is conducting live HD video conferencing between its remote product management and development teams – latency, capacity limitations, and an inability to ensure dedicated bandwidth at a port are serious considerations in designing and building your network infrastructure.

Fiber vs. Copper

Project Spotlight

Project Spotlight

Corning ONE™ Wireless Platform Enables Best-in-Class Fan Experience at Texas A&M Kyle Field Stadium

One of the largest college football stadiums in the U.S., the newly renovated home of the Texas A&M Aggies, now includes a state-of-the art optical fiber infrastructure that delivers increased capacity and more reliable wireless service. ONE Wireless enables more than 100,000 fans to call, text, and tweet about being at the big game – all at the same time.

Read Mobile Sports Report Article (11/9/15) >

Read Mobile Sports Stadium Tech Report Article (12/14) >

Read Press Release >

Additional Network Considerations

What the WAN Means for Your LAN

How the Evolution of the Wide Area Network Is Changing Local Area Network Infrastructure Requirements

What the WAN Means for Your LAN

Starting in the 2000s, the traditional software model began to move to software-as-a-service (SaaS) and cloud-based delivery causing storage and applications to transfer from local servers to data centers.

This change in delivery methods, coupled with mobile device proliferation and rich media content consumption, drove data center expansion and the need to architect the data center for faster delivery moving from 10Gbps to now 40Gbps and 100Gbps.

This shift requires a fiber-rich LAN to minimize latency and capacity/bandwidth limitations.

Future Network Capacity Requirements

Examining future network capacity requirements in healthcare and hospitality environments

Future Network Capacity Requirements

This white paper examines the current and future bandwidth requirements in both hospitals and hotels, and how the growing adoption of wireless applications are impacting current and future network requirements.

Register Now

Explore Communication Networks Resources