Overview
Where's My Order?
Customer Service
Engineering Services
Training Programs
Rental Program
Project Services
Fusion Splicing Resource Center
Test Equipment Resource Center
UniCam Connector Resources
Sales Development
Technical Resources

TS FSD 400 Fiber System Design Course for Enterprise Networks


Click Here to request a seat online for this class or
call us at (800) 743-2671 and ask for Training Services
.

Interactive Design Course for Multimode and Single-mode Optical Local Area Networks

Description
This optical design course targets customers who desire an in-depth knowledge of optical local area networks. The design course was written by experienced system engineers who work with consultants and end-users daily to meet their optical network requirements.  This four-day course covers all aspects of successful fiber optic system design from network protocols and configurations to optical cabling, industry communications standards, cable and fiber count selection, hardware selection, splicing/termination methods, and cable system testing and documentation.  All that is learned is put into practice through several intensive case studies.

This course incorporates case studies requiring the student to build real fiber optic cabling systems designs; these designs start out simple and grow in complexity as the course progresses.  This work is completed simulating a real world environment for systems design.  This means that maps, drawings, specification sheets, installation procedures, spreadsheets, and other custom built computer-based design tools are used by the students in to create real systems designs.  All the tools and materials required for this are supplied by Corning; this includes: (but is not limited to) a USB flash drive, drawings, maps, line diagrams, splice plans, route diagrams, specification sheets, applications notes, Visio® templates, various white papers, spreadsheet templates and a macro-based bill of materials builder tool.  This tool has been custom written by Corning to aid in the design process.  

A student may bring a laptop computer to the for the systems designs. The student’s computer must be equipped with Microsoft® Windows XP or newer, Microsoft® Excel® 2003 (or newer), and Adobe® Reader®. The computer must be capable of allowing macros to run in Excel®. Corning will provide a netbook computer to any student without a laptop computer.

Class Size:
Class size is a minimum of 6 students, maximum of 12 students
Class Time: 8:30 a.m. - 5:00 p.m.
Class Length: 4 days
BICSI Continuing Education Credit (CEC): RCDD® = 28 hours; NTS = 7; Outside Plant = 7 hours; Installer = 15 hours; Technician = 18 hours; Certified Trainer = 28 hours

 

Curriculum

  • Theory and Principles of Fiber Optics
  • Fiber Types
  • Optical Sources
  • Cable Selection in Network Design
  • Termination and Splicing
  • Hardware
  • Structured Cabling Standards including ANSI/TIA-568-C
  • Standards and Subcommittees
  • National Electrical Code®  (NEC®)
  • Ethernet
  • Fibre Channel
  • Network Cabling Design 
    Data Center Design
  • Cross Connect Design
  • Internetworking
  • Logical Network
  • Optical Testing and Measurements


2012 TS FSD 400 Class Schedules with Pricing

Territory
Classes
Price: $1,399.00
per student
  Regional
Classes
Price: $1,295.00
per student
Phoenix, AZ February 7 - 10 Hickory, NC April 24 - 27
Orlando, FL February 21 - 24 Palo Alto, CA May 8 - 11
Newark, NJ March 6 - 9   Hickory, NC June 19 - 22
Minneapolis, MN May 22 - 25  
Detroit, MI June 5 - 8    

 

 

 

 


 

Refer to discount code "Web2012" when requesting a seat online.  This code could save you 5% off the list price provided payment terms are met.

Discounts and Cancellation Policy: Late cancellations and class no-shows for registered students will incur charges.  A credit card number must be supplied 6 or more business days in advance to honor any/all discount(s) on classes. Credit cards for the class price (list minus applicable discounts) will be billed no sooner than the week the training class occurs.  Credit cards will be billed for late cancellations or no-shows per the Cancellation Policy.   Click Here to view our Cancellation Policy for classes. 

Additional Information:

  • Want a private class at your facility? Class price for a private TS FSD 400 class held at the customer’s facility is $1,295.00 per student plus instructor’s expenses. Expenses include Corning Cable Systems instructor’s air fare, meals, hotel, car rental and incidental expenses and will be billed at actual cost.  (Please note: In order to schedule a class at your facility, you must have a minimum of 8 students.) To request a quote online for a TS FSD 400 class at your facility, click here or call 1-800-743-2671 and ask for Training Services.
  • Sales tax is not included in per student pricing and will be added in applicable regions.
  • All class pricing is in United States dollars.
  • Course fee includes class instruction, course materials (including textbook), certificate of completion and the use of Corning Cable Systems ancillary equipment and hardware.
  • Audio or video taping of any Corning Cable Systems training course is strictly prohibited.
  • Corning Cable Systems reserves the right to make changes to the information contained herein without prior notice.

Click Here to request a seat online for this class or
call us at (800) 743-2671 and ask for Training Services.
 

Microsoft, Excel, Excel 2003, and XP are all registered trademarks of the Microsoft Corporation.  Adobe, Adobe Acrobat, and Reader are all registered trademarks of the Adobe Corporation.