Overview
Where's My Order?
Customer Service
Engineering Services
Training Programs
Rental Program
Project Services
Fusion Splicing Resource Center
Test Equipment Resource Center
UniCam Connector Resources
Sales Development
Technical Resources

Training Courses, Locations & Dates


The training course fee includes class instruction, course materials, certificate of completion and use of Corning Cable Systems ancillary equipment and hardware. Audio or video taping of any Corning Cable Systems training course is strictly prohibited. Corning Cable Systems reserves the right to make changes to the information contained herein without prior notice.

TS LAN 500:
Hands-On Comprehensive Installation Technology Course for Multimode and Single-Mode Optical Local Area Networks
TS LAN 500 is a five-day course that prepares craftsmen for all aspects of fiber optic cable installation in a local area network environment. Both multimode and single-mode fiber types are covered. Cable placement, fusion and mechanical splicing, cable termination (connector installation and pigtail splicing) and acceptance testing are taught with extensive hands-on practice. Also covered is the use of equipment, hardware and procedures pertaining to building distribution and campus applications.

TS FSD 400:
Fiber Optic Design Course for Multimode and Single-Mode Optical Local Area Networks
TS FSD 400 is an optical design course that targets customers who desire an in-depth knowledge of optical LANs. The design course was written by experienced system engineers who work with consultants and end-users daily to meet their optical network requirements. This four-day course covers all aspects of successful fiber optic system design from network protocols, network configurations, optical cabling, industry communications standards, determination of fiber count, hardware selection, splicing/termination methods, and cable system testing and documentation. All that is learned is put into practice through multiple and intensive case studies.

TS ANI 500:
Hands-On Installation Course for Optical Single-Mode Access Networks Used in Fiber-to-the-Home (FTTH) and Fiber-to-the Business (FTTB) Deployments — Collectively Called "FTTx"
TS ANI 500 is a five-day course that prepares craftsmen for all aspects of fiber optic cable installation in an optical access network (FTTx) environment.

TS AND 300:
Comprehensive Cabling System Design Class for Optical Single-Mode Access Networks Used in Fiber-to-the-Home (FTTH) and Fiber-to-the Business (FTTB) Deployments — Collectively Called "FTTx"
TS AND 300 is a three-day interactive course that offers state-of-the-art training in optical access network design (FTTx) for installers, designers, developers and potential investors in this leading-edge telecommunications market of fiber-to-the-home and fiber-to-the-business. Course includes practical, real-world design exercises to reinforce key principals and culminates in a design exercise responding to a typical request for proposal.

TS DC 200:
Fiber Optic Design and Installation Course for Data Centers
Corning Cable Systems' TS-DC-200 course is intended for customers who desire an in-depth knowledge of data center optical network structured cabling design.  This two-day course covers all aspects of successful optical fiber data center design including the applicable requirements of TIA/EIA-942, the Telecommunications Infrastructure Standard for Data Centers.  Students will learn about the topology of the data center along with the passive and active components that comprise the telecommunications infrastructure.  Students will have hands-on contact with the optical hardware and cabling, as well as training with testing and termination of ribbon backbone cable.  This course is authored and taught by experienced system engineers who work with consultants and customers daily to meet their optical network design requirements.  Instruction: instructor-led.

TS LAN 200:
Hands-On Installation Course for Connectorization of Multimode Optical Local Area Networks
TS LAN 200 is a two-day hands-on course that prepares craftsmen for fiber optic connector installation and acceptance testing taught with extensive hands-on practice.

TS LAN 200-A:
Hands-On Connectorization Course for Multimode and Single-Mode Optical Networks
TS LAN 200-A is a two-day hands-on course that prepares craftsmen for fiber optic connector installation and acceptance testing taught with extensive hands-on practice.

TS LAN 201:
Hands-On Splicing Course
TS LAN 201 is a two-day hands-on course that covers fiber optic fusion and mechanical splicing.

TS LAN 300:
Hands-On Installation Course for Connectorization of Multimode and Single-Mode Optical Local Area Networks
TS LAN 300 is a three-day hands-on course that prepares craftsmen for various aspects of fiber optic cable installation in a local area network environment. Mechanical splicing, connector installation and acceptance testing are taught with extensive hands-on practice.

TS LAN 400:
Hands-On Installation Technology Course for Multimode Optical Local Area Networks
TS LAN 400 is a four-day course that prepares craftsmen for all aspects of fiber optic cable installation in a local area network environment. Cable placement, fusion and mechanical splicing, cable termination (connector installation and pigtail splicing) and acceptance testing are taught with extensive hands-on practice. Also covered is the use of equipment, hardware and procedures pertaining to building distribution and campus applications.

TS LAN 501
"To the Point" Training Class: Practical Factors
TS LAN 501 is a one-day course.  After you take this class, all the mystery and confusion associated with fiber optics will be a thing of the past. The following topics are covered: learning how fiber works from the ground up to give the installer a solid knowledge base; shedding light on how fiber is manufactured, explaining what everyone means when discussing ‘attenuation’ and ‘dispersion’, understanding what exactly the differences are between multimode and single mode fiber, and discovering how to pick the correct cable type and hardware for your specific application.

TS LAN 502
"To the Point" Training Class: Splicing and OTDRs
TS LAN 502 is a one-day course.  You will learn all the proper techniques and tips to make your job easier when it comes to fusion and mechanical splicing. Also in this class, you will learn the theory and details behind testing and setup and operation of an OTDR.

TS LAN 503
"To the Point" Training Class: Connector Installation
TS LAN 503 is a one-day course.  The installer will learn the proper techniques to install both factory-polished, no-epoxy/no-polish connectors and hand-polished, anaerobic connectors. Both Multimode and Single-mode single fiber connectors are covered.

TS LAN 505
"To the Point" Training Class: Testing and Emergency Restoration
TS LAN 505 is a one-day course. After taking Corning Cable Systems’ LAN 505 course, the installer will learn the proper steps required to reference a test set, when and why to use a mandrel wrap, and how to develop a loss budget and apply it to a fiber optic system. This training will instill the knowledge necessary to provide quick and proper troubleshooting and emergency restoration techniques that can save time and money on any project.

Entrenamiento TS LAN 500 
Curso Práctico Completo de Tecnología en Instalación de Redes de Fibras Opticas Monomodo y Multímodo
Es un curso de cinco dias que entrena los técnicos en todos los aspectos de instalación de cables de fibras ópticas en un ambiente de red de área local (LAN). Ambos tipos de fibras ópticas, multímodo y monomodo son cubiertas en la clase. Instalación de cables, empalme de fibras empleando técnicas mecánicas y de fusión, terminación de cable (instalación de conectores y empalmes tipo “pigtail”) así como pruebas de aceptación son enseňados con suficientes practicas. En la clase los estudiantes construyen, realizan pruebas y diagnostican fallas de sistemas multimodo y monomodo. El uso de los equipos, y procedimientos relacionados con la distribución de la fibra en edificios y aplicaciones en campus son también cubiertos en la clase.