Overview
News & Events
Newsletter
News Releases
Media Contacts

News Releases

Corning Unveils ClearCurve™ Product Suite Optimized for European MDU Market

Revolutionary optical fiber, cable, hardware and equipment solution based on Corning nanoStructures™ technology

Paris, February 26, 2008 – Corning Incorporated (NYSE:GLW) today unveiled its ClearCurve™ optical fiber-based product suite optimized for the European market at the Fiber-to-the-Home (FTTH) Conference in Paris. Corning's ClearCurve solution was first introduced last October during the U.S. FTTH Conference in Orlando, Fla. The product suite helps overcome the installation challenges in multiple-dwelling units (MDUs) by providing a bend-insensitive fiber optimized for the strenuous deployment conditions seen in these complexes.

Corning is presenting its new ClearCurve riser cable assembly and drop cable at the Paris show. These products help solve the historical technical challenges faced by telecommunications carriers installing FTTH networks in European high-rise apartment buildings and MDUs. This solution is based on Corning's ClearCurve optical fiber which features the company's revolutionary nanoStructures™ fiber design. With this design the optical fiber maintains its signal strength when bent or curved, with performance results 100 times better than standard single-mode fibers and an order of magnitude better than other backwards-compatible bend fibers. The new fiber also enables simpler and more aesthetically pleasing designs for cable, hardware and equipment in MDU deployments.

"This fiber technology coupled with our unique cable design allows cabled fiber to be bent around very tight corners with virtually no signal loss," said Malcolm Barnett, managing director Corning Cable Systems, EMEA. "ClearCurve optical cable enables bends of 5mm radius and the use of stapling secures cables during installation, while still protecting and preserving the required power budgets of telecommunications carriers. ClearCurve optical fiber cables are far more flexible, as rugged as copper cable and easier to route within buildings. And, we have reduced the size and improved the performance of bulky hardware cabinetry, giving building owners and developers an aesthetically appealing solution, while making it easier for carriers to install."

Corning is demonstrating the superior performance of ClearCurve optical fiber, cable, hardware and equipment through live demonstrations on the Corning stand and in-depth presentations in their Visitor Centre at the conference. Telecommunications carriers will see how the Corning ClearCurve solution allows them to design optical fiber cable into these complex environments and give their customers the near infinite bandwidth benefits of FTTH.

For detailed product information, visit www.corning.com/ClearCurve

About Corning Incorporated
Corning Incorporated (www.corning.com) is the world leader in specialty glass and ceramics. Drawing on more than 150 years of materials science and process engineering knowledge, Corning creates and makes keystone components that enable high-technology systems for consumer electronics, mobile emissions control, telecommunications and life sciences. Our products include glass substrates for LCD televisions, computer monitors and laptops; ceramic substrates and filters for mobile emission control systems; optical fiber, cable, hardware & equipment for telecommunications networks; optical biosensors for drug discovery; and other advanced optics and specialty glass solutions for a number of industries including semiconductor, aerospace, defense, astronomy and metrology.

Forward-Looking and Cautionary Statements
This press release contains forward-looking statements that involve a variety of business risks and other uncertainties that could cause actual results to differ materially. These risks and uncertainties include the possibility of changes in global economic and political conditions; currency fluctuations; product demand and industry capacity; competition; manufacturing efficiencies; cost reductions; availability of critical components and materials; new product commercialization; changes in the mix of sales between premium and non-premium products; new plant start-up costs; possible disruption in commercial activities due to terrorist activity, armed conflict, political instability or major health concerns; adequacy of insurance; equity company activities; acquisition and divestiture activities; the level of excess or obsolete inventory; the rate of technology change; the ability to enforce patents; product and components performance issues; stock price fluctuations; and adverse litigation or regulatory developments. Additional risk factors are identified in Corning's filings with the Securities and Exchange Commission. Forward-looking statements speak only as of the day that they are made, and Corning undertakes no obligation to update them in light of new information or future events.

Media Relations Contact:
Lara Brown
+49 (0)30 5303 2613
Lara.Brown@corning.com