Overview
Carrier Networks
Enterprise Networks
Fibre-to-the-Home (FTTH)
Main Distribution Frames & xDSL Splitter Solutions
Splice & Test Equipment

Choosing OTDR parameters


OTDR parameters need to be chosen wisely to match the measurement target. With the correct combination of set ups, the instrument can be used effectively and the user doesn't run risking to have overlooked faults or to have made wrong statements.

STE_Testing_pulse_widths
Length of pulse
widths & detection

Pulse widths affect dead zones and detectability

  • Optical pulses sent by OTDR correspond to physical lengths (for instance 10ns is 1 meter long)
  • As long as a pulse length is shorter than the distance between the first and the subsequent event, the subsequent event can be detected (Event Dead Zone)
  • However, shorter pulse widths have less energy. The pulse can travel less and the OTDR effective dynamic is reduced
  • Practically, a compromise between both parameters must be found

STE_range_resolution
Range and
Resolution

Localization accuracy and measrurement capacity through chosen range & resolution

  • The number of sampling points should be used carefully to achieve location information with proper accuracy during a optical link trouble shooting
  • A higher resolution increases the measurement time for the same averaging
  • Chosen range should cover the actual fiber length + 30% to ensure that no loss in physical resolution occurs

The Corning OV1000 OTDR has a measurement mode that determines the necessary parameters automatically. Also the chosen range resolution is logically calculated to make ful use of the available dynamic and resolution...  > More  


Related Applications:

 

 Fiber Characterization with an OTDR

 Network Approval with Source and Meters

 Fault Locatings with a VFL and an Inspection Probe