ONE Wireless Platform
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
Virtual, 3D cityscape in blue light floats above person's palm

Corning® ONE™ Wireless Platform

Corning® ONE™ Wireless Platform

Enabling All Things Wired and Wireless

Product Spotlight

Saving Space

Enabling Convergence to Minimise Valuable Real Estate.

Enabling Convergence to Minimise Valuable Real Estate.

 

The Corning® ONE™ wireless platform enables the convergence of POL, Wi-Fi, and cellular networks, which can save up to half the space compared to traditional systems.*

With Corning ONE wireless platform, you can reduce or even eliminate equipment in the telco closet and consolidate active electronics at the edge of the network. See our Corning ONE wireless platform brochure for more information.

 

* Average when compared to the Corning MobileAccess2000 platform using MobileAccessHX mid-power remotes in a multicarrier, multiband use case in three different vertical market segments.

Read More

Saving Time

Reduce Installation Time with Our Field-Proven Optical System

Reduce Installation Time with Our Field-Proven Optical System

 

Corning has a long history of creating products that reduce valuable installation time, and this includes the Corning® ONE™ wireless platform.

Our modular, preconnectorised solutions eliminate fibre splicing time, and slide-in modules dramatically simplify installation and upgrades. View product details to learn more.

Learn More

Saving Cost

Save Money and Provide Unlimited Bandwidth

Save Money and Provide Unlimited Bandwidth

 

Optical fibre offers unlimited bandwidth, which not only builds a network for the future but also saves costs over the life of the network.

The Corning® ONE™ wireless platform drives installation cost savings, and future upgrades won’t require cable replacements. Watch the story of the Corning ONE wireless platform for more information.

Watch Now

Case Study

How Guthrie Health Decided on an All-Fibre Network

Guthrie Health Decides on an All-Fibre Network

Guthrie Corning Hospital installs a future-ready network to support wired, wireless, and cellular applications.

Guthrie's newest 268,000 square ft. hospital in Corning, New York needed to find an innovative wireless solution that could meet not only the needs of current users, but those of future users with even greater demands for wireless capabilities.

Guthrie Health collaborated with us to install the Corning® ONE™ wireless platform, the first all-optical PON and cellular solution. As a result of the implementation, Guthrie saved considerable installation time, power, and space (as much as 80 percent in the telecommunications closet).
Watch Now >

Case Study

Red Rock Resort and Casino: One Happy Customer

See how we delivered a solution to one of America’s premiere resorts and casinos without negatively impacting the customer experience and without opening a single wall or ceiling. 

(Hint: We used the existing 1-in. conduit and saved them money too.)
Watch Now >

Prepare for Wireless Deployment