Overview
Company Profile
Corning At A Glance
Our Heritage
Our Values
Our Leadership
Fact Central
Corporate Citizenship
Awards & Recognition
Suppliers
Equity Companies
Locations
Contact Us

Glass — Shattering the Myths


Think you know glass? Allow us to refute some of the commonly held misconceptions about this versatile material.

Myth 1 – Glass is for windows

When people think of glass, they tend to think of simple applications, like windows and cookware; but Corning scientists have manipulated glass at the molecular level to take on countless capabilities.

Corning glass makes high speed communication possible through optical fiber, can help turn solar energy into electricity, and enables thinner, lighter, and more durable display devices. Corning scientists continue to expand the capabilities of glass to solve some of the world’s toughest problems.

Myth 2 – Glass smudges

Nobody wants a hand-held device covered in fingerprints. That’s why Corning is developing glass coatings that reduce the appearance of fingerprints and other smudges.

Myth 3 – All glass is the same

After more than 160 years of glass research, Corning holds hundreds of different patents for glass technology. A single element added to glass can significantly change its properties. By manipulating glass compositions, Corning scientists have developed glass that is light, flexible, durable, and even scratch-resistant.

Myth 4 – Glass is heavy

Corning’s photovoltaic glass, about the thickness of a dime, can provide a very light weight solar energy solution while supporting the extra load of a heavy snowfall.

The lightness and durability of Corning® Gorilla® Glass has led to its use as not only a cover
glass, but as an added design element, in products noted for their light weight.

Myth 5 – Glass is fragile

Solar panels have to endure more than just sunny weather. Corning’s photovoltaic glass, for use in solar panels that convert sunlight into electricity, is designed to last for 25-30 years while enduring severe weather conditions. It can withstand hurricane-force winds and severe hail storms.

Myth 6 – Glass doesn’t bend

While most glass doesn’t bend, Corning has several glass products that do. Corning® ClearCurve® optical fiber cable is flexible enough to be stapled and bent around corners, without sacrificing performance.

Corning® Gorilla® Glass, which provides a protective cover for display devices, can be contoured and shaped without sacrificing strength. And Corning’s ultrathin glass can be rolled like sheets of paper and flexed like wire.

Myth 7 – Glass must be thick to be durable

Corning scientists have proven that materials don’t have to be bulky to be durable. Corning has developed cover glass in large sheets measuring less than 1mm thick that can withstand the force of a remote control thrown at 65 mph.

Myth 8 – Glass doesn’t last

Some of the oldest objects in the universe are particles of glass. Astronauts found glass billions of years old in lunar soil. As Corning scientist Dr. Pete Bocko put it, “A glass object will last until the sun blows up.”

Myth 9 – Glass shows every scratch

In a mobile-device market full of plastic and ordinary glass, it is hard to imagine a product resistant to wear. Corning® Gorilla® Glass is chemically strengthened to serve as protection against flaws and scratches. Products designed with Gorilla Glass resist and withstand damage caused by everyday use. Carrying a cell phone in your pocket with keys is no longer a problem.

Myth 10 – Glass is low tech

Corning makes glass tough enough for windows on the space shuttle entering the atmosphere at 25,000 km per hour, clear enough to carry a pulse of light 1000 km, and pristine enough to make an LCD TV with 3 million pixels. Corning glass is anything but simple.

View a PDF version 

Posted September 2010