Introduction
Maintaining healthy, growing
cell cultures is a demanding task made more difficult by the ever-present risk of their
loss through accidents or contamination. In addition, actively growing cell cultures are
not static but, like all populations of microorganisms, subject to age-related or
environmentally-induced changes which can result in their ongoing evolution and potential
loss.
These problems are reduced by
using cryogenic preservation to stop biological time for cell cultures, effectively
putting them into true suspended animation. This concept, long a favorite ploy of science
fiction writers and movie producers, has been a reality since the important discovery by
Polge, Smith and Parkes (11) in 1949 that glycerol
prevents injury to cells caused by freezing. Many cook book-style protocols are now
available for freezing cells and these procedures usually perform well (3,6,13,14,15,16). It is
essential, however, when problems arise or protocol adaptations and improvements must be
made, that the underlying concepts on which they are based are well understood. This guide
examines both the basic theoretical concepts and practical aspects necessary for
successfully freezing animal cells and managing a cell repository.
Advantages of Freezing Cell Cultures
Once successfully frozen and
stored, cell cultures require little time and effort for their maintenance. The only real
cost is the expense of maintaining an ultracold (-130°C or lower) mechanical freezer or
liquid nitrogen supply. This limited expense compares very favorably with the time, effort
and substantial cost of the media and supplies necessary for maintaining actively growing
cultures, or for the cost of obtaining a new culture from a repository. Frozen cultures
provide an important backup supply for replenishing occasional losses due to contamination
or accidents and provide the assurance of a homogeneous culture supply. Cellular changes
or alterations occur in all actively growing populations. These changes often result in
the loss of important characteristics during evolution of the cultures thereby introducing
unwanted variables into long-term experiments. Cryogenically preserved cultures apparently
do not undergo any detectable changes once they are stored below -130°C (1,8). Therefore, the biological effects of in vitro
cellular aging and evolution may be minimized by frequently returning to frozen stock
cultures, allowing ongoing long-term culture experiments to be successfully completed
without these unwanted variables. Frozen cultures also provide a valuable baseline against
which future experimentally-induced changes may be compared or measured.
Advantages
of Freezing Cultures |
- less work saves time and money.
- serves as a backup supply for emergencies.
- provides a more homogeneous population by
minimizing culture aging and evolution.
|
return to top
General Events During Cell Freezing
To understand why freezing
protocols work, it is necessary to examine both the intracellular and extracellular events
occurring in animal cell cultures during the freezing process (2,4,8). Initial cooling from room temperature to 0°C
slows cellular metabolism, rapidly disrupting active transport and ionic pumping. Usually
this disruption does not result in cellular damage if the culture medium is osmotically
balanced. As cooling continues (0° to -20°C) ice crystals begin to form in the
extracellular environment which increases the solute concentration of the culture medium.
As a result, water begins to move out of the cells and into the partially frozen
extracellular medium, beginning the process of cellular dehydration and shrinkage.
When the cooling process is
rapid, intracellular ice crystals form before complete cellular dehydration has occurred.
These ice crystals disrupt cellular organelles and membranes and lead to cell death during
the recovery (thawing) process.
When the cooling process is
slow, free intracellular water is osmotically pulled from the cells resulting in complete
cellular dehydration and shrinkage. This can also cause cellular death but there is little
agreement on the mechanisms involved. The physical stresses of cellular shrinking may
cause some damage resulting in irreparable membrane loss and cytoskeletal and organelle
disruption. Damage may also be caused by the high concentrations of solutes in the
remaining unfrozen extracellular medium (essentially a brine solution). These solutes
attack cells both externally and internally, resulting in membrane damage, pH shifts and
general protein denaturation.

Figure 1:
Effects of Freezing Rates on Cells
However, when the cooling rate
is slow enough to prevent intracellular ice formation, but fast enough to avoid serious
dehydration effects, cells may be able to survive the freezing and thawing process. This
survival zone or window is readily observed in many bacteria and other prokaryotes, but
for most eukaryotic cells it is nonexistent or very difficult to find without using
cryoprotective agents. These agents have little effect on the damage caused by fast
freezing (intracellular ice crystal formation), but rather prevent or lessen the damage
caused by slow freezing (dehydration and shrinkage) (8).
The final storage temperature
is also critical for successful cryopreservation. To completely stop biological time,
storage temperatures must be maintained below -130°C, the glass transition point below
which liquid water does not exist and diffusion is insignificant. While many cell cultures
are successfully stored at -70°C to -90°C for months or even years,- biological time is
not stopped, only slowed, and cellular damage or changes will accumulate.
Storage in liquid nitrogen at
-196°C effectively prevents all thermally driven chemical reactions. Only photo-physical
effects caused by background ionizing radiation still operate at this temperature.
Thousands of years are estimated to be necessary before background radiation will have a
noticeable effect on cryopreserved cultures (2,8).
Preventing Freezing Damage |
- use slow freezing to remove all
intracellular water
- use cryoprotective agents to minimize
dehydration effects
- store below 130°C to completely stop
biological time
|
return to top
Practical Aspects of Cell Freezing
Under the best of
circumstances the process of freezing remains stressful to all cell cultures. It is
important that everything possible be done to minimize these stresses on the cultures in
order to maximize their subsequent recovery and survival. The following suggestions and
recommendations are designed to augment the protocols referred to earlier.
I.
Cell Selection
First ensure that the cells are in their best possible condition. Select cultures near
the end of log phase growth (approximately 90% confluent) and change their medium 24 hours
prior to harvesting. Carefully examine the culture for signs of microbial contamination.
Facilitate this by growing cultures in antibiotic-free medium for several passages prior
to testing. This allows time for any hidden, resistant contaminants (present in very low
numbers) to reach a higher, more easily detected level. Samples of these cultures are then
examined microscopically and tested by direct culture for the presence of bacteria,
yeasts, fungi, and mycoplasmas.
Mycoplasmas present a special
problem since they can be found in cultures at very high concentrations (up to 108
organisms per milliliter of medium) without any visible effects or turbidity. As a result,
as many as 20% of all animal cell cultures are contaminated by these ubiquitous but unseen
organisms. Although special efforts are required to detect mycoplasmas, the serious
consequences of their presence makes testing frozen culture stocks absolutely essential (9,12).
Check for both the identity of
the cultures and the presence of any expected special characteristics. Monitor cell
identities by karyology and isoenzyme analysis, ensuring that they are, at the very least,
the correct species (10).
II.
Cell Harvesting
Start with the standard harvesting procedure generally recommended for the culture and
be as gentle as possible. Remove all dissociating agents by washing or inactivation
(especially important when using serum-free medium). Centrifugation, when absolutely
necessary, should only be hard enough to obtain a soft pellet; 100 x g for 5 to 6 minutes
is usually sufficient. To ensure uniformity of the final frozen stock, pool the contents
of all harvested culture vessels. This also makes it much easier to perform essential
quality control testing for microbial contamination and culture identity.
Count and then dilute or
concentrate the harvested cell suspension to twice the desired final concentration, which
is usually 4 to 10 million viable cells per milliliter. An equal volume of medium
containing the cryoprotective agent at twice its final concentration will be added later
to achieve the desired inoculum. Keep the cells chilled to slow their metabolism and
prevent cell clumping. Avoid alkaline pH shifts by gassing with CO2 when necessary.
return to top
III.
Cryoprotection
As mentioned earlier, cryoprotective agents are necessary to minimize or prevent the
damage associated with slow freezing. The mechanisms providing this protection, although
not completely understood, appear to work primarily by altering the physical conditions of
both the ice and solutions immediately surrounding (external to) the cells. Permeation of
the cells by cryoprotectants does not appear to be necessary for their proper functions (4). Remember, protection against fast freezing damage
(internal ice formation) is not provided by these agents, but rather by careful control of
the freezing rate. A wide variety of chemicals provide adequate cryoprotection, including
methyl acetamide, methyl alcohol, ethyleneglycol and polyvinyl pyrrolidone (7). However, dimethylsulfoxide (DMSO) and glycerol are the
most convenient and widely used. Many of these agents, although providing excellent
cryoprotection, have toxic side effects on cultures making their use difficult.
DMSO is most often used at a
final concentration of 5-15% (v/v). Always use reagent or other high purity grades that
have been tested for suitability. Sterilize by filtration through a 0.2 micron nylon
membrane in a polypropylene or stainless steel housing and store in small quantities
(5mL). CAUTION: Take special care to avoid contact with solutions containing DMSO. It
is a very powerful polar solvent capable of rapidly penetrating intact skin and carrying
in with it harmful contaminants such as carcinogens or toxins. Some cell lines are
adversely affected by prolonged contact with DMSO. This can be reduced or eliminated by
adding the DMSO to the cell suspension at 4°C and removing it immediately upon thawing.
If this does not help, lower the concentration or try glycerol or another cryoprotectant.
Glycerol is generally used at
a final concentration of between 5 and 20% (v/v). Sterilize by autoclaving for 15 minutes
in small volumes (5mL) and refrigerate in the dark. Although less toxic to cells than
DMSO, glycerol frequently causes osmotic problems, especially after thawing. Always add it
at room temperature or above and remove slowly by dilution.
High serum concentrations may
also help cells survive freezing. Replacing standard media-cryoprotectant mixtures with
95% serum and 5% DMSO may be superior for some overly sensitive cell lines, especially
hybridomas.
Add cryoprotective agents to
culture medium (without cells) immediately prior to use to obtain twice the desired final
concentration (2X). Mix this 2X solution with an equal volume of the harvested cell
suspension (also 2X) to obtain the inoculum for freezing. This method is less stressful
for cells, especially when using DMSO as the cryoprotectant.
IV.
Storage Vessels
After the cryoprotective solution is mixed with the cell suspension, the resulting
inoculum is added in small aliquots (usually 1 to 2 milliliters) to each storage vessel.
Due to the extremely low temperatures encountered during cryogenic storage, not all vessel
materials or designs are suitable or safe. Many materials become very brittle at these
temperatures; vessels made from them may shatter or crack during storage or thawing.
Carefully check the vessel manufacturers' recommendations on proper selection and use.
Also important is selecting
the sealing system or cap design used to maintain the integrity of the vessel, especially
for storage in liquid nitrogen. If these vessels leak during storage (as many do) they
will slowly fill with liquid nitrogen. When they are eventually returned to room
temperature, the liquid nitrogen quickly vaporizes causing a rapid pressure buildup. The
vessels may then violently blow off their caps or explode to vent the pressure and release
their contents into the atmosphere. This is a very dangerous situation, especially if the
vessels contained pathogenic organisms or potentially toxic or harmful substances. Storage
above liquid nitrogen to reduce these potential hazards is strongly recommended in such
situations.
Two types of vessels are
commonly used for cryogenic storage: heat-sealable
glass ampules and plastic (usually polypropylene) screw-capped vials. Both are
available in a variety of sizes (1 to 5 milliliter capacity) although the smaller sizes
are preferred for cryogenic storage (See Figure 2).
Because of sealing and
labeling problems, glass ampules are no longer widely used in cell culture laboratories.
Invisible pinhole leaks may occur in vials during the sealing process; if these are later
stored submerged in liquid nitrogen, they may explode when removed for thawing. Pinholes
can usually be detected before freezing by immersing sealed ampules for 30 minutes in a
chilled solution of 70% ethanol containing 1% methylene blue. This solution will rapidly
penetrate and stain any leaky ampules; after rinsing with water, defective ampules are
then easily detected and discarded.
 |
| Figure 2:
Corning Cryovials |
Due to their greater safety and convenience, plastic vials have largely replaced glass
ampules for cryogenic storage. The wide variety of styles and special features like
printed marking areas and colored caps for easier identification also add to their
popularity.
Several cap styles are
available, some with the internally-threaded stopper, and others with externally-threaded
designs which help minimize contamination (See Figure 3).

Figure
3: Corning Cryovial Cap Designs |
return to top
V. Labeling and Recordkeeping
Providing for long-term location and identification of frozen cultures is the most
frequently overlooked area of cryogenic storage. A cryogenic cell repository is expected
to outlast the laboratory workers who contribute to it, but poorly maintained or missing
inventory records, and improperly or illegibly labeled vials and ampules may prevent this,
especially after the people responsible have gone.
Labels must contain enough
information to locate the appropriate records; usually the culture's identity, date
frozen, and initials of the person responsible are sufficient. Most plastic vials have
printed marking spots or areas for easy labeling. On vials and ampules without marking
spots use cloth labels with special adhesives formulated for cryogenic conditions.
Special ceramic-based inks are
available for labeling glass ampules. These are applied prior to filling and then baked
onto the glass, usually during dry heat sterilization. Permanent marking spots can be
applied on glass ampules with white nail polish. A laboratory marking pen is then used to
write on the spot once it has dried.
No matter which labeling
method is chosen, use special care to check its permanency under cryogenic conditions.
Some marking spots, inks, and labels may flake off or fade during long-term storage; a
trial run of at least several weeks is recommended.
Fully detail in the records
the culture's storage conditions, including all of the following information: culture
identity, passage or population doubling level, date frozen, freezing medium and method
used, number of cells per vial, total number of vials initially frozen and the number
remaining, their locations, their expected viability and results of all quality control
tests performed (sterility, mycoplasma, species, karyotype, etc.). Additional culture
information, especially their origin, history, growth parameters, special characteristics,
and applications, is also helpful and should be included whenever possible.
Make special efforts to keep
all records up to date and to ensure everyone in the facility is properly using them. Use
pre-printed forms to make the information recording process easier and more likely to be
completed. Keep updated, duplicate copies of all critical records in a safe place removed
from the laboratory area to guard against their accidental loss or destruction. This is
especially important if a computer-based recordkeeping system is used; a current back up
copy should always be maintained in addition to the information stored in the computer.
VI.
Cooling Rate
The cooling rate used to freeze cultures must be just slow enough to allow the cells
time to dehydrate, but fast enough to prevent excessive dehydration damage. A cooling rate
of -1°C to -3°C per minute is satisfactory for most animal cell cultures. Larger cells,
or cells having less permeable membranes may require a slower freezing rate since their
dehydration will take longer.
The best way to control
cooling rates is using electronic programmable freezing units. Although expensive, they
allow precise control of the freezing process, give very uniform and reproducible results,
and can freeze large numbers of vials or ampules. Most units are available with chart
recorders for a permanent record of the cooling process.
There are a variety of
mechanical freezing units that provide adequate control of the cooling rate and are
relatively inexpensive. Some units use racks designed to hold vials at predetermined
depths in the neck of a liquid nitrogen freezer. The cooling rate is dependent on the
total number of vials and the depth at which the rack is placed. Another design uses an
alcohol filled metal canister containing a rack with a capacity of 24 vials. The filled
canister is placed in an ultracold mechanical freezer where the alcohol acts as a bath to
achieve more uniform heat transfer and cooling. After freezing 4 to 5 hours, the vials are
removed from the canister and transferred to their final storage locations.
Insulated cardboard or
polystyrene foam boxes are commonly used as freezing chambers in ultracold freezers. These
homemade devices work well with many cell lines but do not always give controlled,
reproducible or uniform cooling. As a result, there may be serious differences in
viability among the vials upon thawing. This homemade approach is not recommended for
valuable or irreplaceable cultures.
No matter which cooling method
is used, transfer from the cooling chamber or device to the final storage location must be
done quickly to avoid warming of the vials. Use an insulated container filled with dry ice
or liquid nitrogen as a transfer vessel to ensure that the cells remain below -70°C.
VII. Cryogenic Storage
Only freezers capable of continually maintaining temperature below -130°C should be
considered for long-term cryogenic storage. Although most liquid nitrogen-cooled freezers
and some specially designed mechanical freezers meet this requirement, most cell culture
laboratories prefer liquid nitrogen freezers (See Figure 4). The final choice is often
based on the availability of a reliable supply of liquid nitrogen, the storage capacity
required, and the size of the budget. Liquid nitrogen freezers permit storage either in
the vapor phase above the liquid at temperature between -140°C and -180°C, or submerged
in the liquid at a temperature below -196°C. Using vapor phase storage greatly reduces
the possibility of leaky vials or ampules exploding during removal. However, since the
amount of liquid nitrogen in the freezer is reduced to provide space for vapor phase
storage, the freezer's holding time (the period it can maintain its storage temperature
without adding more liquid nitrogen) is also reduced. This lowers the freezer's margin of
safety and requires more frequent monitoring and filling. Give careful consideration to
these safety issues when deciding upon a storage method.
Frequently check nitrogen
levels in freezers; a schedule should be established and strictly adhered to. Nitrogen
evaporation is dependent on both the degree of use and the static holding time of the
freezer. Sudden, unexplained increases in the evaporation rate may signal damage to the
insulation or other problems with the freezer and must be carefully investigated. Avoid
frost or ice buildup around freezer openings; this increases the nitrogen evaporation rate
and can cause elevated temperatures in the upper portion of vapor phase freezers. Audible
alarm systems for detecting low liquid nitrogen levels are available to provide additional
safeguards; however, they provide a false sense of security if not monitored 24 hours a
day.
 |
| Figure 4:
Typical Cryogenic Freezers |
return to top
VIII.
Thawing
| CAUTION:
Always use appropriate safety equipment when removing vials and ampules from liquid or
vapor phase nitrogen freezers. A full face shield, heavy gloves and lab coat are strongly
recommended for protection against exploding vials or ampules. |
Remove the vial or ampule
from its storage location and carefully check both the label and storage record to ensure
that it is the correct culture. Place the vessel in warm water, agitating gently until
completely thawed. Rapid thawing (60 to 90 seconds at 37°C) provides the best recovery
for most cell cultures; it reduces or prevents the formation of damaging ice crystals
within cells during rehydration.
IX.
Recovery
Since some cryoprotective agents may damage cells upon prolonged exposure, remove the
agents as quickly and gently as possible. Several approaches are used depending on both
the cryoprotective agents and characteristics of the cells.
Most cells recover normally if
they have the cryoprotective agent removed by a medium change within 6 to 8 hours of
thawing. Transfer the contents of the ampule or vial to a T-75 flask or other suitable
vessel containing 15 to 20 milliliters of culture medium and incubate normally. As soon as
a majority of the cells have attached, remove the medium containing the now diluted
cryoprotective agent and replace with fresh medium.
For cells that are sensitive
to cryoprotective agents, removing the old medium is easily accomplished by gentle
centrifugation. Transfer the contents of the vial or ampule to a 15 mL centrifuge tube
containing 10 mL of fresh medium and spin for 5 minutes at 100 x g. Discard the
supernatant containing the cryoprotectant and resuspend the cell pellet in fresh medium.
Then transfer the cell suspension to a suitable culture vessel and incubate normally.
When glycerol is used as the
cryoprotectant, the sudden addition of a large volume of fresh medium to the thawed cell
suspension can cause osmotic shock, damaging or destroying the cells. Use several stepwise
dilutions with an equal volume of warm medium every 10 minutes before further processing
to give the cells time to readjust their osmotic equilibrium.
X. Problem Solving Suggestions
Viability problems associated with cryogenic storage are usually noticed soon after
cultures are thawed and plated. There are four major areas where problems occur:
During harvesting and
processing of the cells. Problems may be caused by excessive exposure of the cells to
dissociating agents; using a cryoprotective agent that is toxic; or allowing high density
cell suspensions to remain too long at room temperature or at a pH that is too basic.
During the cooling
(freezing) process. Excessive cell damage and reduced culture viability often result
from using a cooling rate that is too fast or too slow, or when the cooling process is
temporarily interrupted. Not using a suitable cryoprotective agent at an appropriate
concentration will also result in viability problems.
During cryogenic storage.
Culture viability is often reduced when vials are allowed to warm up during transfer to
the freezer, or if the repository temperature is not consistently maintained at
appropriate cryogenic temperatures.
During thawing and
recovery. Problems arise when the thawing process is too slow or the cryoprotectants
are improperly removed (see above).
These viability problems can
often be corrected by using the following technique to identify the stage in the freezing
process where the problem originates.
Harvest enough cells to
prepare at least four vials. Then remove a sample of cell suspension, equivalent in cell
number to that which will be placed into the vials, and immediately place it into a
culture vessel with an appropriate amount of medium and incubate. This culture will be
used as a control to compare with the cultures set up in the remaining steps.
Next add the cryoprotective
agent to the remaining cells and divide among three vials. Place one vial at 4°C for one
hour. Then remove the cells from the vial, process as though they had just been thawed
from the freezer, and plate in medium as above. This culture will be compared with the
control culture to determine if there are any problems associated with cryoprotective
agent.
Meanwhile, process the
remaining vials through the slow cooling process as usual. One vial is then immediately
thawed and processed as above. This culture will be compared with the control culture to
determine if there are any problems associated with the slow cooling process.
The remaining vial is then
transferred to the cryogenic freezer and stored overnight before being thawed and
processed as above. This culture will be compared with the control culture to determine if
there are any problems associated with the cryogenic storage conditions. If additional
vials of cells are available, several different recovery techniques should be used to
determine if the recovery technique is the source of the problem.
By comparing all of the
cultures to the original culture, it should then be possible to determine at which stage
of the freezing process the problem occurred. Once this is known, the information
presented in this guide and its references should be enough to eliminate the problem.
Freezing Checklist |
- Gently harvest cultures.
- Check cultures for
contamination, especially mycoplasma.
- Check culture identity by
karyotyping or isoenzyme analysis.
- Use tested cryoprotective
agents.
- Only use vials tested for
cryogenic conditions.
- Ensure labels are permanent
and complete.
- Control the cooling rate.
- Store cultures below
130°C.
- Monitor liquid nitrogen levels
frequently.
- Keep good records.
|
return to top
XI. Managing a Cell Repository
The effort and expenses of managing a repository should be kept in line with the value
of the cultures stored within it. This value is determined by answering two questions: How
much time, money and effort is already invested in these stored cell cultures? And, what
are the consequences of losing them? Cultures that are easily replaced through other labs
or commercial sources may not require special efforts, but unique cultures, such as
hybridomas and other genetically engineered cells, are irreplaceable and require that
special efforts be made to ensure their safety. The answers to these questions will help
determine just how extensive and thorough your efforts should be.
Next, identify the potential
problem areas that can cause the loss of these cultures. Some of these areas, such as
vessel selection, recordkeeping, labeling, freezer monitoring, storage conditions, and
quality issues (contamination and species identity), have already been discussed in this
guide. Decide what steps are necessary to eliminate or minimize these problems. Split
irreplaceable or extremely valuable cultures among several freezers, with at least one
freezer in a separate location to protect against fire or other natural disasters.
Colleagues in other labs or buildings may be able to provide good backup storage,
especially if a reciprocal arrangement is made for them.
One final step remains; plan
ahead for emergencies! One of the most serious and unexpected emergencies is the failure
of a cryogenic freezer. Careful monitoring of the liquid nitrogen level or charting the
temperature may give an early warning that failure is occurring, but middle of the night
failures can and do happen. Have plans prepared in advance to deal with freezer failure
and other problems. If these involve a colleague's equipment, get permission and make all
necessary arrangements in advance-late night phone calls are usually not appreciated.
This information has been
compiled to provide a guide for better understanding of the cryogenic preservation
process. For additional assistance in this area, please contact Corning Corporation
Technical Services at 1-800-492-1110.
References
Aswood-Smith,
M. J. and G. B. Friedmann, 1979. Lethal and Chromosomal Effects of Freezing,
Thawing, Storage Time and X-irradiation on Mammalian Cells Preserved at -196°C in
Dimethylsulfoxide. Cryobiology 16:132-140.
Aswood-Smith,
M. J., 1980. Low Temperature Preservation of Cells, Tissues and Organs, p. 19-44.
In Low Temperature Preservation in Medicine and Biology. M. J. Aswood-Smith and
J. Farrant, Eds. (Pitman Medical Limited, Kent, England).
Coriell, L.
L., 1979. Preservation, Storage and Shipment, p. 29-35. In Methods in Enzymology.
Vol. 58, W. B. Jacoby and I. H. Pasten, Eds., (Academic Press, New York).
Farrant,
J., 1989. General Observations on Cell Preservation, p. 1-18. In Low Temperature
Preservation in Medicine and Biology, M. J. Aswood-Smith and J. Farrant, Eds.
(Pitman Medical Limited, Kent, England).
Freshney,
R. I., 1994. Culture of Animal Cells: A Manual of Basic Technique, p.
254-263. (3rd edition; Wiley-Liss, New York.
Hay, R. J.,
1978. Preservation of Cell Culture Stocks in Liquid Nitrogen, p. 787-790.
TCA Manual 4.
Klebe, R.
J. and M. G. Mancuso, 1983. Identification of New Cryoprotective Agents for
Cultured Mammalian Cells. In Vitro 19:167-170.
Mazur, P.,
1984. Freezing of Living Cells: Mechanisms and Implications, p.
C125-C142. Am. J. Physiol. 247 (Cell Physiol. 16).
McGarrity,
G. J., J. Sarama, and V. Vanaman, 1985. Cell Culture Techniques. ASM News
51:170-183.
Peterson,
W. D., W. F. Simpson and B. Hukku, 1973. Cell Culture Characterization:
Monitoring for Cell Identification, p. 164-178. In Tissue Culture: Methods and
Applications, P. F. Kruse and M. K. Patterson Jr. Eds. (Academic Press, New
York).
Polge, C.,
A. U. Smith, and A. S. Parkes, 1949. Revival of Spermatozoa after
Vitrification and Dehydration at Low Temperatures. Nature 164: 666.
Ryan, J.,
1994. Understanding and Managing Cell Culture Contamination, TC-CI-559.
Corning Corporation Technical Monograph.
Schroy, C.
B., and P. Todd, 1976. A Simple Method for Freezing and Thawing Cultured
Cells, p. 309-310. TCA Manual 2, Procedure Number 76035.
Shannon,
J. E. and M. L. Macy, 1973. Freezing, Storage, and Recovery of Cell Stocks, p.
712-718. In Tissue Culture: Methods and Applications. P. F. Kruse and M. K.
Patterson Jr. Eds. (Academic Press, New York).
Smith, K.
O., 1981. Low Temperature Storage of Surface Attached Living Cell Cultures.
Cryobiology 18:251-257.
Waymouth,
C. and D. S. Varnum, 1976. Simple Freezing Procedure for Storage in Serum-free
Media of Cultured and Tumor Cells of Mouse, p. 311-313. TCA Manual 2, Procedure
Number 76165.
return to top
|