|
C/C |
Center Conductor |
| CM |
Catchers Mitt |
| dB |
Decibels |
| ↓ |
Diameter |
| Ø |
Diameter symbol |
| ESD |
Electrostatic discharge |
| FD |
Full Detent |
| GHz |
Gigahertz |
| LD |
Limited Detent |
| mm |
Millimeter |
| MP |
Microporous |
| PCB |
Printed Circuit Board |
| RF |
Radio frequency |
| R/A |
Right Angle |
| R/P |
Reference Plane |
| S/R |
Semi-Rigid |
| SB |
Smooth Bore |
| SQ |
Square |
| VSWR |
Voltage Standing Wave Ratio |
return to top
standard tolerances
All dimensions are in inches, interpretation per ANSI Y14.5.
.XX ± .010
.XXX ± .005
Angular ± 5°
Typical machine surface finish 32 microinches
Fractions ± 1/64
return to top
glossary of common terms
- Blindmate Interconnect
-
or blindmate (often referred to as a ‘bullet’). A female to female within
series adapter which is captivated between two panel or circuit mounted males
(called shrouds). A blindmate allows increased misalignment between two
modules.
- Detent
-
The detent is a ring which interacts with the slotted outer conductor of the
mating female to produce repeatable levels of mate retention. The detent ring
is located within the male shroud.
- GPO Detent
-
The GPO detent is a physical feature located within the GPO male shroud that
interacts with the GPO female to produce repeatable levels of mate retention.
- Female Interface
-
The orientation of an RF connector is determined by the inner conductor. The
female interface uses a slotted inner conductor as a receptable for the pin
contact of the mating male interface.
- Jack Interface
-
The orientation of a RF connector is determined by the inner conductor. The
jack, or female, interface uses a slotted inner conductor as a receptacle for
the pin contact of the mating plug, or male, interface.
- Male Interface
-
The orientation of an RF connector is determined by the inner conductor. The
male interface uses a pin contact to mate with the slotted center contact
receptacle of the female interface.
- Plug Interface
-
The orientation of a RF connector is determined by the inner conductor. The
plug, or male, interface uses a pin contact to mate with the slotted receptacle
contact of the mating jack, or female, interface.
- Shroud
-
The outer conductor portion of the GPO or GPPO male interface. The shroud
protects the female interface, provides electrical contact, and houses the
detent ring.
When used in the GMS product line context the shroud refers to the portion of
the GMS jack outer conductor that protects the electrical contact and guides
the GMS plus into position.
- Cap
-
Captivated
- Sep
-
Separate
|